1. Article purpose[edit | edit source]
This article provides the basic information needed to start using the Linux® kernel tool: ifconfig[1].
2. Introduction[edit | edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ Only supported for STM32MP15x lines | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
ifconfig | Monitoring tools | ifconfig[1] is a system administration utility for network interface configuration. ifconfig is deprecated and has been replaced by ip (A web page provides a comparison between ifconfig and ip [2]) |
3. Installing the trace and debug tool on your target board[edit | edit source]
3.1. Using the STM32MPU Embedded Software distribution[edit | edit source]
ifconfig is installed by default and ready to be used with all STM32MPU Embedded Software Packages.
It comes with the busybox:
which ifconfig | xargs ls -la /sbin/ifconfig -> /bin/busybox.nosuid
3.2. Using the STM32MPU Embedded Software distribution for Android™[edit | edit source]
ifconfig is installed by default and ready to be used with all STM32MPU Embedded Software Packages for Android™.
It comes with the toybox:
which ifconfig | xargs ls -la /system/bin/ifconfig -> toybox
4. Getting started[edit | edit source]
Follow the sequence described below to get started with the ifconfig tool.
Below information is related to the Android™ distribution Need to enable root access rights for any changes
adb root adb shell ...
su ... |
4.1. List the available network interfaces[edit | edit source]
ifconfig
eth0 Link encap:Ethernet HWaddr 00:80:E1:42:43:65 inet addr:10.48.1.144 Bcast:10.48.3.255 Mask:255.255.252.0 inet6 addr: fe80::280:e1ff:fe42:4365%lo/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:181274 errors:0 dropped:14553 overruns:0 frame:0 TX packets:28583 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:23082127 (22.0 MiB) TX bytes:6438412 (6.1 MiB) Interrupt:66 Base address:0x4000 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1%1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:202 errors:0 dropped:0 overruns:0 frame:0 TX packets:202 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:13454 (13.1 KiB) TX bytes:13454 (13.1 KiB)
4.2. Disable the network interface[edit | edit source]
- For example, proceed as follows for eth0
ifconfig eth0 down
4.3. Enable the network interface if it is not already available[edit | edit source]
- For example, proceed as follows for eth0
ifconfig eth0 up
4.4. Assign a given IP address to a network interface[edit | edit source]
- Proceed as follows to assign 10.48.1.324 address to eth0
ifconfig eth0 10.48.1.324
5. To go further[edit | edit source]
Refer to the man page[1] for more details on command options.
6. References[edit | edit source]