1. Article purpose[edit source]
The purpose of this article is to explain how to configure the BSEC using the device tree mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.
2. DT bindings documentation[edit source]
Generic information about NVMEM is available in the NVMEM overview.
The device tree binding documents for BSEC are stored either in the given applicable components listed below, or in the Linux kernel repository:
- TF-A BL2:
- for example: docs/devicetree/bindings/soc/st,stm32-romem.txt
- OP-TEE:
- for example: STM32 BSEC device tree bindings: documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml
- U-Boot, Linux® OS:
- for example: STM32 BSEC device tree bindings: Documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml
- for example: generic NVMEM devicetree bindings: Documentation/devicetree/bindings/nvmem/nvmem.yaml , Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32/SoC level)[edit source]
The BSEC node and NVMEM node are located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.
3.2. DT configuration (board level)[edit source]
The objective of this chapter is to explain how to enable and configure the BSEC DT nodes for a board.
Peripheral configuration should be done in specific board device tree files (board dts file).
3.2.1. BSEC node append[edit source]
The board definition in the device tree may include some additional board-specific OTP declarations :
&bsec {
board_id: board_id@ec {
reg = <0xec 0x4>;
st,non-secure-otp;
};
};
With only 32 lower NVMEM 32-bit data words, the software (OP-TEE) needs to manage exceptions in order to allow some upper OTPs to be accessed by the non-secure world, through secure world services for very specific needs. The user can add an OTP declaration in the device tree, using the st,non-secure-otp property used in secure world device tree, with a 32-bit length granularity (that is, 4 bytes).
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in DT binding files listed in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information: