Template:ArticleMainWriter Template:ArticleApprovedVersion
When your PC is connected on Network protected by Proxy, in order to avoid proxy issue when downloading Open Source packages, some utilities are embedded in a baseline.
1. Proxy issues[edit | edit source]
Before downloading a baseline and having access to the "proxy bypass" help (utility described in next chapter), you may already encounter issues with proxy.
A proxy server is generally another computer serving as a hub through which internet traffic is processed and controlled (in both ways). A proxy used in a facility may exercise some controls on web accesses, including controls on the protocol, the ID of the request, the destination internet address...
"ID of the request" means the proxy server needs to authenticate the requester. So within the proxy settings you will find your login and password.
A proxy that is inappropriately configured may brake the access to useful services on the internet.
1.1. Check your computer has the right proxy settings[edit | edit source]
If needed, ask your IT department for your proxy address. Template:InternalInfo
- Ping your proxy to make sure you have the right name (you obtain in return its IP address (may be useful))
Template:PC$ ping -c 1 <yourproxy.com> PING <yourproxy.com> (xx.yyy.zz.v) 56(84) bytes of data. 64 bytes from <yourproxy.com> (xx.yyy.zz.v): icmp_seq=1 ttl=58 time=14.6 ms --- <yourproxy.com> ping statistics --- 1 packets transmitted, 1 received, 0% packet loss, time 0ms rtt min/avg/max/mdev = 14.669/14.669/14.669/0.000 ms
Any application requesting interaction with the Internet will require your proxy server address because every request to the internet will have to be routed to it first. Check your environment variables, this is usually how applications determine the proxy server. These variables may be defined in upper case or lower case.
- On LinuxTemplate:Sup:
Template:PC$ env | grep proxy http_proxy=http://<login>:<password>@<yourproxy.com>:8080 ftp_proxy=http://<login>:<password>@<yourproxy.com>:8080 https_proxy=http://<login>:<password>@<yourproxy.com>:8080
If not done yet, you have to export the required variables, for ex:
Template:PC$ export http_proxy=http://<login>:<password>@<yourproxy.com>:8080
- On WindowsTemplate:Sup:
Seach "variables" in your WindowsTemplate:Sup environment and enter a new variable for your account in the dialog box like below:
Ex: Variable="HTTP_PROXY" value="http://<login>:<password>@<yourproxy.com>:8080"
1.2. Check your proxy can bypass standard requests (needed for Yocto development)[edit | edit source]
- HTTP
Template:PC$ curl -v http://github.com . . > Host: github.com > Accept: */* . .
- HTTPS
Template:PC$ curl -v https://github.com . . > Host: github.com > Accept: */* . .
- GIT
Template:PC$ git ls-remote git://git.openembedded.org/openembedded-core.git 6b9dd7a589537b12da648be50298cf7d36461797 HEAD . .
- SSH
SSH protocol is not used for ST deliveries, proxy bypass is very complex and IT dependent.
One could test ssh access thanks to Github: See this page.
Template:Info Template:InternalInfo
2. How to use proxy bypass ?[edit | edit source]
From the directory in which the repo sync has been launched, execute the following instructions :
- First use: initialization required
Template:PC$ ./meta-st/scripts/proxy_bypass.sh init Template:PC$ ./meta-st/scripts/proxy_bypass.sh enable
- Populate ENV proxy variables for OpenEmbedded usage (two options)
- Set ENV proxy variables ONLY for the current bash session
Template:PC$ source ./meta-st/scripts/proxy_bypass.sh session
- Preferred solution since modifications are efficient for any new bash session : set/copy ENV proxy variables in your bashrc file
Template:PC$ ./meta-st/scripts/proxy_bypass.sh bashrc Template:PC$ source $HOME/.bashrc
- Dynamic proxy bypass script activation/deactivation
- If a PC is not connected on the Network for which the proxy bypass has been configured: you can disable the proxy bypass configuration:
Template:PC$ ./meta-st/scripts/proxy_bypass.sh disable
- When a PC is connected again on the Network: you can re-enable you proxy bypass configuration:
Template:PC$ ./meta-st/scripts/proxy_bypass.sh enable
- Password update
- Update of the password: .bashrc file will be automatically updated if it was populated previously
Template:PC$ ./meta-st/scripts/proxy_bypass.sh update
- To apply password update:
[current bash session ] Template:PC$ source ./meta-st/scripts/proxy_bypass.sh session [bashrc used by script] Template:PC$ source $HOME/.bashrc