Last edited one month ago

STM32MP25 peripherals overview

Applicable for STM32MP25x lines

This article lists all internal peripherals embedded in STM32MP25x lines More info.png and shows the assignment possibilities to the execution contexts for each one of them.
From this article, you can also access to individual peripheral articles with information related to the overview and configuration aspects.

1. Internal peripherals overview[edit | edit source]

The figure below shows all peripherals embedded in STM32MP25x lines More info.png, grouped per functional domains that are reused in many places of this wiki to structure the articles.
Several execution contexts exist on STM32MP25x lines More info.png[1], corresponding to the different Arm cores and associated security modes:

  •  Arm dual core Cortex-A35 secure  (Trustzone), running ROM code and TF-A BL2 at boot time, and running OP-TEE and/or TF-A BL31 at runtime
  •  Arm dual core Cortex-A35 non secure , running U-Boot at boot time, and running Linux at runtime
  •  Arm Cortex-M33 secure  (Trustzone), running TF-M
  •  Arm Cortex-M33 non-secure , running STM32Cube
  •  Arm Cortex-M0+, running HAL driver.

The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:

STM32MP25IPsOverview legend.png

  • When a peripheral box owns execution context color, that means the assignment of this peripheral is fixed by hardware to the execution context.
  • When a peripheral box owns a mix of two execution colors that means this peripheral is shared by hardware between the two execution contexts.
  • When a peripheral box has dark gray color, that means this peripheral is protected by RIF and could be assigned to any execution context.
  • When a peripheral box has light gray color, that means this peripheral is a RIF-aware peripheral. This peripheral owns several features which can be assigned independently to any execution context.

Internal peripheral assignment tables list assignment capabilities for each peripheral.

Both the diagram below and the following summary tables (in Internal peripherals runtime assignment and Internal peripherals boot time assignment chapters below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP25 reference manual [2] may expose more possibilities than what is shown here.


RTCFMCSAESDCMII3CSAISPDIF-RXI2SUSARTUARTADCVREFBUFUSBHETHLPTIMTIMEXTIIPCCI2CGPUDSILTDCIWDG2IWDG3SysCfgHPDMALPDMAUSB3DRCRCCRYPRNGHASHRCCBSECTAMPHDPGICSTGENCortex-A35DTSPWROCTOSPIFDCANSDMMCIWDG4GPIOA-KDBGMCUPCIeIWDG1ADFCSIGPIO-ZOTFDECRISAFRIFSCRISABNVICLPUARTHSEMMDFCortex-M33ETHSWWWDGOCTOSPIMLVDSDCMIPPVENCVDECPKAUCPDCOMBOPHYSERCUSB2PHYSYSRAMRETRAMDDR CTRLBKPSRAMLPSRAMSRAMSPICortex-M0+IWDG5WWDG2Coresight
STM32MP25 internal peripherals overview

2. Internal peripherals runtime assignment[edit | edit source]

Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by OpenSTLinux BSP:

  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in OpenSTLinux BSP.
  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

ADF internal peripheral
Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
nonsecure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
nonsecure
(STM32Cube)
Cortex-M0+
(STM32Cube)
Core/Processors Arm® Cortex®-A35 Arm® Cortex®-A35 OP-TEE
TF-A BL31
Core/Processors Arm® Cortex®-M33 (coprocessor) Arm® Cortex®-M33 (coprocessor) OP-TEE Controlled by LInux or OP-TEE.
Running the STM32CubeMP2 firmware.
Core/Processors Arm® Cortex®-M0+ (coprocessor) Arm® Cortex®-M0+ (coprocessor) OP-TEE
Power & Thermal VREFBUF VREFBUF OP-TEE OP-TEE offers SCMI regulator service to manage VREFBUF
Analog ADC ADC12 OP-TEE
ADC3 OP-TEE ADC3 may be used by the UCSI firmware to measure the Vbus level on the Type-C connector.
Analog MDF MDF1 OP-TEE
Low speed interface or audio SPI SPI2S1 OP-TEE
SPI2S2 OP-TEE
SPI2S3 OP-TEE
SPI4 OP-TEE
SPI5 OP-TEE
SPI6 OP-TEE
SPI7 OP-TEE
SPI8 OP-TEE
Audio SPDIFRX SPDIFRX OP-TEE
Audio SAI SAI1 OP-TEE
SAI2 OP-TEE
SAI3 OP-TEE
SAI4 OP-TEE
Coprocessor IPCC Info.png IPCC1 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
IPCC2 OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core SYSCFG SYSCFG
Core STGEN STGEN OP-TEE
TF-A BL31
Read-only
(STGENR)
Read-only
(STGENR)
Read-only
(STGENR)
Core RTC Info.png RTC Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core/DMA HPDMA Info.png

HPDMAx (x = 1 to 3) OP-TEE - Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core/DMA LPDMA Info.png

LPDMA OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core/Interrupts EXTI Info.png EXTI1 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
EXTI2 Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core/Interrupts NVIC NVIC CM33 Fixed to CM33
NVIC CM0+
Core/Interrupts GIC GIC OP-TEE
TF-A BL31
Fixed to CA35
Core/IOs GPIO Info.png GPIO Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Core/RAM SYSRAM SYSRAM BL31

OP-TEE

Cortex-A35 secure section required for low power entry and exit

Core/RAM DDRCTRL DDR OP-TEE
TF-A BL31
Core/RAM BKPSRAM BKPSRAM OP-TEE

TF-A BL31

TF-M uses BKPSRAM for ITS (Internal Trusted Storage)
Core/RAM RETRAM RETRAM OP-TEE

TF-A BL31

Core/RAM SRAM SRAM1 OP-TEE

BL31

OP-TEE populate OTP shadow region
SRAM2 OP-TEE

BL31

Core/RAM LPSRAM LPSRAM1 OP-TEE

BL31

Should contain Cortex-M0+ firmware code
LPSRAM2 OP-TEE

BL31

Should contain Cortex-M0+ firmware data
LPSRAM3 OP-TEE

BL31

Core/Timers TIM TIM1 OP-TEE
TIM10 OP-TEE
TIM11 OP-TEE
TIM12 OP-TEE
TIM13 OP-TEE
TIM14 OP-TEE
TIM15 OP-TEE
TIM16 OP-TEE
TIM17 OP-TEE
TIM2 OP-TEE
TIM20 OP-TEE
TIM3 OP-TEE
TIM4 OP-TEE
TIM5 OP-TEE
TIM6 OP-TEE
TIM7 OP-TEE
TIM8 OP-TEE
Core/Timers LPTIM LPTIM1 OP-TEE LPTIM1 can be used for HSE monitoring.
LPTIM2 OP-TEE
LPTIM3 OP-TEE LPTIMy (y = 3, 4, 5) can be used for scheduling in low power modes by Linux
LPTIM4 OP-TEE LPTIMy (y = 3, 4, 5) can be used for scheduling in low power modes by Linux
LPTIM5 OP-TEE LPTIMy (y = 3, 4, 5) can be used for scheduling in low power modes by Linux
Core/Watchdog IWDG IWDG1 OP-TEE
TF-A BL31
IWDG2 OP-TEE
TF-A BL31
IWDG3
IWDG4
IWDG5
Core/Watchdog WWDG WWDG1
WWDG2
High speed interface USB3DR USB3DR OP-TEE The USB3DR running at USB3 speed and the PCIe are mutually exclusive. Both require to use the ComboPHY.
High speed interface USBH USBH OP-TEE
High speed interface UCPD UCPD1 OP-TEE
High speed interface COMBOPHY COMBOPHY OP-TEE COMBOPHY can be assigned to either the USB3DR or the PCIe.
High speed interface USB2PHY Info.png USB2PHY1 OP-TEE
TF-A BL31
Allocation inherited from USBH
USB2PHY2 OP-TEE
TF-A BL31
Allocation inherited from USB3DR
High speed interface PCIE PCIE OP-TEE The PCIe and the USB3DR running at USB3 speed are mutually exclusive. Both require using the ComboPHY.
Low speed interface USART USART1 OP-TEE
TF-A BL31
USART2 OP-TEE
TF-A BL31
USART3 OP-TEE
TF-A BL31
UART4 OP-TEE
TF-A BL31
UART5 OP-TEE
TF-A BL31
USART6 OP-TEE
TF-A BL31
UART7 OP-TEE
TF-A BL31
UART8 OP-TEE
TF-A BL31
UART9 OP-TEE
TF-A BL31
Low speed interface I2C I2C1 OP-TEE
TF-A BL31
I2C2 OP-TEE
TF-A BL31
I2C3 OP-TEE
TF-A BL31
I2C4 OP-TEE
TF-A BL31
I2C5 OP-TEE
TF-A BL31
I2C6 OP-TEE
TF-A BL31
I2C7 OP-TEE
TF-A BL31
I2C8 OP-TEE
TF-A BL31
Low speed interface I3C I3C1 OP-TEE
TF-A BL31
I3C2 OP-TEE
TF-A BL31
I3C3 OP-TEE
TF-A BL31
I3C4 OP-TEE
TF-A BL31
Mass storage OCTOSPI OCTOSPI1 OP-TEE OP-TEE need to access OCTOSPI1 at boot time to set OSPIM mode
OCTOSPI2 OP-TEE OP-TEE need to access OCTOSPI2 at boot time to set OSPIM mode
Mass storage OCTOSPIM OCTOSPIM OP-TEE
Mass storage FMC Info.png FMC Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Mass storage SDMMC SDMMC1 OP-TEE
SDMMC2 OP-TEE
SDMMC3 OP-TEE
Networking FDCAN FDCAN1 OP-TEE
FDCAN2 OP-TEE
FDCAN3 OP-TEE
Networking ETHSW ETHSW OP-TEE
Networking ETH ETH1 OP-TEE
ETH2 OP-TEE
Power & Thermal RCC Info.png RCC Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Power & Thermal PWR Info.png PWR Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Power & Thermal DTS DTS OP-TEE
Security BSEC BSEC OP-TEE
TF-A BL31
Security RNG RNG OP-TEE
Security HASH HASH OP-TEE
Security CRYP CRYP1 OP-TEE
CRYP2 OP-TEE
Security CRC CRC OP-TEE
Security SAES SAES OP-TEE
Security TAMP Info.png TAMP Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Security OTFDEC OTFDEC1 OP-TEE
OTFDEC2 OP-TEE
Security PKA PKA OP-TEE
Security RIFSC RIFSC OP-TEE
Security RISAB RISAB1 OP-TEE
RISAB2 OP-TEE
RISAB3 OP-TEE
RISAB4 OP-TEE
RISAB5 OP-TEE
RISAB6 OP-TEE
Security RISAF RISAF1 OP-TEE OP-TEE configures all regions
RISAF2 OP-TEE OP-TEE configures all regions
RISAF4 OP-TEE OP-TEE configures all regions except its own
RISAF5 OP-TEE OP-TEE configures all regions
Security IAC IAC OP-TEE Fixed to TDCID
Trace & debug SERC SERC OP-TEE
Trace & Debug HDP HDP OP-TEE
Trace & Debug DDRPERFM DDRPERFM OP-TEE Part of DDRSS protected by RCC DDR_CFGR
Visual GPU GPU OP-TEE
Visual DSI Info.png DSI Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Visual LTDC Info.png LTDC OP-TEE Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature
Visual DCMI DCMI OP-TEE
Visual CSI CSI OP-TEE
Visual LVDS LVDS OP-TEE
Visual DCMIPP DCMIPP OP-TEE
Visual VENC VENC OP-TEE
Visual VDEC VDEC OP-TEE

3. Internal peripherals boot time assignment[edit | edit source]

Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by OpenSTLinux BSP:

  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in OpenSTLinux BSP.
  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the OpenSTLinux BSP.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

ADF internal peripheral
Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
nonsecure
(U-Boot)
Core/Processors Arm® Cortex®-A35 Arm® Cortex®-A35
Core/Processors Arm® Cortex®-M33 (coprocessor) Arm® Cortex®-M33 (coprocessor) How to start the coprocessor from the bootloader
How_to_protect_the_coprocessor_firmware
Core/Processors Arm® Cortex®-M0+ (coprocessor) Arm® Cortex®-M0+
Analog VREFBUF VREFBUF OP-TEE offers SCMI regulator service to manage VREFBUF
Analog ADC ADC12
ADC3
Analog MDF MDF1
Low speed interface or audio SPI SPI2S1
SPI2S2
SPI2S3
SPI4
SPI5
SPI6
SPI7
SPI8
Audio SPDIFRX SPDIFRX
Audio SAI SAI1
SAI2
SAI3
SAI4
Coprocessor IPCC Info.png IPCC1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
IPCC2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core SYSCFG SYSCFG
Core STGEN STGEN Read-only
(STGENR)
Core RTC Info.png RTC Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core/DMA HPDMA Info.png HPDMAx (x = 1 to 3) Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core/DMA LPDMA Info.png LPDMA1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core/Interrupts EXTI Info.png EXTI1 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
EXTI2 Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core/Interrupts GIC GIC
Core/IOs GPIO Info.png GPIO Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Core/RAM SYSRAM SYSRAM
Core/RAM DDRCTRL DDR
Core/RAM BKPSRAM BKPSRAM
Core/RAM RETRAM RETRAM DDR parameters are stored in RETRAM by TF-A BL2.
Core/RAM SRAM SRAM1 Used during cold boot by TF-A BL2 for DDR firmware loading
SRAM2
Core/RAM LPSRAM LPSRAM1
LPSRAM2
LPSRAM3
Core/Timers TIM TIMx (x = 1 to 8, 10 to 17, 20)
Core/Timers LPTIM LPTIMx (x = 1 to 5)
Core/Watchdog IWDG IWDG1
IWDG2
IWDG3
IWDG4
IWDG5
Core/Watchdog WWDG WWDG1
WWDG2
High speed interface USB3DR USB3DR The USB3DR can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot.
It can be used also in U-boot with command line tools.
High speed interface USBH USBH
High speed interface COMBOPHY COMBOPHY
High speed interface UCPD UCPD1
High speed interface USB2PHY Info.png USB2PHY1 USB2PHY1 can be used in U-boot by USBH with command line tools.
USB2PHY2 USB2PHY2 can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot.
It can be used also in U-boot by USB3DR with command line tools.
High speed interface PCIE PCIE The PCIe and the USB3DR running at USB3 speed are mutually exclusive. Both require using the ComboPHY.
Low speed interface USART USART1
USART2
USART3
UART4
UART5
USART6
UART7
UART8
UART9
Low speed interface I2C I2C1
I2C2
I2C3
I2C4
I2C5
I2C6
I2C7
I2C8
Low speed interface I3C I3C1
I3C2
I3C3
I3C4
Mass storage OCTOSPI OCTOSPI1
OCTOSPI2
Mass storage OCTOSPIM OCTOSPIM TF-A BL2 relies on OCTOSPIM configuration applied by ROM code
Mass storage FMC Info.png FMC Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Mass storage SDMMC SDMMC1
SDMMC2
SDMMC3
Networking FDCAN FDCAN1
FDCAN2
FDCAN3
Networking ETHSW ETHSW
Networking ETH ETH1
ETH2
Power & Thermal RCC Info.png RCC Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Power & Thermal PWR Info.png PWR Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Power & Thermal DTS DTS
Security BSEC BSEC
Security RNG RNG
Security HASH HASH
Security CRYP CRYP1 ROM code allocation is managed with the bit 8 in OTP 16
CRYP2
Security SAES SAES ROM code allocation is managed with the bit 8 in OTP 16
Security TAMP Info.png TAMP Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Security OTFDEC OTFDEC1
OTFDEC2
Security PKA PKA Assignment is mandatory only for secure boot
Security RIFSC RIFSC
Security RISAB RISAB1
RISAB2
RISAB3 Used by ROM code only in serial boot for USB buffer management
RISAB5 Used by ROM code only during cold boot
Security RISAB RISAB1
RISAB2
RISAB3 Used by ROM code only in serial boot for USB buffer management
RISAB4
RISAB5 Used by ROM code only during cold boot
RISAB6
Security RISAB RISAB1
RISAB2
RISAB3 Used by ROM code only in serial boot for USB buffer management
RISAB4
RISAB5 Used by ROM code only during cold boot
RISAB6
Security RISAF RISAF1
RISAF2
RISAF4 FSBL TF-A configures Cortex-A secure and encrypted memory regions
RISAF5
Security IAC IAC Fixed to TDCID
Trace & debug SERC SERC
Trace & Debug DBGMCU DBGMCU
Trace & Debug HDP HDP
Trace & Debug DDRPERFM DDRPERFM
Visual GPU GPU
Visual DSI Info.png DSI Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Visual LTDC Info.png LTDC Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature
Visual DCMI DCMI
Visual CSI CSI
Visual LVDS LVDS
Visual DCMIPP DCMIPP
Visual VENC VENC
Visual VDEC VDEC

4. References[edit | edit source]