Last edited one week ago

OpenSTLinux expansion packages

OpenSTLinux expansion packages can be combined with STM32 MPU OpenSTLinux distribution to enable the use of additional components for a specific feature such as AI-based computer vision, real-time Linux, or GNSS applications. X-LINUX components can be used as software add-ons only or may be combined with hardware shields, such as NFC expansion boards.
The X-LINUX part numbers are offered and maintained by ST, and I-LINUX part numbers are developed and maintained by partners and third parties.


OpenSTLinux_expansion_packages


Part number Supplier Supported devices Supported boards Latest supported ecosystem release[1]
X-LINUX-AI
to demonstrate AI-based computer vision applications
ST STM32MP13x lines More info.png
STM32MP15x lines More info.png
STM32MP25x lines More info.png
STM32MP1 series' boards More info green.png and STM32MP2 series' boards More info green.png ecosystem release v5.1.0 More info.png
X-LINUX-AWS
to enable the development of your IoT solution by bringing AWS IoT Greengrass[2] software in the Linux® kernel
ST STM32MP13x lines More info.png
STM32MP25x lines More info.png
STM32MP135F-DK More info green.png
STM32MP257F-EV1 More info green.png
ecosystem release v5.1.0 More info.png
X-LINUX-AZURE
to enable the development of your IoT solution by bringing Microsoft® Azure® IoT Edge[3] software in the Linux® kernel
ST STM32MP13x lines More info.png
STM32MP25x lines More info.png
STM32MP135F-DK More info green.png
STM32MP257F-EV1 More info green.png
ecosystem release v5.1.0 More info.png
X-LINUX-GNSS1
to demonstrate GNSS-based applications
ST STM32MP13x lines More info.png
STM32MP15x lines More info.png
STM32MP135F-DK More info green.png
STM32MP157F-DK2 More info green.png
ecosystem release v4.0.0
X-LINUX-IOT01E/A
to demonstrate SPIRIT1 and LSM6DSOX-based applications
ST STM32MP13x lines More info.png
STM32MP15x lines More info.png
STM32MP135F-DK More info green.png
STM32MP157F-DK2 More info green.png
ecosystem release v3.1.0
X-LINUX-ISP
to demonstrate a free-of-charge open-source software package providing Image Signal Processing (ISP) image quality software in the Linux® kernel
ST STM32MP25x lines More info.png STM32MP257F-EV1 More info green.png ecosystem release v5.1.0 More info.png
X-LINUX-MEMS1
to demonstrate MEMS sensor fusion-based applications
ST STM32MP13x lines More info.png
STM32MP15x lines More info.png
STM32MP135F-DK More info green.png
STM32MP157F-DK2 More info green.png
ecosystem release v4.1.0
X-LINUX-NFC5
to demonstrate RFAL-based NFC applications
ST STM32MP15x lines More info.png STM32MP157F-DK2 More info green.png ecosystem release v3.0.0
X-LINUX-NFC6
to demonstrate RFAL-based NFC applications
ST STM32MP15x lines More info.png STM32MP157F-DK2 More info green.png ecosystem release v3.0.0
X-LINUX-PREDMNT
to demonstrate predictive maintenance applications
ST STM32MP15x lines More info.png STM32MP157F-DK2 More info green.png ecosystem release v2.1.0
X-LINUX-QT
to demonstrate QT framework feature in the Linux® kernel
ST STM32MP257 line More info.png
STM32MP255 line More info.png
STM32MP257F-EV1 More info green.png ecosystem release v5.1.0 More info.png
X-LINUX-RT
to demonstrate the real-time (RT) feature in the Linux® kernel
ST STM32MP13x lines More info.png
STM32MP15x lines More info.png
STM32MP25x lines More info.png
STM32MP1 series' boards More info green.png and STM32MP257F-EV1 More info green.png ecosystem release v5.1.0 More info.png
X-LINUX-TSNSWCH
to demonstrate the real-time (RT) feature in the Linux® kernel
ST STM32MP257 line More info.png STM32MP257F-EV1 More info green.png ecosystem release unknown revision 6.0.0 Warning.png
  1. If the latest supported ecosystem release for the expansion package (e.g., ecosystem release v4.0.0 ) is not the latest delivered ecosystem release (ecosystem release v5.1.0 More info.png ), then adaptations might be needed for this expansion package be built and executed on this latest delivered release.
  2. AWS IoT Greengrass
  3. Microsoft® Azure® IoT Edge