Change propagation updates are pending (68 jobs estimated) and it is recommended to wait with modifications to a category until the process has been finalized to prevent intermediary interruptions or contradictory specifications.
OpenSTLinux expansion packages can be combined with STM32 MPU OpenSTLinux distribution to enable the use of additional components for a specific feature such as AI-based computer vision, real-time Linux, or GNSS applications. X-LINUX components can be used as software add-ons only or may be combined with hardware shields, such as NFC expansion boards.
The X-LINUX part numbers are offered and maintained by ST, and I-LINUX part numbers are developed and maintained by partners and third parties.
Part number | Supplier | Supported devices | Supported boards | Latest supported ecosystem release[1] |
---|---|---|---|---|
X-LINUX-AI to demonstrate AI-based computer vision applications |
ST | STM32MP13x lines STM32MP15x lines STM32MP25x lines |
STM32MP1 series' boards and STM32MP2 series' boards | ecosystem release v5.1.0 |
X-LINUX-AWS to enable the development of your IoT solution by bringing AWS IoT Greengrass[2] software in the Linux® kernel |
ST | STM32MP13x lines STM32MP25x lines |
STM32MP135F-DK STM32MP257F-EV1 |
ecosystem release v5.1.0 |
X-LINUX-AZURE to enable the development of your IoT solution by bringing Microsoft® Azure® IoT Edge[3] software in the Linux® kernel |
ST | STM32MP13x lines STM32MP25x lines |
STM32MP135F-DK STM32MP257F-EV1 |
ecosystem release v5.1.0 |
X-LINUX-GNSS1 to demonstrate GNSS-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v4.0.0 |
X-LINUX-IOT01E/A to demonstrate SPIRIT1 and LSM6DSOX-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v3.1.0 |
X-LINUX-ISP to demonstrate a free-of-charge open-source software package providing Image Signal Processing (ISP) image quality software in the Linux® kernel |
ST | STM32MP25x lines | STM32MP257F-EV1 | ecosystem release v5.1.0 |
X-LINUX-MEMS1 to demonstrate MEMS sensor fusion-based applications |
ST | STM32MP13x lines STM32MP15x lines |
STM32MP135F-DK STM32MP157F-DK2 |
ecosystem release v4.1.0 |
X-LINUX-NFC5 to demonstrate RFAL-based NFC applications |
ST | STM32MP15x lines | STM32MP157F-DK2 | ecosystem release v3.0.0 |
X-LINUX-NFC6 to demonstrate RFAL-based NFC applications |
ST | STM32MP15x lines | STM32MP157F-DK2 | ecosystem release v3.0.0 |
X-LINUX-PREDMNT to demonstrate predictive maintenance applications |
ST | STM32MP15x lines | STM32MP157F-DK2 | ecosystem release v2.1.0 |
X-LINUX-QT to demonstrate QT framework feature in the Linux® kernel |
ST | STM32MP257 line STM32MP255 line |
STM32MP257F-EV1 | ecosystem release v5.1.0 |
X-LINUX-RT to demonstrate the real-time (RT) feature in the Linux® kernel |
ST | STM32MP13x lines STM32MP15x lines STM32MP25x lines |
STM32MP1 series' boards and STM32MP257F-EV1 | ecosystem release v5.1.0 |
X-LINUX-TSNSWCH to demonstrate the real-time (RT) feature in the Linux® kernel |
ST | STM32MP257 line | STM32MP257F-EV1 | ecosystem release v6.0.0 |
- ↑ If the latest supported ecosystem release for the expansion package (e.g., ecosystem release v4.0.0 ) is not the latest delivered ecosystem release (ecosystem release v6.0.0 ), then adaptations might be needed for this expansion package be built and executed on this latest delivered release.
- ↑ AWS IoT Greengrass
- ↑ Microsoft® Azure® IoT Edge
Subcategories
This category has the following 8 subcategories, out of 8 total.