Last edited one week ago

Software distributions for STM32MP23 microprocessor

Applicable for STM32MP23x lines

Warning DB.png Important
To help you get started with STM32MP23x product lines evaluation, you can rely on the STM32MP257F-DK Discovery kit and applicable piece of STM32 MPU embedded software to run with STM32MP23 characteristics (peripherals, features, and performances).

The embedded software distributions[1] supported for the STM32MP235 line More info.png are listed below.

For the Linux® distribution, up to three software Packages are delivered:

  • the Starter Package (software image)
  • the Developer Package (SDK for cross-development, source code for the BSP of the distribution)
  • the Distribution Package (build framework on Linux host PC, source code for the whole distribution)
OpenSTLinux Distribution.png Yocto-based OpenSTLinux embedded software[2]
Linux Yocto starter package.png
Rely on the

Yocto-based OpenSTLinux Starter Package for STM32MP25 Discovery kits with characteristics relative to the STM32MP235 line More info.png

Linux Yocto developer package.png
Yocto-based OpenSTLinux Developer Package for STM32 MPUs
Linux Yocto distribution package.png
Yocto-based OpenSTLinux Distribution Package for STM32 MPUs
OpenSTLinux expansion packages can be applied on the top of the OpenSTLinux distribution to enable the use of additional components for a specific feature (such as AI-based computer vision).
  1. The STM32 MPU ecosystem release note details the latest delivered embedded software distributions
  2. The Which STM32MPU Embedded Software Package better suits your needs article provides hints for selecting the most appropriate Package.