Last edited one year ago

How to modify the panel backlight

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


First identify the backlight device linked to your panel, thanks to the sysfs:

 ls /sys/class/backlight
5a000000.dsi.0

In the above example, there is a single entry named "5a000000.dsi.0", which is replaced by "*" in the below command.


To adjust the panel backlight, enter the following command:

 echo 32 > /sys/class/backlight/*/brightness    # set the dsi panel backlight to the value 32

Note: Only values between 0 and max_brightness must be used.

To get the maximum panel backlight value, enter:

 cat /sys/class/backlight/*/max_brightness
255
Info white.png Information
If the max_brightness value is 1, the backlight can only be switched on and off. If the max_brightness value is above 1, the backlight has several levels on luminosity (pwm-based backlight for instance).

To get the actual panel backlight value, enter:

 cat /sys/class/backlight/*/actual_brightness
32


Use one of the following commands to quickly test the panel backlight:

 export bl=/sys/class/backlight/5a000000.dsi.0/brightness
 export max=/sys/class/backlight/5a000000.dsi.0/max_brightness

 # switch on/off test
 (while true; do echo 0 > $bl; sleep 0.5; echo $max > $bl; sleep 0.5; done)

 # slow 32-step tests (only for pwm-based backlights)
 (i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done)

 # fast 1-step test  (only for pwm-based backlights)
 (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done)
Info white.png Information
Be sure the panel is running (power on) before modifying its backlight.