1. Contents[edit source]
- 1. Article Purpose
- 2. Prerequisites
- 2.1 Hardware prerequisites
- 2.2 Software prerequisites
- 3 Hardware setup - connections explained
- 4 Software setup - customization to support X-NUCLEO-NFC05A1 expansion board
- 4.1 Kernel configuration
- 4.2 Kernel device tree configuration
- 4.2.1 Hardware / software interface
- 4.2.2 Kernel device tree configuration
- 4.3 Activate the new configuration in the STM32MP157C-DK2 board
- 4.4 Verify the new configuration on board
2. Article Purpose[edit source]
The purpose of this article is to explain how to integrate the NFC05A1 expansion board with STM32MP157C-DK2, Software will run on Linux on Cortex®-A7. NFC05A1 board is a NFC card reader expansion board based on ST25R3911B for STM32 and STM8 Nucleos.
3. Prerequisites[edit source]
All the dependencies as per the LINK should be installed
3.1. Hardware Prerequisites[edit source]
- STM32MP157C-DK2 Discovery Kit
- X-NUCLEO-NFC05A1
- 8 GB micro SD card to boot the STM32MP157C-DK2
- SD card reader OR
- LAN connectivity
3.2. Software prerequisites[edit source]
- Linux PC with Ubuntu 16.04 LTS installed
- Follow the instructions in the LINK to install all the software packages required for setting up the work env
4. Hardware setup - connections explained[edit source]