How to create secure project on STM32MP25 co-processor in STM32CubeIDE

Revision as of 10:33, 16 July 2024 by Registered User
Applicable for STM32MP25x lines


DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT-DRAFT


This article is a guideline to support secure project on Arm®-Cortex®-M33 core contained in the STM32MP25. The STM32MP25 support is provided in the release v1.16.0 of STM32CubeIDE.

It relies onto the project trusted-firmware-m, It can be used from a Windows or a Linux® workstation.

This article focus on how to build secure firmware - trusted firmware-m together with nonsecure firmware and debug them.

1. Prerequisites[edit source]

1.1. Hardware prerequisites[edit source]

  • STM32MP257F-EV1 Rev C,
  • Linux® console,
  • Ethernet (or Ethernet over USB) for connection of PC workstation to Linux® Arm®-Cortex®-A .

For more information, refer to Getting started/STM32MP2 boards/STM32MP257x-EV1/Let's start/Unpack the STM32MP257x-EV1 board.

1.2. Software prerequisites[edit source]

  • Install build environment and python dependencies for TF-M as described in How to configure TF-M prerequisites chapter.
  • Install python libraries needed by OP-TEE signature python script
 pip install pyelftools
 pip install pycryptodomex

2. Create CM33_trusted-firmware-m project[edit source]

CM33_trusted-firmware-m project need to be created uder CM33

Create MP2 project with TZ=1 using MP257F-EV1 board

2.1. MP2 stm32cube project with STM32CubeIDE with TZ=1[edit source]

MP2 stm32cube project is created from STM32CubeIDE using menu:


File > New STM32 Project...
Then, select Board selector MP2 MP257F-EV1... Next stm32cube Finish

Right clic on ProjectName_CM33 > Create a STM32 Cmake Project using existing Cmake sources

Then, set Import source using Directory... to the trusted-firmware-m selecting:

Note that trusted-firmware-m project is need to be cloned available from STM32Cube repository on local disk or from {{***************}.
Resulting project structure under CM33 contains three projects:

  • Device Tree, contain the tf-m device tree from STM32CubeMX,
  • MP2_CM33_NonSecure, HAL-based project addressing non-secure part of application,
  • MP2_CM33_trusted-firmware-m, pre-set STM32CubeIDE CMake project for TF-M, with link to sources: trusted-firmware-m pointing to cloned from :

ssh://gerrit.st.com:29418/mpu/oe/st/TF-M/trusted-firmware-m


CMake project using existing CMake sources
Link trusted-frimware-m to CMake project
  • STM32CubeIDE debug information for CMake project
MPS-3-preset-debug.png



2.2. MP2_CM33_trusted-firmware-m - final setup[edit source]

The only missing element is the access to trusted-firmware-m project source files.

As depicted here after, trusted-firmware-m link inside STM32CubeIDE project point to a path that has to be populated:

trusted-firmware-m link to source files

To populate it please follow Install Sources chapter from How to configure TF-M article.
Now you can refresh STM32CubeIDE project and view sources.

trusted-firmware-m sources from STM32CubeIDE


CMake trusted-firmware-m project need to defice CMake setting for:

  • STM32MP257F-EV1 board - CMake project usage setting
-DTFM_PLATFORM=stm/stm32mp257f_ev1 -DTFM_TOOLCHAIN_FILE=toolchain_GNUARM.cmake -DTFM_PROFILE=profile_medium -DCMAKE_BUILD_TYPE=debug -DDTS_BOARD=arm/stm/stm32mp257f-ev1-revB_s.dts -DDTS_EXT_DIR=/MP2_CM33/DeviceTree/MP2/tf-m -DNS=OFF
MPS-6-preset-board.png


3. Build[edit source]

Now it is possible to build MP2_CM33_trusted-firmware-m:

MPS-7-build-tfm.png
Warning white.png Warning
Process running STM32CubeIDE must define http and https proxy in order CMake command to successfully access network.

On Linux® workstation it is recommended to launch STM32CubeIDE from xterm with configured proxy environment.



Note that a post-build  :



Note that a post-build command is must be defined by used :
there are three options need to be updated on post build command :

  • workspace_loc workspace_loc:/MP2_CM33_trusted-firmware-m/trusted-firmware-m/config_default/bin/tfm_s.elf
  • Key /local/home/username/STM32CubeIDE/workspace_1.16.0/MP2/CA35/optee_os-3.19.0/optee-os-stm32mp-3.19.0-stm32mp-r2/keys/default.pem
  • python /local/home/username/STM32CubeIDE/workspace_1.16.0/MP2/CA35/optee_os-3.19.0/optee-os-stm32mp-3.19.0-stm32mp-r2/scripts/sign_rproc_fw.py


In order to get key and python script user must install OpenSTlinux sources plugin , SDK on disk , then import optee project and compile it's targets .

MPS-8-preset-board.png



arm-none-eabi-objcopy -S ${workspace_loc:/MP2_CM33_trusted-firmware-m/trusted-firmware-m/config_default/bin/tfm_s.elf}  tfm_s_stripped.elf; arm-none-eabi-objcopy -S ${BuildArtifactFileBaseName}.elf ${BuildArtifactFileBaseName}_stripped.elf; python /local/home/username/STM32CubeIDE/workspace_1.16.0/MP2/CA35/optee_os-3.19.0/optee-os-stm32mp-3.19.0-stm32mp-r2/scripts/sign_rproc_fw.py --in ${BuildArtifactFileBaseName}_stripped.elf --in tfm_s_stripped.elf --out ${BuildArtifactFileBaseName}_tfm_s_sign.bin --key /local/home/username/STM32CubeIDE/workspace_1.16.0/MP2/CA35/optee_os-3.19.0/optee-os-stm32mp-3.19.0-stm32mp-r2/keys/default.pem --plat-tlv BOOTADDR 0x80000000 --plat-tlv BOOTSEC 0x1



Note that a post-build command is used to generated the bin object from the two sub-project elf:

  • MP2_CM33_NonSecure_stripped.elf
  • MP2_CM33_trusted-firmware-m/trusted-firmware-m/config_default/bin/tfm_s.elf


MPS-9-preset-board.png


Select MP2_CM33_NonSecure project. This project has only one build configuration CA35TDCID_m33_ns_tfm_s_sign.
Build can be done using standard Eclipse "Build icon", it will generate MP2_CM33_NonSecure_tfm_s_sign.bin, visible after a project refresh.


4. Debugging[edit source]

4.1. Prerequisite to debug[edit source]

Target is to debug in "production mode".
STM32MP257F-EV1 must be up and running, and connected to the workstation via network & console.
SD-Card has been initialized with Starter Package version 24-06-26.
The Cortex-M33 Secure and non secure firmware image are encapsulated and signed. The resulting binary file "MP2_CM33_NonSecure_tfm_s_sign.bin" has to be loaded by OP-TEE. To check OP-TEE security capabilities of the board, execute following command, into Linux console:

cat /sys/class/remoteproc/remoteproc0/fw_format

that should return "TEE".

Before using production mode debug, proxy network must be adjusted, for that refer to How to set up proxy and P2P Ethernet connection with STM32CubeIDE.

Target Status on the bottom right must show a green light, refer to How_to_use_the_Target_Status_widget_in_STM32CubeIDE.

MPS-10-target-status.png

4.2. Loading .bin object[edit source]

The generated ".bin" object has to be downloaded to STM32MP257F-EV1 and loaded via remoteproc framework.
This is done thanks to a "Run Configuration" set in Production Mode.

In order to successfully load .bin we need to remove the fw_corte_m.sh


-root@stm32mp2:/usr/local/projects/MP2_CM33_NonSecure# ls -l
total 3
-rw-rw-r-- 1 root root  368 Mar  3 14:51 README
-rwxrwxr-x 1 root root  750 Mar  3 14:51 fw_cortex_m4.sh
drwxr-xr-x 3 root root 1024 Mar  3 14:50 lib
root@stm32mp2:/usr/local/projects/MP2_CM33_NonSecure# rm -rf *
root@stm32mp2:/usr/local/projects/MP2_CM33_NonSecure#


4.2.1. Run configuration setup[edit source]

Select MP2_CM33_NonSecure project and right click on Run As > Run Configurations...
Double click onSTM32 C/C++ Application to create a configuration.

  • In "main" tab:
  • "Workspace..." button allows to select ".bin" file
MPS-11-load-2.png


  • In "Debugger" tab:
  • "Load mode" should be "thru Linux core" (Production mode)
  • and for limitation reason, "GDB Connection Settings" should be "Connect to remote GDB server".
MPS-12-load-3.png


It is recommended to enrich the default "Run Configuration" name with for example (Run Cfg - Load). This is to distinguish from Debug Configuration.

4.2.2. Run[edit source]

Make run with this configuration in order transfer .bin and load it.
Here is the transfer pop up:

MPS-13-run-download.png

Open a console inside STM32CubeIDE in order to check that firmware has been loaded and is running on Arm®-Cortex®-M33:

  • cat /sys/class/remoteproc/remoteproc0/firmware
  • cat /sys/class/remoteproc/remoteproc0/state


MPS-14-run-check.png


In case of problem follow chapter How to trace and debug the framework from Linux remoteproc framework overview article.

4.3. Debugging Secure and Non Secure firmware[edit source]

For debugging those firmwares the debug configuration has to reference both secure and non secure ELF files.

4.3.1. Debug configuration setup[edit source]

Select MP2_CM33_NonSecure project and right click on Debug As > C/C++ STM32 Application
This menu creates a debug configuration for the selected project.

MPS-15-load-1.png

It is recommended to enrich the default "Debug Configuration" name with for example (Debug Cfg). This is to distinguish from Run Configuration.

In "Startup" tab

  • edit NonSecure elf and unset Download
MPS-16-dbg-cfg.png
  • Add TF-M elf definition with "Add" menu, and:
    • program path to: trusted-firmware-m/config_default/bin/tfm_s.elf,
    • disable "Download"
    • give "ARM.exidx" file offset "0x9c40". The file offset address is retrieved from tfm-s.elf:
  readelf -a tfm_s.elf | grep "Unwind section '.ARM.exidx' at offset"
Unwind section '.ARM.exidx' at offset 0x9c40 contains 1 entry: 
or
  objdump -hw ./config_default/bin/tfm_s.elf | grep ".ARM.exidx"
17 .ARM.exidx               00000008  80008c40  80008c40  00009c40  2**2  CONTENTS, ALLOC, LOAD, READONLY, DATA
MPS-17-dbg-cfg-tfm.png


Info white.png Information

A way to control entry point of debug session could be to add a debug loop. In picture hereafter a debug loop has been added at the begining of tfm_hal_platform_init() MP2_CM33_trusted-firmware-m/trusted-firmware-m/platform/ext/target/stm/common/stm32mp2/secure/tfm_hal_platform.c.

Debug session will start inside this debug loop and changing i variable to 0 it will be possible to step into tfm initialization code.

Debug loop inside TF-M init code

4.3.2. Debug[edit source]

Launching the debug configuration, it is recommended to select Switch to the Confirm Perspective Switch in order to enter "Debug Eclipse perspective". Then thanks to "Suspend" icon, the control of Arm®-Cortex®-M33 execution can be taken. First instructions are while loop onto a volatile variable, this allows to take control from code start.

Step into tf-m initialization code