Unpack the STM32MP257x-EV1 board

Applicable for STM32MP25x lines

Let's start Develop on Arm® Cortex®-A35
Unpack the board Populate the target and boot the image Execute basic commands Use the demo launcher

1. Overview[edit | edit source]

This first step explains how to unpack the STM32MP257x-EV1 Evaluation board and the additional equipment you need.

2. Required equipment[edit | edit source]

The following table lists the equipment required to start playing with your STM32MP257x-EV1 board.
Some of them are delivered within the STM32MP257x-EV1 Evaluation board. The others need to be purchased separately.

STM32MP257F-EV1 Evaluation board Full-featured board for STM32MP25 microprocessor devices Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software)
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is needed
Delivered
5V/3A power supply The power supply should be able to output 5V / 3A (15W) Not Delivered
USB Type-C cable Used to connect the STM32MP257F-EV1 Evaluation board to the PC
through the USB C (ST-LINK/V3)
Not delivered
USB Type-C to USB Type-A cable Used to connect the STM32MP257F-EV1 Evaluation board to an USB OTG device. Not delivered
Laptop A Linux PC (Ubuntu required version is given in PC prerequisites) Not delivered
Ethernet cable (optional) Used to connect the STM32MP257F-EV1 Evaluation board through ssh (can be done with USB OTG) Not delivered
LVDS screen LVDS WSVGA display B-LVDS7-WSVGA board (Finished good BLVDS7SVGA$PZ1) Not delivered
Camera Module 5-megapixel image sensor raw Bayer B-CAMS-IMX board (Finished good BCAMSIMX$MZ1) Not delivered

3. Board assembly[edit | edit source]

The STM32MP257x-EV1 Evaluation board packages (STM32MP257F-EV1 ), completed by the B-CAMS-IMX package, include the items listed below.

STM32MP257F-EV1 shown here (picture is not contractual)
Position Description
1 MB1936 main board
2 B-LVDS7-WSVGA 7” LVDS WSVGA display module with touch panel (optional)
3 LVDS display cable, provided with the B-LVDS7-WSVGA package (optional)
4 B-CAMS-IMX MB1854 MIPI CSI-2 camera board (optional)
5 Camera board FFC, provided with the B-CAMS-IMX package (optional)


B-LVDS7-WSVGA display and B-CAMS-IMX camera are available for purchase to complete the setup.

The complete set looks like this:

STM32MP257x-EV1 Evaluation board assembly
STM32MP257F-EV1 shown here (picture is not contractual)

3.1. Connecting the LVDS display to the board[edit | edit source]

Display board assembly (picture is not contractual)
  • Check the cable orientation shown above using the black mark and the white twisted pairs.
  • Find the LVDS ports on the STM32MP257x-EV1 Evaluation board (CN2) and the display (CN1). The LVDS display box contains one cable.
  • Insert the cable into each port as shown below:
Display board assembly (picture is not contractual)

3.2. Connecting the MB1854 camera board to the board[edit | edit source]

Camera board assembly (picture is not contractual)
  • Find the camera ports on the STM32MP257x-EV1 Evaluation board (CN4) and MB1854 (CN1). One FFC is provided in the camera box.
  • For each port:
    • Pull the black plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the black plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)

3.3. STM32MP257x-EV1 Evaluation board assembled[edit | edit source]


STM32MP257x-EV1 Evaluation board assembled
STM32MP257F-EV1 shown here (picture is not contractual)

4. Board connections[edit | edit source]

USB Power Delivery Type-C (Power or STLINK)ETHERNET 2/PHY ETH2 (Ethernet)2 x USB type A (host) (such as a mouse or keyboard USB driver)USB2.0 DRD Type-C  (programmable through CubeProgrammer)microSD<sup>™</sup> card slotMB1936 5V/3A power supply jack (Power)RESET button
STM32MP257x-EV1 Evaluation board connections

STM32MP257F-EV1 shown here (picture is not contractual)
Warning
If the supply is provided via the USB Power Delivery Type-C (1), to have the possibility to use ST-Link or the consoles, the USB Power Delivery Type-C (1) must be connected to a PC with USB Type-C/Type-C cable. The USB Type-C on the PC must be a USB Power Delivery Type-C.
Information
Via ST-LINK, it is possible to have access to 2 consoles: one for Cortex-M and one for Cortex-A.


  • Connect your laptop to the board ST-LINK/V3 port (1) through the USB Type-C cable.
  • Connect your laptop to the board USB Type-C™ OTG port (4) through the USB Type-C to USB Type-A.
  • Optionally connect your Ethernet network to the board Ethernet port (2) through the Ethernet cable.
  • JP4 must be set as defined in picture, below, to activate the board supply through USB power typeC (1)
MB1936 board supplied via USB Power TypeC CN21 (picture is not contractual)


Information
The LED located on the left side of the board should be green when the power is on.