Populate the target and boot the image

Applicable for STM32MP15x lines

Let's start Develop on Arm® Cortex®-A7
Unpack the board Populate the target and boot the image Execute basic commands Use the demo launcher


1. Overview[edit | edit source]

This step explains how to get the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.


2. Open a terminal[edit | edit source]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace
cd $HOME/STM32MPU_workspace

3. Check the host computer Internet access[edit | edit source]

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4. Install the tools[edit | edit source]

4.1. STM32CubeProgrammer[edit | edit source]

  • Create your "STM32MPU tools" directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
cd $HOME/STM32MPU_workspace/tmp


4.2. Installing the STM32CubeProgrammer tool[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.23.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.23.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .


4.3. Preparing the USB serial link for flashing[edit | edit source]

It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.

Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.

  • For Linux host PC or Windows host PC with VMWare:

The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:

sudo apt-get install libusb-1.0-0

To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:

cd <your STM32CubeProgrammer install directory>/Drivers/rules 
sudo cp *.* /etc/udev/rules.d/
  • For Windows host PC:

Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.

In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.

To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.


5. Test[edit | edit source]

  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

6. Download the image[edit | edit source]

Warning
Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
  • The STM32MP1 image (binaries) is delivered through one tarball file named
    • FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz for STM32MP135x-DK , STM32MP157x-DKx and STM32MP157x-EV1

  • Download and install the STM32MP1 image (binaries):

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP1 Starter Package image - STM32MP1-Ecosystem-v6.2.1 release
Download
  • Go on st.com to download the STM32MP1 Starter Package image, FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz file.
Installation
cd <working directory path>/Starter-Package
  • Download the tarball file in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
tar xvf FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz
Release note

Details of the content of this software package are available in the associated STM32 MPU OpenSTLinux release note.
If you are interested in older releases, please have a look into the section Archives

  • The binaries and the Flash layout files are in the <Starter Package installation directory>/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp1/ directory. The most important ones are:
stm32mp1
├── arm-trusted-firmware                                                     TF-A binaries
│   ├── bl2                                                                  TF-A binary for FIP binaries creation
│   │   ├── <board name>-bl2-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── debug                                                                Debug binaries for TF-A
│   │   ├── debug-tf-a-<board name>-<boot chain>-<storage>.stm32             Debug file for FSBL
│   │   ├── tf-a-bl2-<soc name>-<board name>-<boot chain>-<storage>.elf      Debug symbol file for TF-A
│   │   └── [...]
│   ├── fwconfig                                                             TF-A device tree for FIP binaries creation
│   │   ├── <board name>-fwconfig-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── metadata.bin                                                         Meta data binary for METADATA partition for the supported boards
│   ├── tf-a-<board name>-<boot chain>-<storage>.stm32                       TF-A binary for FSBL partition
│   └── [...]
├── fip                                                                      FIP binaries for FIP partitions and supported boot chains
│   ├── fip-<board name>-<boot chain>-<storage>.bin                          FIP binary for FIP partition
│   ├── fip-<board name>-<boot chain>-<storage>.txt                          Configuration file for FIP binary content
│   └── [...]
├── flashlayout_st-image-weston                                              Flash layout files (description of the partitions) for the supported boot chains
│   ├── extensible                                                           Recommended setup for package repository service: microSD card boot device without userfs partition to extend rootfs partition till microSD card end
│   │   ├── FlashLayout_sdcard_<board name>-extensible.tsv
│   │   └── [...]
│   ├── fastboot
│   │   ├── FlashLayout_<boot device>_<board name>-fastboot.tsv
│   │   └── [...]
│   ├── fastboot-opteemin
│   │   ├── FlashLayout_<boot device>_<board name>-fastboot-opteemin.tsv
│   │   └── [...]
│   ├── optee
│   │   ├── FlashLayout_<boot device>_<board name>-optee.tsv
│   │   └── [...]
│   └── opteemin
│       ├── FlashLayout_<boot device>_<board name>-opteemin.tsv
│       └── [...]
├── Kernel                                                                     Debug binaries for Linux kernel
│   ├── config-6.6.129                                                         Reference config file for Linux kernel
│   └── vmlinux                                                                Image of the Linux kernel
├── optee                                                                      OPTEE-OS binaries
│   ├── debug                                                                  Debug binaries for OPTEE-OS
│   │   ├── dtb
│   │   │   ├── <board name>-<boot chain>.dtb                                  OPTEE-OS device tree
│   │   │   ├── <board name>-<boot chain>-programmer.dtb                       OPTEE-OS device tree or usb/serial}
│   │   │   └── [...]
│   │   ├── tee-<board name>-<boot chain>.elf                                  Debug symbol file for OPTEE-OS
│   │   ├── tee-<board name>-<boot chain>-programmer.elf                       Debug symbol file for OPTEE-OS configured for usb/serial
│   │   └── [...]
│   ├── tee-header_v2-<board name>-<boot chain>.bin                            OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-header_v2-<board name>-<boot chain>-programmer.bin                 OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pageable_v2-<board name>-<boot chain>.bin                          OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pageable_v2-<board name>-<boot chain>-programmer.bin               OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pager_v2-<board name>-<boot chain>.bin                             OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pager_v2-<board name>-<boot chain>-programmer.bin                  OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   └── [...]
├── scripts
│   └── create_sdcard_from_flashlayout.sh
├── u-boot                                                                     U-BOOT binaries
│   ├── debug                                                                  Debug binaries for U-BOOT
│   │   ├── u-boot-<soc name>-<u-boot config>.elf                              Debug symbol file for U-BOOT
│   │   └── [...]
│   ├── configuration-<soc name>-<u-boot config>_defconfig                     Reference configuration file for U-Boot
│   ├── u-boot-nodtb-<soc name>-<u-boot config>.bin                            U-BOOT binary for FIP binaries creation
│   ├── u-boot-<board name>-<u-boot config>.dtb                                U-BOOT device tree for FIP binaries creation
│   └── [...]
├── st-image-weston-openstlinux-weston-stm32mp1.splitted-bootfs.ext4           Binary for bootfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp1.splitted-userfs.ext4           Binary for userfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp1.splitted-vendorfs.ext4         Binary for vendorfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp1.splitted-rootfs.ext4           Binary for rootfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.license
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs-license_content.html    License summary for all packages needed to feed all partitions
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.spdx.tar.zst
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs_nand_4_256_1024_multivolumde_splitted.ubi Binary for ubi partition on NAND device
└── [...]

Description:

<board name>:
* stm32mp135f-dk
* stm32mp157a-dk1, stm32mp157a-ev1, stm32mp157c-dk2, stm32mp157c-ed1, stm32mp157c-ev1, stm32mp157d-dk1, stm32mp157d-ev1, ,stm32mp157f-dk2, stm32mp157f-ed1, stm32mp157f-ev1
<soc name>:
* stm32mp13
* stm32mp15
<boot chain>:
* fastboot                  optee boot chain for flashing via fastboot
* fastboot-opteemin         opteemin boot chain for flashing via fastboot
* optee                     optee boot chain
* opteemin                  opteemin boot chain
<boot device>:
* emmc                      Boot via emmc storage
* nor-sdcard                Boot via nor storage for first stage (fsbl, fip) and files system are located on sdcard
* nand-4-256-1024-sdcard    Boot via nand storage for first stage (fsbl, fip) and files system are located on sdcard
* sdcard                    Boot via sdcard storage
* sdcard-EFI                Boot via sdcard storage and bootfs is configurated on EFI
<storage>:
* emmc                      emmc storage
* nor                       nor storage
* nand                      nand storage
* programmer-uart           storage programmation via UART
* programmer-usb            storage programmation via USB
* sdcard                    sdcard storage
<u-boot config>:
* default
* fastboot-emmc             Fastboot config enabled with MMC_DEV Id for emmc
* fastboot-sdcard           Fastboot config enabled with MMC_DEV Id for sdcard
* programmer                Programmer config enabled



7. Populate the SD card[edit | edit source]

  • Set the boot switches (located on the MB1263) to the OFF position:
boot switches position to flash the board
  • Connect the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.
  • Power up the board.
  • Press the reset button to reset the board.
  • Launch STM32CubeProgrammer to get the GUI :
STM32CubeProgrammer GUI


  • On the right of the window, select USB (instead of STLINK, set by default) from the connection picklist, and click the "Refresh" button. The serial number is displayed if the USB has been detected.
Select USB for connection with board
  • Click "Connect"
  • Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157x-ev1-optee.tsv" in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Starter-Package/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp1/flashlayout_st-image-weston/optee")
  • Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
open .tsv optee and fill Binaries Path for EV1
  • Click "Download" to launch the flashing process.
  • A progress bar indicates the process progress until a completion pop-up message is displayed.

8. Boot the board[edit | edit source]

  • Set the boot switches (located on the MB1263) to the ON position.
boot switches position to boot the board
  • Power on the board.
  • Press the "Reset" button to reset the board.
  • After few seconds, the board starts and automatically goes through the following screens:
Warning
The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards.
U-Boot splash screen
Linux splash screen
Weston desktop
GTK demo launcher