Applicable for STM32MP25x lines

Develop on Arm® Cortex®-M33 What's next
Install the IDE Install STM32CubeMP2 package Modify, rebuild and reload the firmware for A35-TD flavor
Modify, rebuild and reload the firmware for M33-TD flavor



1. Overview[edit | edit source]

This stage explains how to install the STM32CubeMP2 package.

2. Install STM32CubeMP2 package[edit | edit source]

  • The STM32CubeMP2 Package is delivered through an archive file named stm32cubemp2-v1-3-1.zip.

  • Download and install the STM32CubeMP2 Package

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32CubeMP2 Package - v1.3.1
Download
  • Go on st.com to download the stm32cubemp2-v1-3-1.zip file.
Installation
cd <working directory path>/Developer-Package
  • Download the archive file in this directory
  • Uncompress the archive file to get the STM32CubeMP2 Package:
unzip stm32cubemp2-v1-3-1.zip
Release note

Details about the content of the STM32CubeMP2Package are available in the STM32CubeMP2/Release_Notes.html file.

If you are interested in older releases, please have a look into the section Archives.

  • The STM32CubeMP2 Package installation directory is in the <Developer Package installation directory> directory, and is named STM32Cube_FW_MP2_V1.3.X [X:0,1]:
STM32Cube_FW_MP2_V1.3.X [X:0,1]			STM32CubeMP2 Package: details in STM32CubeMP2 Package content article
├── _htmresc
│   └── [...]
├── Drivers
│   ├── BSP				BSP drivers for the supported STM32MP2 boards
│   │   └── [...]
│   ├── CMSIS
│   │   └── [...]
│   └── STM32MP2xx_HAL_Driver		HAL drivers for the supported STM32MP2 devices
│       └── [...]
├── Middlewares
│   └── [...]
├── Projects
│   ├── _htmresc
│   │   └── [...]
│   ├── STM32MP215F-DK			Set of examples and applications → STM32MP21 Discovery boards
│   │   └── [...]
│   ├── STM32MP235F-DK			Set of examples and applications → STM32MP23 Discovery boards
│   │   └── [...]
│   ├── STM32MP257F-DK			Set of examples and applications → STM32MP25 Discovery boards
│   │   └── [...]
│   ├── STM32MP257F-EV1			Set of examples and applications → STM32MP25 Evaluation boards
│   │   └── [...]
│   ├── Release_Notes.html
│   └── STM32CubeProjectsList.html	List of examples and applications for STM32CubeMP2 Package
├── Utilities
│   └── [...]
├── CODE_OF_CONDUCT.md
├── CONTRIBUTING.md
├── License.md
├── package.xml
├── Package_license.html
├── Package_license.md
├── README.md
├── Release_Notes.html			Release note for STM32CubeMP2 Package
├── sbom_cdx.json
└── SECURITY.md
 
Warning
Due to compatibility issue, once the STM32CubeMP2 Package v1.3.1 is extracted, the external dt provided in <STM32CubeMP2-1.3.1>/Utilities/dt-stm32mp needs to be replaced with the cmake version used in STM32CubeIDE v2.2.0. Please replace the dt-stm32mp folder by the one provided from github here: https://github.com/STMicroelectronics/dt-stm32mp/archive/refs/tags/v6-stm32mp-r3.1.zip, then rename the extracted folder dt-stm32mp-6-stm32mp-r3.1 to dt-stm32mp