1. Overview[edit | edit source]
This stage explains how to create, build and execute a simple C code application using the freshly installed SDK.
2. Code[edit | edit source]
- Create a directory that will host your source codes
mkdir $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/stm32mp1-openstlinux-26.02.18 mkdir $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/stm32mp1-openstlinux-26.02.18/sources
- Create a directory for your user space example
mkdir $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/stm32mp1-openstlinux-26.02.18/sources/gtk_hello_world_example cd $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/stm32mp1-openstlinux-26.02.18/sources/gtk_hello_world_example
- Create the source code file for your user space example: gtk_hello_world.c
#include <gtk/gtk.h>
static void
print_hello (GtkWidget *widget,
gpointer data)
{
g_print ("Hello World\n");
}
static void
activate (GtkApplication *app,
gpointer user_data)
{
GtkWidget *window;
GtkWidget *button;
GtkWidget *button_box;
window = gtk_application_window_new (app);
gtk_window_set_title (GTK_WINDOW (window), "Window");
gtk_window_set_default_size (GTK_WINDOW (window), 200, 200);
button_box = gtk_button_box_new (GTK_ORIENTATION_HORIZONTAL);
gtk_container_add (GTK_CONTAINER (window), button_box);
button = gtk_button_new_with_label ("Hello World");
g_signal_connect (button, "clicked", G_CALLBACK (print_hello), NULL);
g_signal_connect_swapped (button, "clicked", G_CALLBACK (gtk_widget_destroy), window);
gtk_container_add (GTK_CONTAINER (button_box), button);
gtk_widget_show_all (window);
}
int
main (int argc,
char **argv)
{
GtkApplication *app;
int status;
app = gtk_application_new ("org.gtk.example", G_APPLICATION_DEFAULT_FLAGS);
g_signal_connect (app, "activate", G_CALLBACK (activate), NULL);
status = g_application_run (G_APPLICATION (app), argc, argv);
g_object_unref (app);
return status;
}
3. Build[edit | edit source]
- Create the makefile for your user space example: Makefile
| All the indentations in a makefile are tabulations |
PROG = gtk_hello_world SRCS = gtk_hello_world.c CLEANFILES = $(PROG) # Add / change option in CFLAGS and LDFLAGS CFLAGS += -Wall $(shell pkg-config --cflags gtk+-3.0) LDFLAGS += $(shell pkg-config --libs gtk+-3.0) all: $(PROG) $(PROG): $(SRCS) $(CC) -o $@ $^ $(CFLAGS) $(LDFLAGS) clean: rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS))
- Cross-compile the project
make
4. Deploy and execute[edit | edit source]
- Push this binary onto the board (Ethernet connection needed)
scp gtk_hello_world root@<board ip address>:/usr/local
- Execute your user space example by using the user "weston"
cd /usr/local/ su -l weston -c "/usr/local/gtk_hello_world"
- A GTK window is displayed
- Click the "Hello world" button to close the window. Hello world is displayed on the console:
Hello world