Unpack the STM32MP215x-DK board

Applicable for STM32MP21x lines

Let's start Develop on Arm® Cortex®-A35
Unpack the board Populate the target and boot the image Execute basic commands Use the demo launcher

1. Overview[edit | edit source]

This first step explains how to unpack the STM32MP215F-DK Discovery kit and the additional equipment you need.

2. Required equipment[edit | edit source]

The following table lists the equipment required to start playing with your STM32MP215x-DK board.
Some of them are delivered within the STM32MP215F-DK Discovery kit . The others need to be purchased separately.

STM32MP215F-DK Discovery kit Full-featured board for STM32MP21 microprocessor devices Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software)
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is needed
Not delivered
USB to TTL serial cables Used to connect the STM32MP215F-DK Discovery kit to the PC
through the VCPA35 and VCPM33 connector (ST-LINK/V3)
Not delivered
Laptop A Linux PC running Ubuntu (Ubuntu required version is given in PC prerequisites) with a USB Type-C port with power delivery is required. Not delivered
USB Type-C / Type-C cable Used to connect the board to the laptop, for power supply and data path Not delivered
Ethernet cable (optional) Used to connect the STM32MP215F-DK Discovery kit through ssh (can be done with USB OTG) Not delivered
Parallel RGB screen RK043FN78H-CT661C 4.3" TFT 480*272 pixels with LED Backlight and capacitive touch panel Not delivered
Camera Module 5-megapixel image sensor raw Bayer B-CAMS-IMX board Not delivered

3. Board assembly[edit | edit source]

The STM32MP215x-DKx Discovery kit package (STM32MP215F-DK ) contains only the MB2059 motherboard.

STM32MP215F-DK Discovery kit front side (picture not contractual)
Information
Display and camera are available for purchase to complete this basic setup.

The complete set contains:

STM32MP215F-DK and additional accessories kits shown here (picture is not contractual)
Position Description
1 MB2059 main board
2 MicroSD card
3 4.3" TFT 480*272 pixels with LED Backlight and capacitive touch panel RK043FN78H-CT661C (optional)
4 Camera board FFC (provided with the B-CAMS-IMX package) (optional)
5 MB1854 camera board provided with the B-CAMS-IMX package (optional)


STM32MP215F-DK Discovery kit assembly (picture is not contractual)


3.1. Connecting the display to the board (optional)[edit | edit source]

  • Find the DISPLAY connector (CN8) on the top side of the MB2059 main board
  • Flip the connector’s latch up
Display board assembly - step 1 (picture is not contractual)
Display board assembly - step 2 (picture is not contractual)


  • Insert the LCD’s cable with the exposed contacts facing down
Display board assembly - step 3 (picture is not contractual)


  • Flip the connector’s latch down to secure the cable
Display board assembly - step 4 (picture is not contractual)


3.2. Connecting the MB1854 camera board to the board (optional)[edit | edit source]

Camera board assembly (picture is not contractual)


  • Find the camera ports on the STM32MP215x-DK Discovery kit (CN4) (#1 in the image above) and MB1854 (CN1) (#2 in the image above). The camera box contains one FFC.
  • For each port:
    • Pull the plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)


3.3. Connecting USB to TTL serial cables[edit | edit source]

To have 2 consoles on your workstation , one for Cortex-M33 and one for Cortex-A35, 2 "USB to TTL serial cables" are needed.

(picture is not contractual)



3.4. STM32MP215x-DK Discovery kit assembled and connected[edit | edit source]

The picture below presents the recommended board connections for getting started with the STM32MP215x-DKx Discovery kits

Warning
To start the board, it is recommended to go through the corresponding Starter Package article first.

As shown in the board overview, other connectors are available for this board (for example, the GPIO expansion connector).


MB2059 motherboard: STM32MP215F 14x14MicroSD<sup>™</sup> card slotReset buttonEthernet (network)USB Power Delivery Type-C (Power) and USB3.0 DRD/OTG Type-C (programmable through STM32CubeProgrammer)CSI cameraLTDC displayUSB to TTL serial cables
STM32MP215x-DKx Discovery kit connections (picture is not contractual)





3.5. Connections details[edit | edit source]

Main board MB2059, revision B: part of the STM32MP215F-DK Discovery kit .

STM32MP215x-DK Discovery kit front side STM32MP215F-DK shown here (picture is not contractual)


Warning
USART2-RX and USART2-TX are wired to ST-Link connector (CN5) and VCPA35 connector (CN2). ST-LINK and Cortex-A35 Linux console can not used simultaneously via those both connectors.
  • To allow the Cortex-A35 Linux console : The VCPA35 connector (CN2) needs to be plugged and ST-Link connector (CN5) to be unplugged
  • To allow debugging over ST-LINK and Cortex-A35 Linux console : CN5 needs to be plugged and CN2 to be unplugged. In such case, the Cortex-A35 Linux console is available through ST-LINK.


  • Connect the laptop to the board USB Power Delivery Type-C (CN10) for power and programmation through STM32CubeProgrammer.
  • Connect your laptop to the board on CN1 and CN2 through the USB to TTL serial cables.
  • Optionally connect your Ethernet network to the board Ethernet port CN11 through the Ethernet cable.


Information
The LED located on the middle of the board, LD1, should be yellow when the power is on.