Modify, rebuild and reload the Linux® kernel

Applicable for STM32MP23x lines, STM32MP25x lines

Develop on Arm® Cortex®-A35 Develop on Arm® Cortex®-M33
Install the SDK Create a simple hello-world application Modify, rebuild and reload the Linux® kernel


1. Overview[edit | edit source]

This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then you will execute step by step procedures to modify, rebuild and reload the Linux® kernel.

2. Download OpenSTLinux BSP that includes the Linux® kernel source code[edit | edit source]

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

  • The OpenSTLinux BSP package is delivered through a tarball file named SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz applicable for all STM32 microprocessor series.

  • Download and install the STM32MPU OpenSTLinux BSP package.
STM32MPU Developer Package - STM32MPU ecosystem v6.2.1 release
Download

MPx-DEV-SRC).

Installation
cd <working directory path>/Developer-Package
tar xvf SOURCES-stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz
Release note

Details about the content of the OpenSTLinux BSP package are available in the associated STM32 MPU OpenSTLinux release note.

For information on older releases, go to Archives.


cd stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/sources/ostl-linux/linux-stm32mp-6.6.129-stm32mp-r3.1-r0

3. Prepare the Linux® kernel source code[edit | edit source]

Extract the Linux® kernel source

tar xvf linux-6.6.129.tar.xz

Apply ST patches

cd linux-6.6.129
for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
  • Configure build directory
export OUTPUT_BUILD_DIR=$PWD/../build
mkdir -p ${OUTPUT_BUILD_DIR}
  • Apply fragments
make O="${OUTPUT_BUILD_DIR}" defconfig fragment*.config
for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O ${OUTPUT_BUILD_DIR} ${OUTPUT_BUILD_DIR}/.config $f; done
(yes '' || true) |  make oldconfig O="${OUTPUT_BUILD_DIR}"

4. Build the Linux® kernel source code for the first time[edit | edit source]

Information
Building the kernel for the first time can take several minutes.


Build kernel images (Image.gz and vmlinux) and device tree (dtbs):

make Image.gz vmlinux dtbs O="${OUTPUT_BUILD_DIR}"
export IMAGE_KERNEL="Image.gz"


  • Build kernel module
make modules O="${OUTPUT_BUILD_DIR}"
  • Generate output build artifacts
make INSTALL_MOD_PATH="${OUTPUT_BUILD_DIR}/install_artifact" modules_install O="${OUTPUT_BUILD_DIR}"
mkdir -p ${OUTPUT_BUILD_DIR}/install_artifact/boot/
cp ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/${IMAGE_KERNEL} ${OUTPUT_BUILD_DIR}/install_artifact/boot/
find ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/dts/ -name 'st*.dtb' -exec cp '{}' ${OUTPUT_BUILD_DIR}/install_artifact/boot/ \;

5. Deploy the Linux® kernel on the board[edit | edit source]

5.1. Push the Linux® kernel and the devicetree onto the board[edit | edit source]

cd ${OUTPUT_BUILD_DIR}/install_artifact
scp -r boot/* root@<ip of board>:/boot/

5.2. Push the kernel modules onto the board[edit | edit source]

  • Remove the link created inside the install_artifact/lib/modules/<kernel version> directory
rm lib/modules/6.6.129/build
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
find . -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
  • Copy kernel modules
scp -r lib/modules/* root@<ip of board>:/lib/modules
  • Using the Linux® console, regenerate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
/sbin/depmod -a
  • Synchronize data on disk with memory
sync

5.3. Reboot the board[edit | edit source]

reboot

6. Modify a built-in Linux® kernel device driver[edit | edit source]

This simple example adds unconditional log information when the display driver is probed.

  • Using the Linux® console, check that there is no log information when the display driver is probed
dmesg | grep -i modified

  • Go to the Linux® kernel source directory
cd $HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/sources/ostl-linux/linux-stm32mp-6.6.129-stm32mp-r3.1-r0/linux-6.6.129

  • Edit the ./drivers/pinctrl/stm32/pinctrl-stm32.c source file
  • Add a log information in the stm32_pctl_probe function as follows
int stm32_pctl_probe(struct platform_device *pdev)
{
   [...]
   dev_info(dev, "Pinctrl STM32 initialized\n");
   dev_info(dev, "I modified a linux kernel device driver\n");
   [...]
}
  • Save the file
  • Rebuild the Linux® kernel
make Image.gz O="${OUTPUT_BUILD_DIR}"
  • Update the Linux kernel image into board
scp ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/Image.gz root@<board ip address>:/boot


  • Reboot the board
reboot 
  • Check that log information is now present when the display driver is probed
dmesg | grep -i modified
[    2.309171] stm32mpxxx-pinctrl soc@0:pinctrl@44240000: I modified a linux ker
nel device driver                                                               
[    2.331734] stm32mpxxx-pinctrl soc@0:pinctrl@46200000: I modified a linux ker
nel device driver