Applicable for STM32MP23x lines, STM32MP25x lines

Develop on Arm® Cortex®-M33 What's next
Install the IDE Install STM32CubeMP2 package Modify, rebuild and reload the firmware for A35-TD flavor
Modify, rebuild and reload the firmware for M33-TD flavor


1. Overview[edit | edit source]

This stage explains how to install STM32CubeIDE to develop on STM32MPU Arm® Cortex®-M coprocessors.

2. Install STM32CubeIDE[edit | edit source]

STM32 MPU support, inside STM32CubeIDE, is available on Linux® and Windows® host PCs, but it is NOT on macOS®.

STM32CubeIDE for Linux® host PC STM32CubeIDE for Windows® host PC
Download

Version v2.2.0

  • Download the preferred all-in-one Linux installer from st.com
    • Generic Linux Installer - STM32CubeIDE-Lnx
    • RPM Linux Installer - STM32CubeIDE-RPM
    • Debian Linux Installer - STM32CubeIDE-DEB

Version v2.2.0

  • Download the all-in-one Windows installer from st.com
    • Windows Installer - STM32CubeIDE-Win
Installation guide
  • Refer to STM32CubeIDE installation guide (UM2563) available on st.com.
User manual
  • When the installation is completed, see additional information about STM32CubeIDE in st.com:
    • STM32CubeIDE quick start guide (UM2553)
Detailed release note
  • Details about the content of this tool version are available in the STM32CubeIDE release v2.2.0 release note from st.com
Restrictions Main restrictions are identified in this chapter
  • STM32CubeIDE errata( This page is hosted in the STM32 MCU wiki. Selecting the link opens a new tab. Be aware that visiting this page leaves the STM32 MPU wiki)

Minor releases may be available from the update site. Check chapter 10 in (UM2609) for more information on how to update STM32CubeIDE.