Populate the target and boot the image

Applicable for STM32MP21x lines

Let's start Develop on Arm® Cortex®-A35
Unpack the board Populate the target and boot the image Execute basic commands Use the demo launcher


1. Overview[edit | edit source]

This step explains how to get the Starter Package, then install and boot the STM32MP21 Discovery kit boards with the Starter Package.


2. Open a terminal[edit | edit source]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace
cd $HOME/STM32MPU_workspace

3. Check the host computer Internet access[edit | edit source]

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4. Install the tools[edit | edit source]

4.1. STM32CubeProgrammer[edit | edit source]

  • Create your "STM32MPU tools" directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
cd $HOME/STM32MPU_workspace/tmp


4.2. Installing the STM32CubeProgrammer tool[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.23.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.23.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .


4.3. Preparing the USB serial link for flashing[edit | edit source]

It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.

Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.

  • For Linux host PC or Windows host PC with VMWare:

The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:

sudo apt-get install libusb-1.0-0

To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:

cd <your STM32CubeProgrammer install directory>/Drivers/rules 
sudo cp *.* /etc/udev/rules.d/
  • For Windows host PC:

Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.

In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.

To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.


5. Test[edit | edit source]

  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

6. Download the image[edit | edit source]

For A35-TD flavor

Warning
Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
  • The STM32MP2 image (binaries) is delivered through one tarball file named FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz applicable to STM32MP215F-DK , STM32MP257F-DK for STM32MP23x lines evaluation , STM32MP257x-DK and STM32MP257x-EV1

  • Download and install the STM32MP2 image (binaries):

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP2 Starter Package image - STM32MP2-Ecosystem-v6.2.1 release for A35-TD flavor
Download
Warning
Check first here, if a minor release based on this ecosystem release v6.2.1 is already published.
If a minor release exists, replace the name of the STM32MP2 Starter Package file, used below, and in other wiki articles, by the name of file delivered with the minor release.

Go on st.com to download the STM32MP2 Starter Package image, FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz file.

Installation
cd <working directory path>/Starter-Package
  • Download the tarball file in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
tar xvf FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz
Release note

Details of the content of this software package are available in the associated STM32 MPU OpenSTLinux release note.
If you are interested in older releases (STM32MP2-Ecosystem-v6.0.0, STM32MP2-Ecosystem-v6.1.0 and STM32MP2-Ecosystem-v6.2.0), please have a look into the section Archives

  • The binaries and the Flash layout files are in the <Starter Package installation directory>/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp2/ directory. The most important ones are:
stm32mp2
├── arm-trusted-firmware                                                               TF-A binaries for FSBL partitions and supported boot chains
│   ├── bl31                                                                           TF-A BL31 binary for FIP binaries creation
│   │   ├── debug                                                                      Debug binaries for BL31
│   │   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.elf      Debug symbol file for TF-A BL31
│   │   │   └── [...]
│   │   ├── <board name>-<hardware security>-<boot chain>-<storage>.dtb                TF-A BL31 device tree for FIP binaries creation
│   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.bin      TF-A BL31 binary for FIP binaries creation
│   │   └── [...]
│   ├── ddr                                                                            Trained DDR binary for FIP binaries creation
│   │   ├── ddr_pmu-<board name>-<hardware security>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── debug                                                                          Debug binaries for TF-A
│   │   ├── debug-tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32   Debug file for FSBL
│   │   ├── tf-a-bl2-<soc name>-<boot chain>-<storage>.elf                             Debug symbol file for TF-A
│   │   └── [...]
│   ├── fwconfig                                                                       TF-A device tree for FIP binaries creation
│   │   ├── <board name>-<hardware security>-fwconfig-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── metadata.bin                                                                   Meta data binary for METADATA partition for the supported boards
│   ├── tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32             TF-A binary for FSBL partition
│   └── [...]
├── arm-trusted-firmware-m                                                             TF-M binaries
│   ├── debug                                                                          Debug binaries for TF-M
│   │   ├── tfm-<board name>-<hardware security>_s.elf                                 Debug symbol file for TF-M
│   │   └── [...]
│   ├── tfm-<board name>-<hardware security>_s.bin                                    TF-M binary for m33 firmware as copro
│   └── [...]
├── fip                                                                                FIP binaries for FIP partitions and supported boot chains
│   ├── fip-<board name>-<hardware security>-ddr-<boot chain>-<storage>.bin            FIP binary for FIP DDR partition
│   ├── fip-<board name>-<hardware security>-<boot chain>-<storage>.bin                FIP binary for FIP partition
│   └── [...]
├── flashlayout_st-image-weston                                                        Flash layout files (description of the partitions) for the supported boot chains on supported boot devices and boards
│   ├── [...]
│   ├── extensible                                                                     Flash layout files for microSD card boot device with no userfs partition but a rootfs partition extended to microSD card size
│   │   ├── FlashLayout_sdcard_<board name>-<hardware security>-extensible.tsv         (recommended setup for package repository service) microSD card boot device with rootfs partition extended to microSD card size
│   │   └── [...]
│   ├── fastboot                                                                       Flash layout files for flashing via fastboot with optee boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-fastboot.tsv   
│   │   └── [...]
│   ├── fastboot-opteemin                                                              Flash layout files for flashing via fastboot with opteemin boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-fastboot-opteemin.tsv   
│   │   └── [...]
│   ├── optee                                                                          Flash layout files for optee boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-optee.tsv
│   │   └── [...]
│   └── opteemin                                                                       Flash layout files for opteemin boot chain
│       ├── FlashLayout_<boot device>_<board name>-<hardware security>-opteemin.tsv
│       └── [...]
├── Kernel                                                                             Debug binaries for Linux kernel
│   ├── config-6.6.129                                                              Reference config file for Linux kernel
│   └── vmlinux                                                                        Image of the Linux kernel
├── optee                                                                              OPTEE-OS binaries
│   ├── debug                                                                          Debug binaries for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>.elf                      Debug symbol file for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>-programmer.elf           Debug symbol file for OPTEE-OS configured for usb/serial
│   │   └── [...]
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>.bin              OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>-programmer.bin   OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>.bin            OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>-programmer.bin OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>.bin               OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>-programmer.bin    OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   └── [...]
├── scripts
│   └── create_sdcard_from_flashlayout.sh
├── u-boot                                                                             U-BOOT binaries
│   ├── debug                                                                          Debug binaries for U-BOOT
│   │   ├── u-boot-<soc name>-<u-boot config>.elf                                      Debug symbol file for U-BOOT
│   │   └── [...]
│   ├── configuration-<soc name>-<u-boot config>_defconfig                             Reference configuration file for U-Boot
│   ├── u-boot-nodtb-<soc name>-<u-boot config>.bin                                  U-BOOT binary for FIP binaries creation
│   ├── u-boot-<board name>-<hardware security>-<u-boot config>.dtb                    U-BOOT device tree for FIP binaries creation
│   └── [...]
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.ext4                            Binary for full image content (no split of partition)
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.license
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs-license_content.html            License summary for all packages needed to feed all partitions
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp2.splitted-bootfs.ext4                    Binary for bootfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2.splitted-vendorfs.ext4                  Binary for vendorfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2.splitted-rootfs.ext4                    Binary for rootfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2.splitted-userfs.ext4                    Binary for userfs partition on eMMC and microSD card devices)
└── [...]

Description:

<soc name>:
* stm32mp21
* stm32mp23
* stm32mp25
<board name>:
* stm32mp215-dk, stm32mp235f-dk, stm32mp257f-dk, stm32mp257f-ev1
<hardware security>:
* if nothing declared then there is a minimal hardware configuration for RIFF profile OPEN
* ca35tdcid-ostl                 custom hardware configuration (can be different following use-case and hardware) for RIFF profile  CUSTOM (CLOSED)
* ca35tdcid-ostl-m33-examples    custom hardware configuration (can be different following use-case and hardware) for RIFF profile CUSTOM (CLOSED)
<boot chain>:
* fastboot                  optee boot chain for flashing via fastboot
* fastboot-opteemin         opteemin boot chain for flashing via fastboot
* optee                     optee boot chain
* opteemin                  opteemin boot chain
<storage>:
* emmc                            eMMC storage
* nand                            NAND storage
* nor                             NOR storage
* programmer-uart                 storage programmation via UART
* programmer-usb                  storage programmation via USB
* sdcard                          microSD card storage
<boot device>:
* emmc                            boot via emmc storage
* nand-4-256-1024 (nand-x-y-z)    boot via nand storage
* nand-4-256-1024-sdcard          boot via nand storage for first stage (fsbl, fip) and files system are located on sdcard
* nor                             boot via nor storage
* nor-sdcard                      boot via nor storage for first stage (fsbl, fip) and files system are located on sdcard
* sdcard                          boot via sdcard storage
* sdcard-EFI                      boot via sdcard but bootfs is configurated on EFI
<u-boot config>:
* default
* fastboot-emmc             Fastboot config enabled with MMC_DEV Id for emmc
* fastboot-sdcard           Fastboot config enabled with MMC_DEV Id for sdcard
* programmer                Programmer config enabled


For M33-TD flavor

Warning
Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
  • The STM32MP2 image (binaries) is delivered through one tarball file named FLASH-stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz applicable to STM32MP215F-DK and STM32MP257x-EV1

  • Download and install the STM32MP2 image (binaries):

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP2 Starter Package image - STM32MP2-Ecosystem-v6.2.1 release for M33-TD flavor
Download
Warning
Check first here, if a minor release based on this ecosystem release v6.2.1 is already published.
If a minor release exists, replace the name of the STM32MP2 Starter Package file, used below, and in other wiki articles, by the name of file delivered with the minor release.

Go on st.com to download the STM32MP2 Starter Package image, FLASH-stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz file.

Installation
cd <working directory path>/Starter-Package
  • Download the tarball file in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
tar xvf FLASH-stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10.tar.gz
Release note

Details of the content of this software package are available in the associated STM32 MPU OpenSTLinux release note.
If you are interested in older releases (STM32MP2-Ecosystem-v6.1.0 and STM32MP2-Ecosystem-v6.2.0), please have a look into the section Archives

  • The binaries and the Flash layout files are in the <Starter Package installation directory>/stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp2-m33td/ directory. The most important ones are:


stm32mp2-m33td
├── arm-trusted-firmware                                                                    TF-A binaries for FSBLa partitions and supported boot chains
│   ├── bl2                                                                                 TF-A BL2 binary for FIP binaries creation
│   │   ├── tf-a-<board name>-<hardware security>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── bl31                                                                                TF-A BL31 binary for FIP binaries creation
│   │   ├── debug                                                                           Debug binaries for BL31
│   │   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.elf           Debug symbol file for TF-A BL31
│   │   │   └── [...]
│   │   ├── <board name>-<hardware security>-<boot chain>-<storage>.dtb                     TF-A BL31 device tree for FIP binaries creation
│   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.bin           TF-A BL31 binary for FIP binaries creation
│   │   └── [...]
│   ├── ddr                                                                                 Trained DDR binary for FIP binaries creation
│   │   ├── ddr_pmu-<board name>-<hardware security>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── debug                                                                               Debug binaries for TF-A
│   │   ├── debug-tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32        Debug file for FSBL
│   │   ├── tf-a-bl2-<soc name>-<boot chain>-<storage>.elf                                  Debug symbol file for TF-A
│   │   └── [...]
│   ├── fwconfig                                                                            TF-A device tree for FIP binaries creation
│   │   ├── <board name>-<hardware security>-fwconfig-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── metadata.bin                                                                        Meta data binary for METADATA partition for the supported boards
│   ├── tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32                  TF-A binary for FSBL partition
│   └── [...]
├── arm-trusted-firmware-m                                                                  TF-M binaries for FSBLm partitions and supported boot chains
│   ├── debug                                                                               Debug binaries for TF-M
│   │   ├── debug-bl2-<board name>-<hardware security>.stm32                                Debug file for FSBLm
│   │   ├── tfm-<board name>-<hardware security>-<storage m33>-<storage a35>_s.elf          Debug symbol file for TF-M
│   │   └── [...]
│   ├── key                                                                                 Security key used by TF-M
│   │   ├── image_ns_signing_public_key-<board name>-<hardware security>-<storage m33>.pem
│   │   ├── image_s_signing_private_key-<board name>-<hardware security>-<storage m33>.pem
│   │   ├── image_s_signing_public_key-<board name>-<hardware security>-<storage m33>.pem
│   │   └── [...]
│   ├── bl2-<board name>-<hardware security>-<storage m33>.stm32                            TF-M binary for FSBLm partition
│   ├── ddr_phy_signed-<board name>-<hardware security>-<storage m33>.bin                   TF-M binary for M33ddr partition
│   └── [...]
├── fip                                                                                     FIP binaries for FIP partitions and supported boot chains
│   ├── fip-<board name>-<hardware security>-ddr-<boot chain>-<storage>.bin                 FIP binary for FIP DDR partition
│   ├── fip-<board name>-<hardware security>-<boot chain>-<storage>.bin                     FIP binary for FIP partition
│   └── [...]
├── flashlayout_st-image-weston                                                             Flash layout files (description of the partitions) for the supported boot chains on supported boot devices and boards
│   ├── [...]
│   ├── extensible                                                                          Flash layout files for microSD card boot device with no userfs partition but a rootfs partition extended to microSD card size
│   │   ├── FlashLayout_sdcard_<board name>-<hardware security>-extensible.tsv              (recommended setup for package repository service) microSD card boot device with rootfs partition extended to microSD card size
│   │   └── [...]
│   └── optee                                                                               Flash layout files for optee boot chain
│       ├── FlashLayout_<boot device>_<board name>-<hardware security>-optee.tsv
│       └── [...]
├── Kernel                                                                                   Debug binaries for Linux kernel
│   ├── config-6.6.129                                                                    Reference config file for Linux kernel
│   └── vmlinux                                                                              Image of the Linux kernel
├── m33-firmware                                                             TF-M/CubeMp2 binaries for M33FW partitions and supported boot chains
│   ├── ddr_phy-<board name>-cm33tdcid-ostl-sdcard_Signed.bin  <hardware security>-<storage m33>_Signed.bin  DDR binary for M33ddr' partition
│   ├── tf-m-starterapp-<board name>-<hardware security>-<storage m33>-<storage a35>_s_ns.bin  TF-M/CubeMP2 binary for M33FW partition
│   └── [...]
├── m33-project                                                             CubeMp2 firmware binaries which can be assembled with TF-M secure binaries
│   ├── StarterApp_M33TD_full-dynamic-<board name>-<hardware security>-<storage m33>-<storage a35>_ns.bin CubeMP2 binary
│   └── [...]
├── optee                                                                                    OPTEE-OS binaries
│   ├── debug                                                                                Debug binaries for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>.elf                            Debug symbol file for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>-programmer.elf                 Debug symbol file for OPTEE-OS configured for usb/serial
│   │   └── [...]
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>.bin                    OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>-programmer.bin         OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>.bin                  OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>-programmer.bin       OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>.bin                     OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>-programmer.bin          OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   └── [...]
├── scripts
│   └── create_sdcard_from_flashlayout.sh
├── u-boot                                                                                   U-BOOT binaries
│   ├── debug                                                                                Debug binaries for U-BOOT
│   │   ├── u-boot-<soc name>-<u-boot config>.elf                                            Debug symbol file for U-BOOT
│   │   └── [...]
│   ├── configuration-<soc name>_defconfig                                                   Reference configuration file for U-Boot
│   ├── u-boot-nodtb-<soc name>-<u-boot config>.bin                                        U-BOOT binary for FIP binaries creation
│   ├── u-boot-<board name>-<hardware security>-<u-boot config>.dtb                          U-BOOT device tree for FIP binaries creation
│   └── [...]
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.rootfs.ext4                            Binary for full image content (no split of partition)
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.rootfs.license
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.rootfs-license_content.html            License summary for all packages needed to feed all partitions
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.rootfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.splitted-bootfs.ext4                    Binary for bootfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.splitted-vendorfs.ext4                  Binary for vendorfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.splitted-rootfs.ext4                    Binary for rootfs partition on eMMC and microSD card devices)
├── st-image-weston-openstlinux-weston-stm32mp2-m33td.splitted-userfs.ext4                    Binary for userfs partition on eMMC and microSD card devices)
└── [...]

Description:

<soc name>:
* stm32mp21
* stm32mp25
<board name>:
* stm32mp215-dk, stm32mp257f-ev1
<hardware security>:
* if nothing declared then there is a minimal hardware configuration for RIFF profile OPEN
* cm33tdcid-ostl                     custom hardware configuration (can be different following use-case and hardware) for RIFF profile  CUSTOM (CLOSED)
* cm33tdcid-ostl-serial-ca35tdcid    specific configuration used for programmation
<boot chain>:
* optee                     optee boot chain
<storage>:
* emmc                            eMMC storage
* nor                             NOR storage
* programmer-uart                 storage programmation via UART
* programmer-usb                  storage programmation via USB
* sdcard                          microSD card storage
<storage a35>:
* emmc                            eMMC storage
* nor                             NOR storage
* sdcard                          microSD card storage
<storage m33>:
* emmc                            eMMC storage
* nor                             NOR storage
* sdcard                          microSD card storage
<boot device>:
* emmc                            boot Cortex M33 via emmc storage and Cortex A35 via emmc storage
* nor-emmc                        boot Cortex M33 via nor storage and Cortex A35 via emmc storage
* nor-nor-sdcard                  boot Cortex M33 via nor storage and Cortex A35 via nor storage for first stage (fsbl, fip) and files system are located on sdcard storage
* nor-sdcard                      boot Cortex M33 via nor storage and Cortex A35 via sdcard
* sdcard                          boot Cortex M33 via sdcard storage and Cortex A35 via sdcard storage
<u-boot config>:
* default
* programmer                Programmer config enabled


7. Populate the SD card[edit | edit source]

  • Set the boot switches (located on the MB2059) to the OFF position "Boot from UART/USB":
Boot from UART/USB
  • Connect the PC to CN15/USB_DRD port of the STM32MP215F-DK mother board through the USB Type A to Type C cable.
  • Power up the board.
  • Press the reset button to reset the board.
  • Launch STM32CubeProgrammer to get the GUI :
STM32CubeProgrammer GUI


  • On the right of the window, select USB (instead of STLINK, set by default) from the connection picklist, and click the "Refresh" button. The serial number is displayed if the USB has been detected.
  • Click Connect
Select USB for connection with board


  • Please expand one of the following section depending of whether A35-TD flavor or M33-TD flavor is used

For A35-TD flavor

  • Select the Open File tab and choose the FlashLayout_sdcard_stm32mp215f-dk-optee.tsv in the Starter Package installation folder ($HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Starter-Package/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp2/flashlayout_st-image-weston/optee)

For M33-TD flavor

  • Select the Open File tab and choose the FlashLayout_sdcard_stm32mp215f-dk-cm33tdcid-ostl-optee.tsv in the Starter Package installation folder ($HOME/STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Starter-Package/stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v26.06.10/images/stm32mp2-m33td/flashlayout_st-image-weston/optee)


  • Fill the Binaries Path by browsing to the $[Starter_Pack_Path]/images/stm32mp2 folder.
open .tsv optee and fill Binaries Path for EV1 - Picture is not contractual
  • Click Download to launch the flashing process.
  • A progress bar indicates the process progress until a completion pop-up message is displayed.

8. Boot the board[edit | edit source]

  • Set the boot switches (located on the MB2059) to the microSD card boot position, depending of whether A35-TD flavor or M33-TD flavor is used

For A35-TD flavor

Boot from microSD card


For M33-TD flavor

Boot from microSD card


  • Reconnect the TTL serial cable(s)
  • Power on the board.
  • Press the Reset button to reset the board.
  • After few seconds, the board starts and automatically goes through the following screens:
Warning
The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards.
U-Boot splash screen
Linux splash screen
Weston desktop
GTK demo launcher
  • If the board power supply does not supply enough current (< 1500 mA, with a PC USB-A typically), the power LED indicates the issue following the rules below:
Power LED status Display connected Console message Boot process
Red LVDS Console stuck at :
No EFI system partition
Failed to persist EFI variables
Stop before autoboot
Orange HDMI No particular warning Continue and orange LED stays on
Orange No display No particular warning Continue and orange LED stays on