Last edited 11 months ago

STM32MP215x-DKx - board assembly

Applicable for STM32MP21x lines


This article explains how to assemble the STM32MP215x-DKx Discovery kits. It is valid for the STM32MP215F-DK Discovery kit: the part numbers are specified in the STM32MP21 microprocessor part numbers article.

Warning
To start the board, it is recommended to go through the corresponding Starter Package article first.


The STM32MP215x-DKx Discovery kit package (STM32MP215F-DK ) contains only the MB2059 motherboard.

STM32MP215F-DK Discovery kit front side (picture not contractual)
Information
Display and camera are available for purchase to complete this basic setup.

The complete set contains:

STM32MP215F-DK and additional accessories kits shown here (picture is not contractual)
Position Description
1 MB2059 main board
2 MicroSD card
3 4.3" TFT 480*272 pixels with LED Backlight and capacitive touch panel RK043FN78H-CT661C (optional)
4 Camera board FFC (provided with the B-CAMS-IMX package) (optional)
5 MB1854 camera board provided with the B-CAMS-IMX package (optional)


STM32MP215F-DK Discovery kit assembly (picture is not contractual)


1. Connecting the display to the board (optional)[edit | edit source]

  • Find the DISPLAY connector (CN8) on the top side of the MB2059 main board
  • Flip the connector’s latch up
Display board assembly - step 1 (picture is not contractual)
Display board assembly - step 2 (picture is not contractual)


  • Insert the LCD’s cable with the exposed contacts facing down
Display board assembly - step 3 (picture is not contractual)


  • Flip the connector’s latch down to secure the cable
Display board assembly - step 4 (picture is not contractual)


2. Connecting the MB1854 camera board to the board (optional)[edit | edit source]

Camera board assembly (picture is not contractual)


  • Find the camera ports on the STM32MP215x-DK Discovery kit (CN4) (#1 in the image above) and MB1854 (CN1) (#2 in the image above). The camera box contains one FFC.
  • For each port:
    • Pull the plastic (#1 in the image below) lightly to insert the contact side of the FFC towards the board (#2 in the image below).
    • Push the plastic carefully to hold the FFC (#3 in the image below).
Camera board assembly (picture is not contractual)


3. Connecting USB to TTL serial cables[edit | edit source]

To have 2 consoles on your workstation , one for Cortex-M33 and one for Cortex-A35, 2 "USB to TTL serial cables" are needed.

(picture is not contractual)



4. STM32MP215x-DK Discovery kit assembled and connected[edit | edit source]

The picture below presents the recommended board connections for getting started with the STM32MP215x-DKx Discovery kits

Warning
To start the board, it is recommended to go through the corresponding Starter Package article first.

As shown in the board overview, other connectors are available for this board (for example, the GPIO expansion connector).


MB2059 motherboard: STM32MP215F 14x14MicroSD<sup>™</sup> card slotReset buttonEthernet (network)USB Power Delivery Type-C (Power) and USB3.0 DRD/OTG Type-C (programmable through STM32CubeProgrammer)CSI cameraLTDC displayUSB to TTL serial cables
STM32MP215x-DKx Discovery kit connections (picture is not contractual)