Modify, rebuild and reload the firmware for A35-TD flavor

Applicable for STM32MP21x lines

Develop on Arm® Cortex®-M33 What's next
Install the IDE Install STM32CubeMP2 package Modify, rebuild and reload the firmware for A35-TD flavor
Modify, rebuild and reload the firmware for M33-TD flavor


Trusted domain applicability
This article is not applicable to M33-TD flavor of STM32MP2 series

1. Overview[edit | edit source]

This stage explains how to modify, rebuild, and reload an STM32MP2 Arm® Cortex®-M33 coprocessor firmware.

It proposes to customize the STM32MP2Cube package application example, named OpenAMP_TTY_Echo, using STM32CubeIDE.

2. STM32CubeMP2 Firmware prerequisites[edit | edit source]

  • For this part, it is needed to flash another tsv.
Information
This tsv modifies the security configuration to have the needed peripherals accessible at M33 side and it disables lot of things not needed to test the M33 examples, like the internet at Linux level.
  • Boot from SD card with ecosystem release v6.2.1 , using
    • For STM32MP215F-DK Discovery kit  : FlashLayout_sdcard_stm32mp215f-dk-ca35tdcid-ostl-m33-examples-optee.tsv
    • For STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation  : FlashLayout_sdcard_stm32mp235f-dk-optee.tsv
    • For STM32MP257F-DK Discovery kit  : FlashLayout_sdcard_stm32mp257f-dk-ca35tdcid-ostl-m33-examples-optee.tsv
    • For STM32MP257F-EV1 Evaluation board : FlashLayout_sdcard_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee.tsv
  • Install build environment
1- Install dependencies, normally already done in PC Prerequisite :
sudo apt-get install -y git curl wget build-essential libssl-dev python3 \
           python3-pip cmake make libncurses5
2-Add CMake path into environment:
export PATH=<CMake path>/bin:$PATH
3-Verify cmake version:
cmake --version
4-Use cmake at least or newer than 3.22.1.
  • Install Python libraries needed by OP-TEE signature Python script.
sudo apt install python3-pyelftools
sudo apt install python3-pycryptodome
sudo apt install python-is-python3

3. Disconnect the "minicom" console[edit | edit source]

  • If minicom is already open, disconnect it to use the STM32CubeIDE built-in serial console.
Ctrl + A then Q

4. Open STM32CubeIDE[edit | edit source]

  • Start STM32CubeIDE
STM32CubeIDE Starter Screen


  • Choose a workspace (default is fine).
  • Notice the information provided on the Information Center page and close it. (You can open it later.)


STM32CubeIDE Information Center Page


  • Go into your workspace project view.
STM32CubeIDE Project View

5. Import an existing example in STM32CubeIDE[edit | edit source]

  • In the File menu, select Import. Then, in General choose Existing Project into Workspace.
STM32CubeIDE import screen
  • Browse and select the OpenAMP_TTY_echo application example in the folder matching your board :
    • For STM32MP215F-DK Discovery kit  : $HOME//STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/STM32Cube_FW_MP2_V1.3.X [X:0;2]/Projects/STM32MP215F-DK/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE,
    • For STM32MP257F-DK Discovery kit for STM32MP23x lines evaluation  : $HOME//STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/STM32Cube_FW_MP2_V1.3.X [X:0;2]/Projects/STM32MP235F-DK/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE,
    • For STM32MP257x-DK Discovery kit  : $HOME//STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/STM32Cube_FW_MP2_V1.3.X [X:0;2]/Projects/STM32MP257F-DK/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE,
    • For STM32MP257x-EV1 Evaluation board  : $HOME//STM32MPU_workspace/STM32MPU-Ecosystem-v6.2.1/Developer-Package/STM32Cube_FW_MP2_V1.3.X [X:0;2]/Projects/STM32MP257F-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/STM32CubeIDE.
  • STM32CubeIDE brings a specific project structure for dual-core devices such as STM32MP2. A top-level project contains sub-projects for each core.
  • Here, the OpenAMP_TTY_echo top project contains OpenAMP_TTY_echo_CM33_NonSecure and OpenAMP_TTY_echo_CM33 sub-projects. Keep the three projects selected and click on "Finish".
STM32CubeIDE project selection
  • The OpenAMP_TTY_echo project is open, and you can browse inside using the left panel.
OpenAMP_TTY_echo project structure

6. Build the firmware[edit | edit source]

  • Select project OpenAMP_TTY_Echo_CM33_NonSecure and choose CA35TDCID_m33_ns_sign build configuration (the little arrow on the right of the hammer in the toolbar). By default, CA35TDCID_m33_ns is selected.
STM32CubeIDE build the project


  • Due to a temporary issue related to the cmake version used, please update the Properties->C/C++Build->Settings->Build Steps

append the Command line with "-DCMAKE_POLICY_VERSION_MINIMUM=3.5"

STM32CubeIDE build the project
  • "Build" is finished with no errors.
STM32CubeIDE build finished with no error

7. Check connection to the target[edit | edit source]

STM32CubeIDE requires a connection to Linux® running on an STM32MP2 device though a serial connection.
This connection is automatically detected and configured when you connect the cable to the ST-Link port and the board has booted.

You can check if you can get the Linux® log and prompt by clicking on the STM32 butterfly button :

STM32CubeIDE Serial Console button

Connection is correct if the Linux® log or prompt is displayed in the console window.

STM32CubeIDE Linux Prompt

Your board might be connected to the PC by Ethernet, either using RJ45 (point-to-point or VLAN) or USB0 EthernetOverUSB gadget (point-to-point connection with PC using TypeA-TypeC cable). The screenshot below uses the second solution.

When a serial connection is established, STM32CubeIDE automatically detects the board IP address and displays it in the Serial Target widget status window in the bottom right part of the screen.

STM32Cube Serial Target widget status

In case of different statuses such as busy or console in use, check that you have no other terminal connected and close the console. Also, check that the preferred device is /dev/ttyACM0 in the menu Window > Preferences > STM32Cube > MPU Serial:

STM32CubeIDE serial preferred device

Furthermore, if the status is Stopped, right-click there and then click on Start:

STM32Cube Serial Target widget change status

8. Start Debug Session[edit | edit source]

  • Click on your OpenAMP_TTY_echo_CM33_NonSecure project to select it.
  • With the arrow right of the hammer sign, choose the project configuration with _sign in the name, then it builds it.
  • If not already created, you will need a run configuration (to load without debug) and a debug configuration (to debug without download).
  • Run configuration: create it by right-clicking on " OpenAMP_TTY_echo_CM33_NonSecure and selecting Run As and STM32 C/C++ Application. It opens the Embedded C/C++ Application window.


Select application to run
  • Click the OK button. It opens the Edit the Configuration window. You may modify the name of the run configuration and must replace CA35TDCID_m33_ns_sign/OpenAMP_TTY_echo_CM33_NonSecure.elf with CA35TDCID_m33_ns_sign/OpenAMP_TTY_echo_CM33_NonSecure_sign.bin as shown in the following picture and press the OK button.


Change Application to load in Run Configuration


  • The other tabs of the configuration should be fine by default. To check the IP, in the debugger tab you can check if the address is correctly filled.
  • Make sure the Thru Linux core (production mode) is selected.
  • When the configuration is correct, click on OK.
  • To run the configuration, first click on the arrow right on the run button and then click on Run Configurations...
Run configurations...
  • When the Run Configurations window is open, select the user configuration and click on the Run button. The binary file is loaded. After this step, the user configuration appears in the menu of the Run button.
Run configurations menu
  • Now the firmware is loaded. To debug it, a debug configuration is needed. Create it by right-clicking on OpenAMP_TTY_echo_CM33_NonSecure and selecting Debug As and STM32 C/C++ Application. It will open the Embedded C/C++ Application window.


Select application to debug


  • In the Edit the Configuration window, click the OK button. Click on the Startup tab and select the file. You may modify the name by adding _Debug.


Start up tab


  • Then click on the Edit button, in the Add/Edit item, uncheck Download and click OK.


Uncheck Download
  • Click OK in the Edit Configuration where there is a False for the download.
No Download selected
  • The debug perspective is started. If not, proceed in the same way as the run configuration but with the debug button instead. Press the suspend button, and the firmware will stop as shown here:
Suspend in the code

In "production mode", the firmware does not break at main. GDB is simply attached to the running target. You can then use all features of the debugger.

Information
To benefit of the best GDB debug experience it's recommended to upgrade the onboard ST-Link version with the latest release. You can simply do it from STM32CubeIDE using menu "Help -> ST-Link Upgrade"

For further information, refer to the STM32CubeIDE documentation available on my.st.com.

9. Test the firmware[edit | edit source]

The OpenAMP_TTY_echo_CM33 firmware do the following:

  • CPU2(CM33) initializes OpenAMP middleware which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framework infrastructure,
  • CPU2(CM33) creates 2 rpmsg channels for 2 virtual UART instances (UART0 and UART1),
  • CPU2(CM33) is waiting for messages from CPU1(CA35) on these both channels,
  • When CPU2(CM33) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA35) on the same Virtual UART instance.

Reopen the Serial console of STM32CubeIDE and enter following commands :

  • Initialize the ttyRPMSG0 configuration.
stty -onlcr -echo -F /dev/ttyRPMSG0
  • Read constantly the ttyRPMSG0 channel in background
cat /dev/ttyRPMSG0 &
  • Send a message on one ttyRPMSG0 channel and receive the echo on the same ttyRPMSG0 channel.
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
  • You can perform the same steps with the ttyRPMSG1 channel.
  • Terminate the STM32CubeIDE debug session will stop the firmware.

10. Modify the firmware[edit | edit source]

The original firmware example receives a message for the host on one channel and acknowledges by returning the same message to the host on the same channel.

As it is not obvious which channel receives the message, we propose modifying the firmware to add an indication of the channel receiving the message.

To do this, modify the main.c original code as follows:

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    OPENAMP_check_for_message();

    /* USER CODE END WHILE */
    if (VirtUart0RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      int msg_size = 0;
      VirtUart0RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size);
    }

    if (VirtUart1RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      uint16_t msg_size = 0;
      VirtUart1RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size);
    }
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
  • Save your modifications.
  • Then open the properties of the project by right-clicking on it and selecting Properties.

Go to C/C++ Build > Settings > MCU GCC Compiler > Preprocessor.

Add a new symbol: __LOG_TRACE_IO_.

This symbol will enable the log_info macro.

11. Testing the modified firmware[edit | edit source]

11.1. Relaunch debug session[edit | edit source]

  • By clicking on the Run button, as explained in the Start Debug Session chapter, you can download the firmware. Then, by clicking on the Debug button, the STM32CubeIDE relaunches the debug session after performing an incremental build to account for your modifications.
  • If everything is correct, you will switch back to the Debug Perspective window after reloading the new firmware.

11.2. Test[edit | edit source]

  • Initialize the ttyRPMSG0 and ttyRPMSG1 configurations.
stty -onlcr -echo -F /dev/ttyRPMSG0
stty -onlcr -echo -F /dev/ttyRPMSG1
  • Read constantly the ttyRPMSG0 and ttyRPMSG1 channels in the background.
cat /dev/ttyRPMSG0 &
cat /dev/ttyRPMSG1 &
  • Send a message on one ttyRPMSG0 channel and check the echo log.
echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Channel RPMSG0: Hello Virtual UART0
  • Send a message on one ttyRPMSG1 channel and check the echo log.
echo "Hello Virtual UART1" > /dev/ttyRPMSG1
Channel RPMSG1: Hello Virtual UART1


Information
  • on STM32MP15x lines : When the firmware is running, you can output log from the firmware by using the following command:
 cat /sys/kernel/debug/remoteproc/remoteproc0/trace0
  • On STM32MP2 series: When the firmware is running, log traces are output on an external terminal through a UART peripheral. For instance, for an STM32MP257F-EV1 board, the terminal is available on a Linux PC at /dev/ttyACM1:
 minicom -D /dev/ttyACM1


  • Terminate the STM32CubeIDE debug session.

12. To go further[edit | edit source]

If you want to build and debug a secure project, refer to How to build and debug secure project on Cortex-M33 coprocessor in STM32CubeIDE