This page is a candidate for renaming (move). The requested new name is: How to develop an STM32 MPU Expansion Package (I-Pack) . The supplied reason is: In the ST product tree, it is not "STM32MPU" but rather "STM32 MPU" . -- Registered User (-) 10:26, 24 March 2023 (CET). Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |
This article explains how to create your own STM32 MPU Expansion Package to extend the limits of the ecosystem.
1. Design of an STM32 MPU Expansion Package for an OpenSTLinux Distribution Package[edit source]
An STM32 MPU Expansion Package for an OpenSTLinux Yocto distribution is a solution proposed to extend a Distribution Package by providing new features, examples, or demonstrations.
Three possible profile types are defined to cover different user needs according to the changes required in the OpenSTLinux distribution:
- OpenSTLinux tools add-on: use when making changes only at the Linux® user space level, without applying any change to the boot chain or the Linux® OS.
- OpenSTLinux embedded software add-ons: when modifying the Linux® kernel part (configuration, device tree update), or/and adding user space applications/frameworks needed to demonstrate the Arm® Cortex®-A processor functionality.
- Coprocessor and OpenSTLinux embedded software add-ons: use in the case of the profile type 2, and/or when modifying the STM32Cube MPU part and/or including new firmware source code example to demonstrate the Cortex®-M coprocessor functionality.
2. Check for OpenSTLinux compatibility version[edit source]
To ensure the adherence with a given OpenSTLinux version, the dependency is managed with a dedicated ST_OSTL_COMPATIBILITY_VERSION_<layer_name> variable to set in the I-PACK Yocto meta layer (layer.conf file).
This information is verified at the compilation phase.
To get the version to set, refer to the variable value given in meta-st-openstlinux/conf/layer.conf , for example:
ST_OSTL_COMPATIBILITY_VERSION_st-openstlinux = "4.1"
3. STM32 MPU Expansion cases[edit source]
3.1. OpenSTLinux tools add-on[edit source]
This profile type covers the case when only changes/additions are done at the Linux® user space level for applications, tools, or scripts on the root file system.
Two possible approaches:
- Add a Standard Yocto layer to the OpenSTLinux distribution: refer to the existing skeleton example[1] in Yocto Project®.
- Deploy a Debian package on the target: when all dependencies are already managed in the embedded software on the target, it is possible to install the new applications by using a standard Debian package.
3.2. OpenSTLinux embedded software add-ons[edit source]
This profile type covers previous one and is recommended when some additional changes are required at the Linux® kernel level (configuration and/or device tree update), and/or adding user space application(s)/framework(s) needed to demonstrate Cortex®-A processor functionalities.
For this case, the OpenSTLinux distribution must be updated, and the proposed solution is to add a new add-on meta layer to provide the services described below. A meta layer template is proposed as reference to help modifying BSP components: meta-st-stm32mp-addons[2].
Otherwise, if only the user space applications and image must be updated, refer to the existing skeleton example[1] in Yocto Project® for a standard Yocto layer.
3.2.1. New image creation with additional Linux user space packages[edit source]
Refer to the How_to_create_your_own_image wiki page.
As example, have a look to the X-LINUX-AI Expansion Package image recipe: https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/blob/master/recipes-st/images/st-image-ai.bb
3.2.2. TF-A, OP-TEE, U-Boot, Kernel device tree(s) update[edit source]
Two possible approaches, which depend of the way the top device tree source file is written for the given reference board:
- The dts file contain the complete device tree settings and is generated by using STM32CubeMX (see STM32CubeMX_generated_device_tree)
- A new device tree source file (.dts) inherits from an existing DT file of an ST board and is used to modify/add DT node Overload the device tree (i.e. minor changes compared to existing boards)
For both approaches, the way to declare it in the I-Pack meta layer is the same, and is done in the machine file (conf/machine directory). For example see conf/machine/stm32mp13-mx.conf (STM32MP13x lines ) or conf/machine/stm32mp15-mx.conf (STM32MP15x lines ).
- Force the new device tree source file usage: ENABLE_CUBEMX_DTB ?= "1"
- Define the dtb binary name to be generated, which is the same as the dts file you want to use: CUBEMX_DTB = "<your_dtb_file_name>"
- Define the path for the device tree files: CUBEMX_PROJECT = "'<your_dt_file_path>"
Ensure the corresponding device tree source files that have to be taken into account must be present in the path given by variable CUBEMX_PROJECT previously defined.
Then, as the examples provided in meta-st-stm32mp-addons[2], this is possible for each BSP components to define the device tree source file to be used by an update of the corresponding recipes.
Component | Yocto recipe append example for BSP components |
---|---|
TF-A | tf-a-stm32mp_%.bbappend |
OP-TEE | optee-os-stm32mp_%.bbappend |
U-Boot | u-boot-stm32mp_%.bbappend |
Linux Kernel | linux-stm32mp_%.bbappend |
3.2.3. Linux® kernel configuration change[edit source]
Two possible approaches:
- Make defconfig changes by using a configuration fragment file (recommended)
- Provide a full defconfig file
3.2.3.1. Change defconfig with a configuration fragment file[edit source]
A simple way to update the Linux® kernel configuration is to use a fragment file. You can refer to the Yocto Project® web article Creating Configuration Fragments for information.
The config fragment file must be added in the path meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp/<config_fragment_file_name>.
The linux-stm32mp recipe file must be appended to update the build setup. It is done through the file meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend.
In this file, the new config fragment file must be added to the variable KERNEL_CONFIG_FRAGMENTS and listed in the SRC_URI variable as given below:
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:" SRC_URI += "file://<config_fragment_file_name>" KERNEL_CONFIG_FRAGMENTS += "<config_fragment_file_name>"
3.2.3.2. Use new full defconfig file[edit source]
This is also possible to provide a full defconfig file for the Linux® kernel configuration building.
For creating a defconfig file, refer to the Yocto Project® web article Creating a defconfig File.
The file must be present in the path meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp/<defconfig_file_name>.
The linux-stm32mp recipe file must be appended to update the build setup. It is done through the file meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend.
In this file, the variable KERNEL_DEFCONFIG must be cleaned, the new variable KERNEL_EXTERNAL_DEFCONFIG must be defined, and the path of the <defconfig_file_name> listed in the SRC_URI variable must be as given below:
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:" SRC_URI += "file://<defconfig_file_name>" KERNEL_DEFCONFIG = "" KERNEL_EXTERNAL_DEFCONFIG = "<defconfig_file_name>"
3.2.4. Addition of source code / binary files for new applications[edit source]
Refer to How_to_add_a_customer_application wiki article.
Two other wiki pages are also proposed to help for meta-st-stm32mp-addons usage:
3.3. Coprocessor and OpenSTLinux embedded software add-ons[edit source]
Coming soon |
This profile type inherits from OpenSTLinux embedded software add-ons and is recommended when some changes are required at STM32CubeMPU part and/or to include new firmware source code example to demonstrate Cortex®-M coprocessor functionality (including hardware resources reallocations).
4. I-Pack Expansion Package example[edit source]
X-LINUX-AI_OpenSTLinux_Expansion_Package
5. References[edit source]