Last edited 8 months ago

How to create your own machine

Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines



1. Introduction[edit | edit source]

For your own needs, you can add in the Yocto project a new machine reflecting your own board and your own features.
This article is reserved to Yocto experts or at least people who have already practiced with the Yocto environmment.

This section describes how to add and configure a machine that is similar to those that the OpenSTLinux Distribution Package already supports.
This customer machine is associated to STM32CubeMX tool which provides DeviceTree files per component (e.g. tf-a, optee-os, u-boot, kernel and others).

We suppose here that all the material described below is done inside an existing STM32MP BSP layer 'addons'.
For reminder this addons layer is deployed here in our delivery : <path of STM32_MPU_Distribution_Package>/layers/meta-st/meta-st-stm32mp-addons/

2. Generate device tree[edit | edit source]

The principle is that the user generates device tree files from the STM32CubeMX tool.
With the STM32CubeMX tool, the user browses inside the OpenSTLinux Distribution Package file system until mx folder located into STM32MP BSP layer addons : <path of STM32_MPU_Distribution_Package>/layers/meta-st/meta-st-stm32mp-addons/mx/

  • several sub-folders are created and populated with generated device tree files :
mx
└── <ProjectPath>
    ├── <CortexA>
    │   └── DeviceTree
    │       └── <ProjectName>
    │           ├── kernel                                     Device tree files for Linux kernel
    │           │   │── <soc-machine>-<ProjectName>-mx.dts
    │           │   └── [...]
    │           ├── optee-os                                   Device tree files for OP-TEE
    │           │   │── <soc-machine>-<ProjectName>-mx.dts
    │           │   └── [...]
    │           ├── tf-a                                       Device tree files for TF-A
    │           │   │── <soc-machine>-<ProjectName>-mx.dts
    │           │   └── [...]
    │           └── u-boot                                     Device tree files for U-BOOT
    │               │── <soc-machine>-<ProjectName>-mx.dts
    │               └── [...]
    ├── CM33           (Availability depending of configuration used with STM32CubeMX tool)
    │   ├── DeviceTree
    │   │   └── <ProjectName>
    │   │       ├── mcuboot                                    Device tree files for MCUBOOT
    │   │       │   │── <soc-machine>-<ProjectName>-mx.dts
    │   │       │   └── [...]
    │   │       └── tf-m                                       Device tree files for TF-M
    │   │           │── <soc-machine>-<ProjectName>-mx.dts
    │   │           └── [...]
    │   ├── NonSecure                                          M33 firmware non-secure application files
    │   └── PlatformTF-M                                       Platform files for TF-M
    └── ExtMemLoader   (Availability depending of configuration used with STM32CubeMX tool)
        └── <ProjectName>
            ├── optee-os                                       Specific device tree files to generate FIP programmer binary
            │   │── <soc-machine>-<ProjectName>-mx.dts
            │   └── [...]
            ├── tf-a                                           Specific device tree files to generate TF-A and FIP programmer binaries
            │   │── <soc-machine>-<ProjectName>-mx.dts
            │   └── [...]
            └── u-boot                                         Specific device tree files to generate FIP programmer binary
                │── <soc-machine>-<ProjectName>-mx.dts
                └── [...]

Description:

 <CortexA>:	CA7 or CA35 depending of configuration selected with STM32CubeMX tool
 <ProjectPath>:	the sub-path of STM32CubeMX user project within mx folder
 <ProjectName>:	the STM32CubeMX user project name
 <soc-machine>:	the soc name without '-dkX' or '-evX' extension (e.g. stm32mp135f, stm32mp157f, stm32mp257f, etc)


3. Create a customer machine[edit | edit source]

Create a machine based on the one provided by ST and align some environment variables with the content of mx/<ProjectName> sub-folders

3.1. Create the new machine[edit | edit source]

cd <path of STM32_MPU_Distribution_Package>/layers/meta-st/meta-st-stm32mp-addons/conf/machine
cp <stm32mp1x|stm32mp2x>-mx.conf <stm32mp1x|stm32mp2x>-<ProjectName>.conf

3.2. Edit the new machine file[edit | edit source]

In the customer machine file, move to User machine customization sections paragraph to configure your machine:

  • Boot Scheme
To select your boot scheme configuration(s), comment and uncomment the BOOTSCHEME_LABELS lines.
  • Boot Device Choice
To select your boot device configuration(s), comment and uncomment the BOOTDEVICE_LABELS lines.
  • Support Feature Choice
To select additional features to enable on board, uncomment the MACHINE_FEATURES proposed lines.
  • Specific firmware and kernel modules configuration
This section allows user to configure some specificities related to its board hardware.
- KERNEL_MODULE_AUTOLOAD you may need to feed this variable with the list of kernel modules that need to be loaded at boot time, such as 'goodix' for current touch-screen used on STM32MP157F-EV1 evaluation board.
- BLUETOOTH_LIST in case you enable the bluetooth feature for your machine, you should set, at least, the firmware module to use for your hardware (e.g. 'linux-firmware-bluetooth-bcm4343' for STM32MP157F-DK2 discovery board).
- WIFI_LIST in case you enable the wifi feature for your machine, you should set, at least, the firmware module to use for your hardware (e.g.'linux-firmware-bcm43430' for STM32MP157F-DK2 discovery board).
  • CubeMX Project config
You have to uncomment and configure the following variables to set your CubeMX project:
- CUBEMX_DTB name of CubeMX generated device tree files, without file extension (e.g. stm32mp135f-<ProjectName>-mx)
- CUBEMX_PROJECT path of CubeMX generated device tree files relative to layer path folder (e.g. mx/<ProjectPath>)
- CUBEMX_PROJECT_NAME name of CubeMX project (e.g. <ProjectName>)
Optionally you can also uncomment and configure the CUBEMX_M33_TZ variable to indicate if M33 co-processor is used with Trustzone enabled or not (only for STM32MP2 series).

In order to give a better view on how to configure these variables, some machine samples are provided to show how to set-up a disco and eval board CubeMX machine: refer to conf/machine/examples from meta-st-stm32mp-addons layer.


3.3. Create symbolic link for EULA with new machine created[edit | edit source]

To support GPU and third party content, you need to accept the EULA. So a symbolic link must be created with the EULA existing file and the new machine :

cd <path of STM32_MPU_Distribution_Package>/layers/meta-st/meta-st-stm32mp-addons/conf/eula
ln -s ST_EULA_SLA <stm32mp1x|stm32mp2x>-<ProjectName>

4. Miscellaneous[edit | edit source]

4.1. STM32CubeMX class[edit | edit source]

A dedicated class is provided here :

<STM32MP BSP layer addons>/classes/cubemx-stm32mp.bbclass

The main goal of this class is to manage any change done by the customer in sub folders mx/<ProjectName>/...

So if a device tree file is updated for one or more of components, this change will be taken into account automatically during the next compilation done in the Distribution Package.

5. Compile your image with the yocto build process[edit | edit source]

cd <path of yocto delivery>
 (directory which contains meta-st, openembedded-core, meta-openembedded)
MACHINE=<stm32mp1x|stm32mp2x>-<ProjectName> DISTRO=openstlinux-weston source layers/meta-st/scripts/envsetup.sh Accept the term of EULA (if you agree with)
bitbake st-image-weston The generated images are available on build-openstlinuxweston-<stm32mp1x|stm32mp2x>-<ProjectName>/tmp-glibc/deploy/images/<stm32mp1x|stm32mp2x>-<ProjectName>
Warning
In case build fail for an error in the machine.conf, pay attention to do a -c cleanall prior to relaunch the build after correction


5.1. Issue with for stm32mp2 machine[edit | edit source]

Warning
Point of attention with M33FW_FIRMWARE configuration on A35-TD flavor

With A35-TD flavor , several ST boards use the Cortex M33 processor (associated to a specific firmware provided by STM32Cube MP2).
For this usage the flag MACHINE_FEATURES have the tag m33copro present.

In this context, you must declare M33FW_FIRMWARE and M33FW_DEFAULT_FIRMWARE variables.

Table of default firmware to use with ST boards:

Board Configuration to have
STM32MP215F-DK M33FW_FIRMWARE[cubemx] ="Projects/STM32MP215F-DK/Demonstrations/OpenAMP/OpenAMP_TTY_echo,OpenAMP_TTY_echo"

M33FW_DEFAULT_FIRMWARE[cubemx] ="OpenAMP_TTY_echo"

STM32MP257F-DK for STM32MP23x lines evaluation M33FW_FIRMWARE[cubemx] ="Projects/STM32MP235F-DK/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

STM32MP257F-DK M33FW_FIRMWARE[cubemx] ="Projects/STM32MP257F-DK/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

STM32MP257F-EV1 M33FW_FIRMWARE[cubemx] ="Projects/STM32MP257F-EV1/Demonstrations/USBPD_DRP_UCSI,USBPD_DRP_UCSI"

M33FW_DEFAULT_FIRMWARE[cubemx] ="USBPD_DRP_UCSI"

Information
If you don't need to use the Cortex M33 processor, you can disable it by not providing the tag 'm33copro' on 'MACHINE_FEATURES'