This article describes how the STM32MP2 series firewall should be configured to allow STM32 MPU Embedded Software distribution execution.
1. Overview[edit source]
The objective of this article is to provide guidelines for the hardware system firewall configuration taking into account the different platform constraints.
On STM32MP2 series, the system firewall protects internal RAM, external memories and internal peripherals. It is the Resource Isolation Framework.
A minimal coherent RIF configuration is required to execute STM32 MPU Embedded Software distribution and support the different low power modes.
2. Firewall attributes of OSTL software components[edit source]
Firewall Attributes | TF-A | OP-TEE Core | OP-TEE Trusted Applications | U-Boot | Linux kernel space | Linux user space | TF-M Core | TF-M Applications RoT | Cube Firmware |
---|---|---|---|---|---|---|---|---|---|
Secure level | Secure | Secure | Secure | Non-Secure | Non-Secure | Non-Secure | Secure | Secure | Non-Secure |
Privilege level | Privileged | Privileged | Non-Privileged | Privileged | Privileged | Non-Privileged | Privileged | Non-Privileged | Privileged |
CID attribute | CID1 | CID1 | CID1 | CID1 | CID1 | CID1 | CID2 | CID2 | CID2 |
3. RIF initial hardware configuration[edit source]
The RIF is made up of several protection units like described in Resource Isolation Framework overview.
The initial hardware configuration depends on the type of peripheral/memory to protect and their usage by the ROM code.
3.1. RIFSC and RISAx[edit source]
Default state for RIFSC and RISAx protection units:
- RIFSC RISUP protected peripherals:
- Non-secure
- Unprivileged
- CID filtering disabled
- RIFSC RIMU for bus master peripherals:
- Non-secure
- Unprivileged
- CID in RISUP CID inheritance mode. This implies a CID0 for all bus master peripherals as RISUP initial configuration is CID filtering disabled
- RISAF protected external memories:
- Base region0 only accessible by main processor (TDCID) in secure mode (CID1 Secure when Cortex-A35 is the main processor, CID2 secure when Cortex-M33 is the main processor).
- RISAB protected internal memories:
- No CID filtering,
- Security level depends on protected memory. Please refer to RISAB internal peripheral article.
3.2. RIF-Aware peripherals[edit source]
Default state for RIF-Aware peripherals:
RIF component | Secure level | Privilege level | CID filtering |
---|---|---|---|
GPIO | Secure | Unprivileged | CID filtering disabled |
EXTI | Non-secure | Unprivileged | CID filtering disabled |
FMC | Non-secure | Unprivileged | CID filtering disabled |
HPDMA | Non-secure | Unprivileged | CID filtering disabled |
IPCC | Non-secure | Unprivileged | CID filtering disabled |
PWR | Non-secure | Unprivileged | CID filtering disabled |
RCC | Non-secure | Unprivileged | CID filtering disabled |
RTC | Non-secure | Unprivileged | CID filtering disabled |
TAMP | Non-secure | Unprivileged | CID filtering disabled |
HSEM | Non-secure | Unprivileged | CID filtering disabled |
3.3. Minimal RIF configuration rules[edit source]
According to above statements, a minimal RIF configuration should be performed by the secure OS running on main processor (TDCID) to allow a correct and coherent execution for the embedded software:
- Secure level of GPIO should be configured to allow access to the HW execution context configuring and using them. For IO ports used by peripherals, non secure peripherals can use secure pins as well but secure peripherals cannot use non secure pins.
- RISAB memory blocks should be configured to allow access to the HW execution contexts using them.
- RISAF memory regions should be configured to allow access to the HW execution contexts using them.
- Secure level of some peripherals such as RNG should be set.
4. ROM code constraints[edit source]
The STM32MP25x lines ROM code which is running on Cortex-A35, shall be certified SESIP level3. This implies a certain number of security and isolation rules to guarantee ROM code execution:
- All secure and non secure HW resources required by ROM secure and/or non secure code shall be accessible respectively to the Cortex-A35 secure and/or non-secure each time the ROM code is executed (cold boot, application reset, low power exit).
- RIFSC RISUP configuration associated to ROM code resources shall allow Cortex-A35 access
- RISAB1&2 dedicated to SYSRAM protection shall allow Cortex-A35 access
- It shall not be possible to change RIF configuration of secure resources used by ROM code during its execution.
- When Cortex-M33 is the main processor (TDCID), RIFSC RISUP configuration associated to ROM code secure resources must be locked.
- No active bus master peripheral shall have same RIF configuration as Cortex-A35 secure context executing secure ROM code.
- If a RIFSC RIMU of a bus master peripheral is defined as Secure and CID1, its associated clock must be disabled during ROM code execution.
ROM code is checking RIFSC and RISAB1&2 (dedicated to SYSRAM protection) configurations. If one setting doesn't match ROM code requirements, ROM code stops its execution and goes in failure.
For more information, please refer to STM32MP2 ROM code resource isolation.
5. STM32MPU Embedded Software ecosystem configuration[edit source]
The ecosystem "*-ostl" configuration present in the External device tree is an example of a complete and secure ecosystem firewall configuration, it enables:
- Cortex-A35 and Cortex-M33 secure OSes
- Isolation between Cortex-A35 and Cortex-M33
- LTDC secure layer
- Authenticated Cortex-M33 co-processor
To do that, RIF is configured to assign peripherals and features to the different execution contexts with the following rules:
- The peripherals and resources used by Cortex-A35 secure OS are configured as secure, privileged, with CID filtering enabled on CID1
- The peripherals and resources used by Cortex-M33 secure OS are configured as secure, privileged with CID filtering enabled on CID2
- The peripherals and resources shared by Cortex-A35 and by Cortex-M33 secure OS are configured as secure, privileged and semaphore mode enabled for CID1/2 when possible, else TDCID only.
- The peripherals and resources used by Cortex-A35 non-secure OS are configured as non-secure, privileged, with CID filtering enabled on CID1
- The peripherals and resources used by Cortex-M33 non-secure OS are configured as non-secure, privileged, with CID filtering enabled on CID2
- The GPIO associated to one peripheral are usually configured with the same configuration as associated peripheral
- RCC and PWR system resources (resources common to several execution contexts) are configured to be controlled by the main processor (TDCID) secure OS.
- All peripherals used by ROM code are configured with access rights compliant with ROM code execution.
Regarding bus master peripherals, it is important to define the identity of their accesses by configuring their RIFSC RIMU. There are two possible methods:
- RIFSC RISUP CID inheritance: In that case, the master port accesses on the bus will have the same RIF CID attributes as the associated RISUP of the peripheral (default value).
- Define a specific CID for this RIMU through the RIFSC RIMC master attribute register. Notice that RISAF and RISAB configurations should be adapted to allow these peripherals' master port to access memory regions shared with the software component controlling it.
Regarding memories, RISAB and RISAF shall be configured according to product memory mapping.
- Memory regions exclusively used by a software component shall be configured to allow only access of the execution context (security level, privilege level and CID) running the software component
- DDR Memory regions used by secure OS can be defined as encrypted
- Memory regions shared between software components (for inter OS or processor communication) shall be configured to both execution contexts
Examples:
- In case of Cortex-A35 main processor boot from eMMC, SDMMC2 shall be accessible by:
- This implies to configure SDMMC2 RISUP in non-secure, privilege and CID1 (CID filtering enabled).
- Moreover, SDMMC2 shall be able to access any buffer allocated by the different software components. It shall behave as an extension of Cortex-A35 non-secure.
- This implies to configure associated RIMU in non-secure, unprivileged with CID inheritance.
- Associated device tree configuration is the following one:
&rifsc { st,protreg = < RIFPROT(STM32MP25_RIFSC_SDMMC2_ID, RIF_UNUSED, RIF_UNLOCK, RIF_NSEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN) >; st,rimu = < RIMUPROT(RIMU_ID(2), RIF_UNUSED, RIF_NSEC, RIF_PRIV, RIF_CIDSEL_P) >; };
- In case of Cortex-A35 main processor secure boot, some security peripherals like SAES or PKA shall be accessible by
- Associated device tree configuration is the following one:
&rifsc { st,protreg = < RIFPROT(STM32MP25_RIFSC_PKA_ID, RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN) RIFPROT(STM32MP25_RIFSC_SAES_ID, RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN) >; };
- In case of Cortex-A35 main processor secure boot and secondary secure OS running in Cortex-M33 secure context, some peripherals like SAES or PKA could be accessible by
- This implies to configure SAES and PKA RISUP in secure, privilege and shared between CID1 and CID2 thanks to RIF semaphore.
- Associated device tree configuration is the following one:
&rifsc { st,protreg = < RIFPROT(STM32MP25_RIFSC_PKA_ID, RIF_CID1_BF|RIF_CID2_BF, RIF_LOCK, RIF_SEC, RIF_PRIV, RIF_UNUSED, RIF_SEM_EN, RIF_CFEN) RIFPROT(STM32MP25_RIFSC_SAES_ID, RIF_CID1_BF|RIF_CID2_BF, RIF_LOCK, RIF_SEC, RIF_PRIV, RIF_UNUSED, RIF_SEM_EN, RIF_CFEN) >; };
OSTL RIF ecosystem configuration for ST reference board is available in external device tree repository.
6. STM32MPU Embedded Software upstream configuration[edit source]
The upstream configuration is the one present in the trusted OS repository (Either https://github.com/STMicroelectronics/optee_os.git or https://github.com/STMicroelectronics/trusted-firmware-m.git. This configuration is very permissive and should be used for development purposes. For that, this minimal configuration is following these rules:
- Secure resources (peripherals and memory regions) used by either Cortex-A35 or Cortex-M33 secure OS are defined as secure. CID filtering may be enabled
- Access to peripherals (and associated IOs) unused by secure OSes are defined as non-secure, unprivileged and CID filtering disabled
- Bus master peripherals accesses remain at their default value (non-secure, unprivileged and CID inheritance)
- Memory regions unused by secure OSes are configured to allow accesses from any bus master peripherals (non-secure, unprivileged, RW for all CID)
7. How to configure RIF[edit source]
7.1. RIF configuration ownership[edit source]
RIF main configuration is under the TDCID responsibility. CID filtering configuration registers can't be accessed by other masters. That means RIF configuration should be done by the secure OS running on main processor.
Nevertheless, almost all RIF registers are in read for all, that means any execution context can read them to check if it can access a resource or not.
It is also possible to delegate some sub-configurations to some execution contexts. For examples:
- Secure master having access to a resource can change its security level
- Privileged master having access to a resource can change its privilege level
- Memory regions can be delegated to an owner (defined by CID, secure and privilege levels) that can define new secure/privilege access rights and sub-regions. It is useful for memory sharing management.
7.2. How to generate RIF configuration[edit source]
The RIF configuration could be done via STM32CubeMX graphical tool:
- Peripheral assignment between the different execution contexts allows to generate RIFSC RISUP configuration
- RIF-aware configuration panels allow to assign each feature to the different execution contexts to generate associated configuration
- RIF panel provides a way to configure the different master interfaces and generate RIFSC RIMU configuration, to create the different memory regions and to generate associated RISAF, RISAB and RISAL
The advantage of using STM32CubeMX is that consistencies between the different RIF components and between the different software components running on the platform including ROM code are managed. RIF peripheral protection is extended to associated IOs, clock and reset. To guarantee the coherency between all the software components, CubeMX generates device tree files for all software components which include RIF and memory and clock tree configuration.
7.3. RIF drivers bindings[edit source]
For more information about RIF configuration in device tree files please refer to device tree configuration pages:
- RIFSC : RIFSC device tree configuration
- RISAF : RISAF device tree configuration
- RISAB : RISAB device tree configuration
- GPIO : GPIO device tree configuration
- RCC : Clock device tree configuration
- PWR : How to configure PWR Wake-up pins
- FMC : FMC device tree configuration
- IPCC : IPCC device tree configuration
- TAMP : TAMP device tree configuration
- RTC : RTC device tree configuration
- HPDMA : HPDMA device tree configuration