How to customize OpenSTDroid distribution

Revision as of 15:46, 18 July 2024 by Registered User (Created page with "<noinclude>{{ApplicableFor |MPUs list=STM32MP25x |MPUs checklist=STM32MP13x, STM32MP15x, STM32MP25x }}</noinclude> This articles explain how you can customize the OpenSTDroid distribution. It's intent to be used by distribution package users. == Prerequisites == The environment used must have been installed using the Distribution Package adapted to your microprocessor device. See Which_STM32MPU_Embedded_Software_Package_for_Android_better_suits_your_needs#Distributio...")
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)
Applicable for STM32MP25x lines

This articles explain how you can customize the OpenSTDroid distribution. It's intent to be used by distribution package users.

1. Prerequisites[edit source]

The environment used must have been installed using the Distribution Package adapted to your microprocessor device. See Distribution_Package.

To execute the following instructions, go to your distribution root directory and initialize your environment:

 source build/envsetup.sh
 lunch aosp_<BoardId>-userdebug

Example for STM32MP257F-EV1 Evaluation board More info green.png:

 lunch aosp_eval-userdebug

2. Layout configuration[edit source]

The memory layout can be configure through the android_layout.config file located in device/stm/<STM32Series>/layout (example: device/stm/stm32mp2/layout for STM32MP2 series). It contains all the necessary data.

When changes are complete, reload the environment:

 source build/envsetup.sh
 lunch aosp_<BoardId>-userdebug

Example for STM32MP257F-EV1 Evaluation board More info green.png:

 lunch aosp_eval-userdebug

2.1. Memory size[edit source]

To adapt your build to your memory size, change the PART_MEMORY_SIZE parameter in the android_layout.config file. PART_MEMORY_SIZE values can be:

  • 4GiB (4 Gbytes)
  • 8GiB (8 Gbytes)

Its value must match the parameter of name PART_<Memory size>_MEMORY_MAX_SIZE, located at the end of the file.

It might need to be changed. For example, if the memory type was "sd" (microSD card):

PART_8GiB_MEMORY_MAX_SIZE 7432M x1 sd

The 7432M must be adapted if your memory size is lower that the value defined.

To find the correct value, execute the command below:

 sgdisk -p /dev/mmcblk<x>

It displays the following information:

Disk /dev/mmcblk0: 15433728 sectors, 7.4 GiB
Logical sector size: 512 bytes
Disk identifier (GUID): XXXXXXXX-XXXX-XXXX-XXXX-XXXXXXXXXXX
Partition table holds up to 128 entries
First usable sector is 34, last usable sector is 15433694
Partitions will be aligned on 2-sector boundaries
Total free space is 0 sectors (0 bytes)

The first line show the microSD card available size: here 15433728 sectors.

To calculate the size in MiB (Mbytes):

size = (NbSectors * SectorSize) / 1024 / 1024
In this example: (15433728 * 512) / 1024 / 1024 = 7536 MiB

Report this value in PART_8GiB_MEMORY_MAX_SIZE:

PART_8GiB_MEMORY_MAX_SIZE 7536M x1 sd

For more details, refer to the README file located in the same folder.

2.2. Partition size[edit source]

To change the size of a partition, modify it in the android_layout.config file.

Adapt the following parameters:

PART_<NAME> <PART_SIZE> <PART_NB> <PART_LABEL> <PART_SUFFIX> <PART_ENABLE>
NAME: name of the local variable (last partition MUST start with PART_LAST_)
PART_SIZE: as xxxMB or xxxKB or xxxGB
PART_NB: number of instances of partition (x1 or x2)
PART_LABEL: name of the partition label
PART_SUFFIX (optional): name of the suffix in case PART_NB equal x2 (_a/_b by default)
PART_ENABLE (optional): device for which the partition is only applicable (sd)

Then adapt every FlashLayout_*.tsv under device/stm/<STM32Series>/layout/programmer (example: device/stm/stm32mp2/layout/programmer/ for STM32MP2 series) to match your changes.

To do this, use the device/stm/<STM32Series>/scripts/layout/build_tsv.py script (example: device/stm/stm32mp2/scripts/layout/build_tsv.py for STM32MP2 series).

2.3. Add a new partition[edit source]

To add a new partition (ex: named test), first add it in the android_layout.config file.

Add the following parameters:

PART_TEST <PART_SIZE> <PART_NB> test <PART_SUFFIX> <PART_ENABLE>
PART_SIZE: as xxxMB or xxxKB or xxxGB
PART_NB: number of instances of partition (x1 or x2)
PART_SUFFIX (optional): name of the suffix in case PART_NB equal x2 (_a/_b by default)
PART_ENABLE (optional): device for which the partition is only applicable (sd)

From this stage, the format_device and provision_device scripts can be used to flash the new partition (an image, named test.img must be available in the out/target/product/<BoardId> directory (example out/target/product/eval for STM32MP257F-EV1 Evaluation board More info green.png).

Then adapt device/stm/<STM32Series>/scripts/layout/build_tsv.py script (example: device/stm/stm32mp2/scripts/layout/build_tsv.py for STM32MP2 series):

  • add PART_TEST in android_allowed_part list
  • add "test": {"opt": "PE", "type": "FileSystem\t", "id": None}, in the tsv_dict dictionary

The partition type (FileSystem in the example) can be adapted depending on your needs: see more details in the flashlayout partition types.

Finally adapt every FlashLayout_*.tsv under device/stm/<STM32Series>/layout/programmer to match your changes (example: device/stm/stm32mp2/layout/programmer/FlashLayout_*.tsv for STM32MP2 series).

To do this, use the updated device/stm/<STM32Series>/scripts/layout/build_tsv.py script.

From this stage, the flash-device script can be used.

3. Modification of the OpenSTDroid distribution[edit source]

The list of changes performed during the <STM32Series>setup (example: stm32mp2setup for STM32MP2 series) can be adapted by modifying the android_patch.config available in device/stm/<STM32Series>/patch/android/ file (example: device/stm/stm32mp2/patch/android/android_patch.config for STM32MP2 series).

First retrieve the original configuration:

 <STM32Series>clear -p

Then adapt the file (add or/and remove list of commits and patches).

Some rules must be respected for adding patches:

  • Patch files shall be added with the relative path to device/stm/<STM32Series>/patch/android/ directory.
  • Patches shall be added in the correct order.

Some rules must the respected for removing patches:

  • Test the new configuration on the targeted directory by applying the patches manually (generate them again if required).
  • Do not remove patches and commits with do not modify mention.

When this is done, apply the new configuration:

 <STM32Series>setup

Then rebuild the distribution to take into account your changes:

 make -j