RCC internal peripheral

Revision as of 14:59, 2 January 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the RCC peripheral and its main features,
  • indicate the peripheral instances assignment at boot time and their assignment at runtime (including whether instances can be allocated to secure contexts),
  • list the software frameworks and drivers managing the peripheral,
  • explain how to configure the peripheral.

2. Peripheral overview[edit source]

The RCC peripheral is used to manage the clock and reset generation for the complete circuit. The RCC gets several internal and external oscillators. They are used as clock sources for the hardware blocks, either directly or indirectly, via the PLLs that allow to achieve high frequencies.

The different features of RCC could be assigned to the execution contexts of the platform:

  • On STM32MP13x lines More info.png, each resource/sub-function is allocated either to the secure world or to the non-secure world via bits in the RCC_SECCFGR register.
  • On STM32MP15x lines More info.png, there are two levels of security, which are controlled via two bits in the RCC_TZCR register (only accessible in secure mode):
  • TZEN allows to set some RCC registers in secure mode, in particular registers for configuring PLL1 and PLL2, in order to secure a TrustZone perimeter for the Cortex®-A7 secure core and its peripherals.
  • MCKPROT allows extending the TZEN secure clock control perimeter to PLL3 and to the MCU subsystem, so to the Cortex®-M4 and its bus clock.
  • On STM32MP2 series, RCC is a RIF-aware peripheral. That means
  • Dedicated RCC features are protected by RIF protection embedded in RCC following peripheral firewall rules described in Resource Isolation Framework overview
  • Internal peripheral reset and clock gating control inherit from RIFSC configuration
Note:
Clock gating registers of system resources (Internal RAM, RIF-aware peripherals) are protected by RCC RIF protection (no RIFSC inheritance). This allows to manage automatic clock gating according to either processor low power state or system low power state. Indeed, when a peripheral is shared, it should always be available to any execution context at any time.

Please note that all RCC registers can be read from any execution context.

Refer to the STM32 MPU reference manuals for the complete list of features, and to the software frameworks and drivers, introduced below, to see which features are implemented.

3. Peripheral usage[edit source]

This chapter is applicable in the scope of the OpenSTLinux BSP running on the Arm® Cortex®-A processor(s), and the STM32CubeMPU Package running on the Arm® Cortex®-M processor.

3.1. Boot time assignment[edit source]

3.1.1. On STM32MP1 series[edit source]

The RCC is used by all the boot components: the ROM code, the FSBL, the SSBL and up to the Linux® kernel. Each component is able to reset and gate internal peripherals

FSBL is responsible to make a minimal clock tree initialization for loading the next boot stages. Then the main clock tree initialization step is performed by the OP-TEE secure OS: it consists in configuring all the input clocks, the PLLs and the clock sources that are selected as kernel clocks for all peripherals. The whole clock tree configuration is carried out by the device tree (see STM32MP13 clock tree and STM32MP15 clock tree).


Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Power & Thermal RCC RCC

3.1.2. On STM32MP2 series[edit source]

In Cortex-A main processor mode, the RCC is used by all the boot components: the ROM code, the Cortex-A FSBL, the Secure OS, the SSBL and the Linux® kernel. Each SW component is able to reset and gate internal peripherals assigned to it.

ROM code clock tree configuration is fixed, mainly based on HSI internal oscillator. The goal is to configure in a safe mode the platform to load, authenticate and execute the FSBL.

The Cortex-A FSBL is responsible to make a minimal clock tree initialization for loading the next boot stages. Then the main clock tree initialization step is performed by the OP-TEE secure OS: it consists in configuring all the input clocks, the PLLs and the clock sources that are selected as kernel clocks for all peripherals. The whole clock tree configuration is carried out by the device tree (see STM32MP25 clock tree).


Click on How to.png to expand or collapse the legend...

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
Power & Thermal RCC Info.png RCC Shareable at internal peripheral level thanks to the RIF: see the boot time allocation per feature

The below table shows the possible boot time allocations for the features of the RCC instance.

Feature Boot time allocation Info.png Comment
Cortex-A35
secure
(ROM code)
Cortex-A35
secure
(TF-A BL2)
Cortex-A35
non-secure
(U-Boot)
FCALC
SYSRST
BOOT_STDB
RDCR
SYSCLK
CPU1_RES
CPU2_RES
CPU3_RES
DEBUG_CFGR
SYSRAM_CFGR
VDERAM_CFGR
RETRAM_CFGR
BKPSRAM_CFGR
SRAM1_CFGR
SRAM2_CFGR
LPSRAM1_CFGR
LPSRAM2_CFGR
LPSRAM3_CFGR
HPDMA1_CFGR
HPDMA2_CFGR
HPDMA3_CFGR
LPDMA_CFGR
IPCC1_CFGR
IPCC2_CFGR
HSEM_CFGR
GPIOA_CFGR
GPIOB_CFGR
GPIOC_CFGR
GPIOD_CFGR
GPIOE_CFGR
GPIOF_CFGR
GPIOG_CFGR
GPIOH_CFGR
GPIOI_CFGR
GPIOJ_CFGR
GPIOK_CFGR
GPIOZ_CFGR
RTC_CFGR
BSEC_CFGR
DDRC_CFGR
PLL3_CFGR
SYSCPU1_CFGR
MCO1_CFGR
MCO2_CFGR
OSPI1_CFGR
OSPI2_CFGR
FMC_CFGR
HSI_MON

3.2. Runtime assignment[edit source]

3.2.1. On STM32MP1 series[edit source]

The Arm® Cortex®-A7 secure core controls all the secure registers through the RCC OP-TEE driver. The access to some secure registers from the Cortex®-A7 non-secure core can be achieved via SCMI requests.

3.2.1.1. On STM32MP13x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP13 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Power & Thermal RCC RCC
3.2.1.2. On STM32MP15x lines More info.png[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Power & Thermal RCC RCC

3.2.2. On STM32MP25x lines More info.png[edit source]

In Cortex-A main processor mode, the Cortex-A secure OS OP-TEE controls all the RCC system resources, i.e. resources which are shared between execution contexts or between different internal peripherals, like oscillators, PLLs, root clocks or reset and clock gating of RIF-aware peripherals. The Cortex-A secure OS OP-TEE provides SCMI services to access system resources. For RIFSC RISUP protected internal peripheral, each SW component can directly access RCC registers to control reset and clock gating.


Click on How to.png to expand or collapse the legend...

STM32MP25 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP25 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
Power & Thermal RCC Info.png RCC OP-TEE

TF-A BL31

Shareable at internal peripheral level thanks to the RIF: see the runtime allocation per feature

The below table shows the possible runtime allocations for the features of the RCC instance.

Feature Runtime allocation Info.png Comment
Cortex-A35
secure
(OP-TEE /
TF-A BL31)
Cortex-A35
non-secure
(Linux)
Cortex-M33
secure
(TF-M)
Cortex-M33
non-secure
(STM32Cube)
Cortex-M0+
Warning.png
(STM32Cube)
FCALC OP-TEE
SYSRST OP-TEE
TF-A BL31
BOOT_STDB OP-TEE
TF-A BL31
RDCR OP-TEE
TF-A BL31
SYSCLK OP-TEE
TF-A BL31
CPU1_RES OP-TEE
TF-A BL31
CPU2_RES if TZ_EN if TZ_DIS
CPU3_RES OP-TEE
DEBUG_CFGR OP-TEE
SYSRAM_CFGR OP-TEE
TF-A BL31
VDERAM_CFGR OP-TEE
RETRAM_CFGR OP-TEE
TF-A BL31
BKPSRAM_CFGR OP-TEE
TF-A BL31
SRAM1_CFGR OP-TEE
SRAM2_CFGR OP-TEE
LPSRAM1_CFGR OP-TEE
LPSRAM2_CFGR OP-TEE
LPSRAM3_CFGR OP-TEE
HPDMA1_CFGR OP-TEE
HPDMA2_CFGR OP-TEE
HPDMA3_CFGR OP-TEE
LPDMA_CFGR OP-TEE
IPCC1_CFGR OP-TEE
IPCC2_CFGR OP-TEE
HSEM_CFGR OP-TEE
GPIOA_CFGR OP-TEE
TF-A BL31
GPIOB_CFGR OP-TEE
TF-A BL31
GPIOC_CFGR OP-TEE
TF-A BL31
GPIOD_CFGR OP-TEE
TF-A BL31
GPIOE_CFGR OP-TEE
TF-A BL31
GPIOF_CFGR OP-TEE
TF-A BL31
GPIOG_CFGR OP-TEE
TF-A BL31
GPIOH_CFGR OP-TEE
TF-A BL31
GPIOI_CFGR OP-TEE
TF-A BL31
GPIOJ_CFGR OP-TEE
TF-A BL31
GPIOK_CFGR OP-TEE
TF-A BL31
GPIOZ_CFGR OP-TEE
TF-A BL31
RTC_CFGR OP-TEE
TF-A BL31
BSEC_CFGR OP-TEE
TF-A BL31
DDRC_CFGR OP-TEE
TF-A BL31
PLL3_CFGR OP-TEE
SYSCPU1_CFGR OP-TEE
TF-A BL31
MCO1_CFGR OP-TEE
MCO2_CFGR OP-TEE
OSPI1_CFGR OP-TEE
OSPI2_CFGR OP-TEE
FMC_CFGR OP-TEE
HSI_MON OP-TEE

4. Software frameworks and drivers[edit source]

Below are listed the software frameworks and drivers managing the RCC peripheral for the embedded software components listed in the above tables.

See also the SCMI overview.

5. How to assign and configure the peripheral[edit source]

The peripheral assignment can be done via the STM32CubeMX graphical tool (and manually completed if needed).

This tool also helps to configure the peripheral:

  • partial device trees (pin control and clock tree) generation for the OpenSTLinux software components,
  • HAL initialization code generation for the STM32CubeMPU Package.

The configuration is applied by the firmware running in the context in which the peripheral is assigned.

For configuration of reset part of RCC, refer to Reset device tree configuration.

For configuration of clock part of RCC, the STM32CubeMX tool allows configuring the clock tree and integrates all the information documented in the STM32 MPU reference manuals. It is highly recommended to use it to generate your device tree as explained in:

On STM32MP15x lines More info.png, the RCC security level differs for each boards and is defined by RCC compatible in OP-TEE device tree:

  • "st,stm32mp1-rcc-secure": sets TZEN to 1 and MCKPROT to 0
  • "st,stm32mp1-rcc": sets TZEN to 0 and MCKPROT to 0

The STMicroelectronics STM32MP15x lines More info.png boards use TZEN=0 to avoids issue with shared resources on secured I2C.

6. How to go further[edit source]

The RCC is interfaced with the HDP internal peripheral, thus offering the flexibility to monitor the main RCC state signals on the debug pins.

Please refer to the STM32MPU reference manuals for the full list of signals that can be monitored.

7. References[edit source]