This article gives information about the Linux® V4L2 video codec framework.
1. Framework purpose[edit source]
The V4L2 Linux kernel framework[1] allows the control of video hardware codecs in order to decode and encode compressed video contents such as H264, VP8 or JPEG video bitstreams.
This could be typically used, with the help of other Linux multimedia frameworks, and applications, to play local videos, stream video contents, make a video recording or even remotely stream video compressed images from the camera sensor.
2. System overview[edit source]
2.1. Component description[edit source]
- media-ctl (User space)
A V4L2 utility relying on Media Controller Linux kernel interface[2] aiming to configure, and link each sub devices composing the camera subsystem in order to configure it.
- Application (User space)
Any application relying on V4L2 Linux kernel interface[3] or libv4l abstraction layer. GStreamer framework provides such application.
- V4L2 utilities (User space)
A set of tools to test, configure, and use the whole camera subsystem, including the external camera sensor, and the camera interface. v4l2-ctl is one of the most useful utility.
- V4L2 libraries (libv4l) (User space)
A set of libraries on top of the V4L2 Linux kernel interface[3] which abstract the kernel interface in order to simplify, keep compatibility or add some hooks between V4L-based applications, and the V4L2 kernel interface.
- V4L2 core (Kernel space)
This layer represents the standard Linux kernel V4L2 Framework.
- hantro_vpu (Kernel space)
This V4L2 Linux device driver handles the VDEC hardware block and the VENC hardware block.
- VDEC (Hardware)
The Video DECoder hardware block.
- VENC (Hardware)
The Video ENCoder hardware block.
2.2. APIs description[edit source]
The V4L2 userland API is documented in the Linux Media subsystem documentation[3]
More specifically, the V4L2 video memory-to-memory userland API is documented in the chapter[4]
The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux kernel documentation[5]
The Media Controller API is documented in the Linux Media subsystem documentation[2]
3. Configuration[edit source]
3.1. Kernel configuration[edit source]
The STM32 hantro_vpu driver is enabled by default in STMicroelectronics deliveries.
Nevertheless, this could not be the case when using the upstream kernel version. In this case, the hantro_vpu V4L2 driver with its STM32MP25 backend can be enabled using Linux kernel menuconfig tool:
[*] Device Drivers ---> [*] Multimedia support ---> [*] Media drivers ---> [*] Media platform devices ---> [*] Hantro VPU driver ---> [*] Hantro STM32MP25 support
3.2. Device tree configuration[edit source]
Refer to VDEC device tree configuration and VENC device tree configuration articles for Linux kernel device tree details.
4. How to use the framework[edit source]
The use cases described here are enabled using media-ctl, v4l2-ctl, gst-launch or gst-play command line utilities.
4.1. List the video codec devices and their capabilities[edit source]
List all the available video devices using v4l2-ctl --list-devices option:
v4l2-ctl --list-devices
st,stm32mp25-vdec-dec (platform: hantro-vpu): /dev/video0 /dev/media0 st,stm32mp25-venc-enc (platform: hantro-vpu): /dev/video1 /dev/media1
If several devices are available, use -d option after any v4l2-ctl commands to target a specific device. If -d option is not specified, /dev/video0 is targeted by default.
In order to have information on a specific device, use -D option.
/dev/video0 is the video decoder device:
v4l2-ctl -d /dev/video0 -D
Driver Info:
Driver name : hantro-vpu
Card type : st,stm32mp25-vdec-dec
Bus info : platform: hantro-vpu
Driver version : 6.1.28
Capabilities : 0x84204000
Video Memory-to-Memory Multiplanar
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04204000
Video Memory-to-Memory Multiplanar
Streaming
Extended Pix Format
Media Driver Info:
Driver name : hantro-vpu
Model : hantro-vpu
Serial :
Bus info : platform: hantro-vpu
Media version : 6.1.28
Hardware revision: 0x00000000 (0)
Driver version : 6.1.28
Interface Info:
ID : 0x0300000c
Type : V4L Video
Entity Info:
ID : 0x00000001 (1)
Name : st,stm32mp25-vdec-dec-source
Function : V4L2 I/O
Pad 0x01000002 : 0: Source
Link 0x02000008: to remote pad 0x1000004 of entity 'st,stm32mp25-vdec-dec-proc' (Video Decoder): Data, Enabled, Immutable
/dev/video1 is the encoder device:
v4l2-ctl -d /dev/video1 -D
Driver Info:
Driver name : hantro-vpu
Card type : st,stm32mp25-venc-enc
Bus info : platform: hantro-vpu
Driver version : 6.1.28
Capabilities : 0x84204000
Video Memory-to-Memory Multiplanar
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04204000
Video Memory-to-Memory Multiplanar
Streaming
Extended Pix Format
Media Driver Info:
Driver name : hantro-vpu
Model : hantro-vpu
Serial :
Bus info : platform: hantro-vpu
Media version : 6.1.28
Hardware revision: 0x00000000 (0)
Driver version : 6.1.28
Interface Info:
ID : 0x0300000c
Type : V4L Video
Entity Info:
ID : 0x00000001 (1)
Name : st,stm32mp25-venc-enc-source
Function : V4L2 I/O
Pad 0x01000002 : 0: Source
Link 0x02000008: to remote pad 0x1000004 of entity 'st,stm32mp25-venc-enc-proc' (Video Encoder): Data, Enabled, Immutable
4.2. Get the supported compressed format, pixel format and resolution[edit source]
Use v4l2-ctl --list-formats-out-ext option to get the supported compressed formats and resolutions supported by the decoder:
v4l2-ctl --list-formats-out-ext ioctl: VIDIOC_ENUM_FMT [0]: 'VP8F' (VP8 Frame, compressed) Size: Stepwise 96x96 - 4080x4080 with step 16/16 [1]: 'S264' (H.264 Parsed Slice Data, compressed) Size: Stepwise 96x96 - 4080x4080 with step 16/16
Both VP8 and H264 bitstream decoding are supported up to 4080x4080.
Use --list-formats-ext option to get the supported output pixel formats:
v4l2-ctl -d /dev/video0 --list-formats-ext ioctl: VIDIOC_ENUM_FMT [0]: 'NV12' (Y/UV 4:2:0)
Only YUV420 semi-planar is supported in output of decoder.
Informations are also available at GStreamer level by inspecting v4l2slvp8dec and v4l2slh264dec decoder elements using commands:
gst-inspect-1.0 --no-colors v4l2slvp8dec [...] Pad Templates: SINK template: 'sink' Availability: Always Capabilities: video/x-vp8 SRC template: 'src' Availability: Always Capabilities: video/x-raw format: { (string)NV12, (string)YUY2, (string)NV12_4L4, (string)NV12_32L32, (string)NV12_16L32S, (string)I420, (string)P010_10LE, (string)RGB16, (string)BGRx, (string)RGBx, (string)xBGR, (string)xRGB } width: [ 1, 2147483647 ] height: [ 1, 2147483647 ] framerate: [ 0/1, 2147483647/1 ] [...]
gst-inspect-1.0 --no-colors v4l2slh264dec [...] Pad Templates: SINK template: 'sink' Availability: Always Capabilities: video/x-h264 SRC template: 'src' Availability: Always Capabilities: video/x-raw format: { (string)NV12, (string)YUY2, (string)NV12_4L4, (string)NV12_32L32, (string)NV12_16L32S, (string)I420, (string)P010_10LE, (string)RGB16, (string)BGRx, (string)RGBx, (string)xBGR, (string)xRGB } width: [ 1, 2147483647 ] height: [ 1, 2147483647 ] framerate: [ 0/1, 2147483647/1 ] [...]
Same can be applied for the encoder:
v4l2-ctl -d /dev/video1 --list-formats-out-ext ioctl: VIDIOC_ENUM_FMT [0]: 'NV12' (Y/UV 4:2:0) [1]: 'YM12' (Planar YUV 4:2:0 (N-C)) [2]: 'NM12' (Y/UV 4:2:0 (N-C)) [3]: 'YUYV' (YUYV 4:2:2) [4]: 'UYVY' (UYVY 4:2:2) [5]: 'RGBP' (16-bit RGB 5-6-5) [6]: 'XR24' (32-bit BGRX 8-8-8-8) [7]: 'BGR4' (32-bit BGRA/X 8-8-8-8) [8]: 'XB24' (32-bit RGBX 8-8-8-8) [9]: 'RX24' (32-bit XBGR 8-8-8-8) [10]: 'BX24' (32-bit XRGB 8-8-8-8) [11]: 'RGB4' (32-bit A/XRGB 8-8-8-8)
Encoder can be fed with YUV420 semi-planar and YUV420 planar, YUV422 coplanar, RGB565 16 bits and RGB 32 bits pixels formats.
v4l2-ctl -d /dev/video1 --list-formats-ext [0]: 'JPEG' (JFIF JPEG, compressed) Size: Stepwise 96x32 - 8176x8176 with step 16/16 [1]: 'VP8F' (VP8 Frame, compressed) Size: Stepwise 96x96 - 4080x4080 with step 16/16
Encoder can generate JPEG up to 8176 and VP8 bitstream up to 4080.
Informations are also available at GStreamer level by inspecting v4l2slvp8enc and v4l2jpegenc encoder elements using command:
gst-inspect-1.0 --no-colors v4l2slvp8enc [...] Pad Templates: SINK template: 'sink' Availability: Always Capabilities: video/x-raw format: { (string)NV12, (string)YUY2, (string)NV12_4L4, (string)NV12_32L32, (string)NV12_16L32S, (string)I420, (string)P010_10LE, (string)RGB16, (string)BGRx, (string)RGBx, (string)xBGR, (string)xRGB } width: [ 1, 2147483647 ] height: [ 1, 2147483647 ] framerate: [ 0/1, 2147483647/1 ] SRC template: 'src' Availability: Always Capabilities: video/x-vp8 [...]
gst-inspect-1.0 --no-colors v4l2jpegenc [...] Pad Templates: SINK template: 'sink' Availability: Always Capabilities: video/x-raw format: { (string)I420, (string)YUY2, (string)UYVY, (string)RGB16, (string)BGRA, (string)RGBx, (string)xBGR, (string)ARGB, (string)xRGB, (string)BGRx, (string)NV12 } width: [ 1, 32768 ] height: [ 1, 32768 ] framerate: [ 0/1, 2147483647/1 ] SRC template: 'src' Availability: Always Capabilities: image/jpeg parsed: true [...]
4.3. Playing/streaming a video[edit source]
When using high level utilities such as gst-play or complex GStreamer bins such as playbin, playbin3 or decodebin, decodebin3, hardware acceleration is abstracted to user and automatically selected to achieve the best level of performances.
Refer to gst-play GStreamer command line utility, for examples of "how to play audio/video files" or "how to stream content on STM32 board".
4.4. Encoding a video[edit source]
When using complex GStreamer bins such as encodebin or encodebin2, hardware acceleration is abstracted to user and automatically selected to achieve the best level of performances.
Here is an example with a local encoding of a 10s video test pattern in VP8:
gst-launch-1.0 videotestsrc num-buffers=300 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-vp8" ! matroskamux ! filesink location=v_vp8_640x480_30fps.webm
[...]
Got EOS from element "pipeline0".
Execution ended after 0:00:01.229040368
[...]
Play back the file to check encoded content:
gst-play-1.0 v_vp8_640x480_30fps.webm [...] 0:00:10.0 / 0:00:10.0 Reached end of play list.
4.5. Controlling encoder[edit source]
It is interesting to tune quality, bitrate and I frames refresh to better fit to application requirements. Local video recording from camera requires good image quality with variable bitrate to adapt to image complexity while video streaming or visiophony requires bandwidth respect with constant bitrate dealing with quality tradeoff.
There are no yet common controls at encodebin level to tune quality, bitrate and key frames refresh rate, to do so, the encoder element must be directly controlled:
gst-inspect-1.0 --no-colors v4l2slvp8enc [...] Element Properties: bitrate : Set bitrate target flags: readable, writable Unsigned Integer64. Range: 0 - 4294967295 Default: 100000 keyframe-interval : Interval between keyframes flags: readable, writable Integer. Range: 0 - 2147483647 Default: 30 max-quality : Set upper quality limit (lower number equates to higher quality but more bits) flags: readable, writable Integer. Range: 0 - 63 Default: 63 media-device : Path to the media device node flags: readable, writable String. Default: "/dev/media2" min-force-key-unit-interval: Minimum interval between force-keyunit requests in nanoseconds flags: readable, writable Unsigned Integer64. Range: 0 - 18446744073709551615 Default: 0 min-quality : Set lower quality limit (lower number equates to higher quality but more bits) flags: readable, writable Integer. Range: 0 - 63 Default: 0
For quality: the less value is, better is the quality. Default keyframe interval is 30, ie one entire key frame generated every 1s at 30fps.
encodebin can still be used while tuning encoder with a custom "profile=<video> | element-properties,<property=value>" property. Here are some example to tune quality.
#best quality gst-launch-1.0 -e videotestsrc num-buffers=300 horizontal-speed=3 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-vp8|element-properties,min-quality=0,max-quality=0" ! matroskamux ! filesink location=v_vp8_640x480_30fps_best.webm
#worst quality gst-launch-1.0 -e videotestsrc num-buffers=300 horizontal-speed=3 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-vp8|element-properties,min-quality=63,max-quality=63" ! matroskamux ! filesink location=v_vp8_640x480_30fps_worst.webm
ls -s v_vp8_640x480_30fps_best.webm v_vp8_640x480_30fps_worst.webm 14132 v_vp8_640x480_30fps_best.webm 3804 v_vp8_640x480_30fps_worst.webm
We can see that quality impacts by 4 the size of encoded video.
Here are some examples to tune key-frame refresh rate:
gst-launch-1.0 -e videotestsrc num-buffers=300 horizontal-speed=3 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-vp8|element-properties,keyframe-interval=100" ! matroskamux ! filesink location=v_vp8_640x480_30fps_key_3s.webm
gst-launch-1.0 filesrc location=v_vp8_640x480_30fps_key_3s.webm ! matroskademux ! identity silent=false ! fakesink -v 2>&1 | grep chain | grep -v delta-unit
/GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (47070 bytes, dts: none, pts: 0:00:00.000000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04040 discont tag-memory , meta: none) 0x17c547e0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11495 bytes, dts: none, pts: 0:00:03.033000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x17c546c0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11706 bytes, dts: none, pts: 0:00:06.067000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x17c545a0
3 key-frames for 10s video which conforms to one key-frames every 100 frames at 30fps.
gst-launch-1.0 -e videotestsrc num-buffers=300 horizontal-speed=3 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin profile="video/x-vp8|element-properties,keyframe-interval=30" ! matroskamux ! filesink location=v_vp8_640x480_30fps_key_1s.webm
gst-launch-1.0 filesrc location=v_vp8_640x480_30fps_key_1s.webm ! matroskademux ! identity silent=false ! fakesink -v 2>&1 | grep chain | grep -v delta-unit
/GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (47070 bytes, dts: none, pts: 0:00:00.000000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04040 discont tag-memory , meta: none) 0x217186c0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (19478 bytes, dts: none, pts: 0:00:01.033000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217187e0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11813 bytes, dts: none, pts: 0:00:02.067000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x21718a20 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11688 bytes, dts: none, pts: 0:00:03.100000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217186c0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11627 bytes, dts: none, pts: 0:00:04.133000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217185a0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11576 bytes, dts: none, pts: 0:00:05.167000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x21718a20 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11602 bytes, dts: none, pts: 0:00:06.200000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217186c0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11785 bytes, dts: none, pts: 0:00:07.233000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217185a0 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11515 bytes, dts: none, pts: 0:00:08.267000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x21718a20 /GstPipeline:pipeline0/GstIdentity:identity0: last-message = chain ******* (identity0:sink) (11637 bytes, dts: none, pts: 0:00:09.300000000, duration: 0:00:00.033333333, offset: -1, offset_end: -1, flags: 000 04000 tag-memory , meta: none) 0x217187e0
10 key-frames for 10s video which conforms to one key-frames every 30 frames at 30fps.
4.6. Audio/Video encoding[edit source]
encodebin can handle both video and audio track by connecting an audio source to audio_0 encodebin pad while specifying a profile which handles both audio & video like webm profile which will encode video to VP8 format and audio to Vorbis format: Here is an example with an audio tone generator:
gst-launch-1.0 videotestsrc num-buffers=300 ! video/x-raw, width=640, height=480, framerate=30/1 ! encodebin name=encoder profile="webm" ! filesink location=av_vp8_640x480_vorbis.webm \ audiotestsrc num-buffers=400 ! encoder.audio_0
Use gst-discoverer to check back encoded content:
gst-discoverer-1.0 av_vp8_640x480_vorbis.webm [...] container #0: WebM video #1: VP8 Width: 640 Height: 480 Depth: 24 Frame rate: 30/1 audio #2: Vorbis Channels: 1 (unknown layout) Sample rate: 44100 Depth: 32 Bitrate: 80000
4.7. Pictures streaming over network[edit source]
Refer to How to stream RAW camera over network article to get some examples on how to stream camera content over network using encodebin.
5. How to trace and debug[edit source]
5.1. How to monitor[edit source]
5.1.1. Check of devicetree configuration[edit source]
Here are some commands to verify that DCMIPP is enabled, check which camera sensor is used and log other details about devicetree configuration:
echo "#!/bin/bash" > dtdumpentry.sh;echo "hexdump -e '\"=\"' -e '20/1 \"%c\"\"\t\"' -e '20/1 \"%02x\"\"\n\"' \$1" >> dtdumpentry.sh;chmod +x dtdumpentry.sh echo "#!/bin/bash" > dtdump.sh;echo "find \$1* -type f -print0 -exec ./dtdumpentry.sh {} \;" >> dtdump.sh;chmod +x dtdump.sh
rm devicetree.txt echo "[devicetree]" >> devicetree.txt echo "|-[dcmipp]" >> devicetree.txt ./dtdump.sh /proc/device-tree/soc/dcmi | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt echo "|" >> devicetree.txt echo "|-[camera:" | tr -d "\n" >> devicetree.txt cat /proc/device-tree/soc/i2c*/camera*/compatible >> devicetree.txt echo "]" >> devicetree.txt ./dtdump.sh /proc/device-tree/soc/i2c*/camera* -type f -print0 -exec ./dtdump.sh {} \; | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt echo "|" >> devicetree.txt echo "|-[mipi bridge:" | tr -d "\n" >> devicetree.txt cat /proc/device-tree/soc/i2c*/*mipi*/compatible >> devicetree.txt echo "]" >> devicetree.txt ./dtdump.sh /proc/device-tree/soc/i2c*/*mipi* -type f -print0 -exec ./dtdump.sh {} \; | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt echo "" >> devicetree.txt cat devicetree.txt
[devicetree] |-[dcmipp] | |-dcmipp@5a000000/compatible=st,stm32mp13-dcmipp 73742c73746d33326d7031332d64636d69707000 | |-dcmipp@5a000000/clocks� 000000080000008f | |-dcmipp@5a000000/resets5� 00000008000035c1 | |-dcmipp@5a000000/pinctrl-1=b 00000062 | |-dcmipp@5a000000/port/endpoint/hsync-active= 00000000 | |-dcmipp@5a000000/port/endpoint/vsync-active= 00000000 | |-dcmipp@5a000000/port/endpoint/remote-endpoint=c 00000063 | |-dcmipp@5a000000/port/endpoint/pclk-max-frequency=' 07270e00 | |-dcmipp@5a000000/port/endpoint/bus-width= 00000008 | |-dcmipp@5a000000/port/endpoint/pclk-sample= 00000000 | |-dcmipp@5a000000/port/endpoint/phandle=> 0000003e | |-dcmipp@5a000000/port/endpoint/name=endpoint 656e64706f696e7400 | |-dcmipp@5a000000/port/name=port 706f727400 | |-dcmipp@5a000000/clock-names=kclk 6b636c6b00 | |-dcmipp@5a000000/status=okay 6f6b617900 | |-dcmipp@5a000000/interrupts=O 000000000000004f00000004 | |-dcmipp@5a000000/phandle=� 000000d4 | |-dcmipp@5a000000/reg=Z 5a00000000000400 | |-dcmipp@5a000000/pinctrl-0=a 00000061 | |-dcmipp@5a000000/name=dcmipp 64636d69707000 | |-dcmipp@5a000000/pinctrl-names=defaultsleep 64656661756c7400736c65657000 | |-[camera:ovti,ov5640] | |-i2c@4c006000/camera@3c/compatible=ovti,ov5640 6f7674692c6f763536343000 | |-i2c@4c006000/camera@3c/powerdown-gpios=/ 0000002f0000000300000001 | |-i2c@4c006000/camera@3c/DOVDD-supply=6 00000036 | |-i2c@4c006000/camera@3c/clocks=5 00000035 | |-i2c@4c006000/camera@3c/port/endpoint/data-lanes= 0000000100000002 | |-i2c@4c006000/camera@3c/port/endpoint/clock-lanes= 00000000 | |-i2c@4c006000/camera@3c/port/endpoint/phandle=� 000000a5 | |-i2c@4c006000/camera@3c/port/endpoint/name=endpoint 656e64706f696e7400 | |-i2c@4c006000/camera@3c/port/name=port 706f727400 | |-i2c@4c006000/camera@3c/clock-names=xclk 78636c6b00 | |-i2c@4c006000/camera@3c/status=disabled 64697361626c656400 | |-i2c@4c006000/camera@3c/reset-gpios=/ 0000002f0000000400000001 | |-i2c@4c006000/camera@3c/phandle=� 000000a4 | |-i2c@4c006000/camera@3c/reg=< 0000003c | |-i2c@4c006000/camera@3c/name=camera 63616d65726100 | |-[mipi bridge:st,st-mipid02] | |-i2c@4c006000/stmipi@14/compatible=st,st-mipid02 73742c73742d6d69706964303200 | |-i2c@4c006000/stmipi@14/clocks=; 0000003b | |-i2c@4c006000/stmipi@14/VDDIN-supply=< 0000003c | |-i2c@4c006000/stmipi@14/clock-names=xclk 78636c6b00 | |-i2c@4c006000/stmipi@14/ports/#address-cells= 00000001 | |-i2c@4c006000/stmipi@14/ports/#size-cells= 00000000 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/hsync-active= 00000000 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/vsync-active= 00000000 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/remote-endpoint=> 0000003e | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/bus-width= 00000008 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/pclk-sample= 00000000 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/phandle=c 00000063 | |-i2c@4c006000/stmipi@14/ports/port@2/endpoint/name=endpoint 656e64706f696e7400 | |-i2c@4c006000/stmipi@14/ports/port@2/reg= 00000002 | |-i2c@4c006000/stmipi@14/ports/port@2/name=port 706f727400 | |-i2c@4c006000/stmipi@14/ports/port@0/endpoint/remote-endpoint== 0000003d | |-i2c@4c006000/stmipi@14/ports/port@0/endpoint/data-lanes= 0000000100000002 | |-i2c@4c006000/stmipi@14/ports/port@0/endpoint/phandle=7 00000037 | |-i2c@4c006000/stmipi@14/ports/port@0/endpoint/lane-polarities= 000000000000000000000000 | |-i2c@4c006000/stmipi@14/ports/port@0/endpoint/name=endpoint 656e64706f696e7400 | |-i2c@4c006000/stmipi@14/ports/port@0/reg= 00000000 | |-i2c@4c006000/stmipi@14/ports/port@0/name=port 706f727400 | |-i2c@4c006000/stmipi@14/ports/name=ports 706f72747300 | |-i2c@4c006000/stmipi@14/status=okay 6f6b617900 | |-i2c@4c006000/stmipi@14/reset-gpios=/ 0000002f0000000200000001 | |-i2c@4c006000/stmipi@14/VDDE-supply=< 0000003c | |-i2c@4c006000/stmipi@14/phandle=� 000000a6 | |-i2c@4c006000/stmipi@14/reg= 00000014 | |-i2c@4c006000/stmipi@14/name=stmipi 73746d69706900
5.1.2. Camera subsystem configuration debugging[edit source]
Refer to section #Get the topology of camera subsystem for basics on how to get and set camera subsystem configuration. Find below some debugging tips to help configuration handling.
5.1.2.1. subdevice configuration syntax error[edit source]
media-ctl utility returns an error when a configuration syntax mistake is made. Example here with erroneous entity name:
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480]" Unable to setup formats: Invalid argument (22)
In order to have details on the exact error, add -v option:
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480]" -v no such entity "dcmipp_dump_postpr" 'dcmipp_dump_postpr':0[fmt:RGB565_2X8_LE/640x480] ^
Another example with pad number mistake (only pad number 0 or 1 are allowed):
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':4[fmt:RGB565_2X8_LE/640x480]" -v No pad '4' on entity "dcmipp_dump_postproc". Maximum pad number is 1 'dcmipp_dump_postproc':4[fmt:RGB565_2X8_LE/640x480] ^
Example with format mistake (BA81 is a raw-bayer V4L2 pixel format while subdevice expects V4L2 mbus code such as SBGGR8_1X8):
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:BA81/640x480]" -v Invalid pixel code 'BA81' 'dcmipp_dump_postproc':0[fmt:BA81/640x480] ^
5.1.2.2. subdevice negotiation[edit source]
Requested configuration may not be fully accepted by the subdevice, in this case, the subdevice configures itself with the part of configuration it can handle. media-ctl -v option when setting configuration shows the effective subdevice configuration.
Here is an example with 5 fps framerate not accepted by the subdevice and 30 fps selected instead:
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/640x480@1/5 field:none]" -v Setting up format RGB565_2X8_BE 640x480 on pad gc2145 1-003c/0 Format set: RGB565_2X8_BE 640x480 Setting up frame interval 1/5 on pad gc2145 1-003c/0 Frame interval set: 1/30
Example with resolution negotiation (4000x4000 reduced to 2592x1944)
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/4000x4000@1/15 field:none]" -v Setting up format RGB565_2X8_BE 4000x4000 on pad gc2145 1-003c/0 Format set: RGB565_2X8_BE 1600x1200
Example with format negotiation (AYUV8_1X32 not supported, defaults to RGB565_2X8_LE):
media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:AYUV8_1X32/640x480]" -v Setting up format AYUV8_1X32 640x480 on pad dcmipp_dump_postproc/0 Format set: RGB565_2X8_LE
5.2. How to trace[edit source]
5.2.1. V4L2 userland API tracing[edit source]
Tracing of V4L2 userland API[3] can be enabled using command:
echo 0x3 > /sys/devices/platform/soc/5a000000.dcmipp/video4linux/video0/dev_debug
Traces are output in kernel log buffer:
dmesg [ 655.479016] video0: VIDIOC_QUERYCAP: driver=dcmipp, card=dcmipp_bytecap, bus=platform:dcmipp, version=0x00050f00, capabilities=0x852000011 [ 655.481591] video0: VIDIOC_G_FMT: type=vid-cap, width=640, height=480, pixelformat=RGBP little-endian (0x50424752), field=none, bytesperl0 [ 655.481656] video0: VIDIOC_ENUM_FMT: index=0, type=vid-cap, flags=0x0, pixelformat=RGBP little-endian (0x50424752), mbus_code=0x0000, des' [ 655.481696] video0: VIDIOC_ENUM_FMT: index=1, type=vid-cap, flags=0x0, pixelformat=YUYV little-endian (0x56595559), mbus_code=0x0000, des' [ 655.481732] video0: VIDIOC_ENUM_FMT: index=2, type=vid-cap, flags=0x0, pixelformat=YVYU little-endian (0x55595659), mbus_code=0x0000, des' [ 655.481767] video0: VIDIOC_ENUM_FMT: index=3, type=vid-cap, flags=0x0, pixelformat=UYVY little-endian (0x59565955), mbus_code=0x0000, des' [ 655.481802] video0: VIDIOC_ENUM_FMT: index=4, type=vid-cap, flags=0x0, pixelformat=VYUY little-endian (0x59555956), mbus_code=0x0000, des' [ 655.481836] video0: VIDIOC_ENUM_FMT: index=5, type=vid-cap, flags=0x0, pixelformat=GREY little-endian (0x59455247), mbus_code=0x0000, des' [ 655.481873] video0: VIDIOC_ENUM_FMT: index=6, type=vid-cap, flags=0x0, pixelformat=BA81 little-endian (0x31384142), mbus_code=0x0000, des' [ 655.481909] video0: VIDIOC_ENUM_FMT: index=7, type=vid-cap, flags=0x0, pixelformat=GBRG little-endian (0x47524247), mbus_code=0x0000, des' [ 655.481944] video0: VIDIOC_ENUM_FMT: index=8, type=vid-cap, flags=0x0, pixelformat=GRBG little-endian (0x47425247), mbus_code=0x0000, des' [ 655.481981] video0: VIDIOC_ENUM_FMT: index=9, type=vid-cap, flags=0x0, pixelformat=RGGB little-endian (0x42474752), mbus_code=0x0000, des' [ 655.482017] video0: VIDIOC_ENUM_FMT: index=10, type=vid-cap, flags=0x1, pixelformat=JPEG little-endian (0x4745504a), mbus_code=0x0000, de' [ 655.482061] video0: VIDIOC_S_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0 [ 655.526124] video0: VIDIOC_REQBUFS: count=4, type=vid-cap, memory=mmap [ 655.526221] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=0, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4 [ 655.526272] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [ 655.526296] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=1, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4 [ 655.526339] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [ 655.526359] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=2, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4 [ 655.526401] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [ 655.526420] video0: VIDIOC_QUERYBUF: 00:00:00.000000 index=3, type=vid-cap, request_fd=0, flags=0x00002000, field=any, sequence=0, memory4 [ 655.526462] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [ 655.527192] video0: VIDIOC_G_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0 [ 655.536625] video0: VIDIOC_STREAMON: type=vid-cap [ 655.536701] video0: VIDIOC_G_FMT: type=vid-cap, width=2592, height=1952, pixelformat=JPEG little-endian (0x4745504a), field=none, bytespe0 [ 655.892309] video0: VIDIOC_STREAMOFF: type=vid-cap [ 655.892435] video0: VIDIOC_STREAMOFF: type=vid-cap [ 655.901481] video0: VIDIOC_REQBUFS: count=0, type=vid-cap, memory=mmap
5.2.2. V4L2 core framework tracing[edit source]
Tracing of the V4L2 core framework[5] can be enabled using commands:
echo 0x3 > /sys/module/videobuf2_common/parameters/debug echo 0x3 > /sys/module/videobuf2_v4l2/parameters/debug
Traces are output in kernel log buffer:
dmesg [ 1218.626235] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 0, plane 0 offset 0x00000000 [ 1218.642445] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 1, plane 0 offset 0x004d4000 [ 1218.656398] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 2, plane 0 offset 0x009a8000 [ 1218.669843] videobuf2_common: [cap-7b50f8bf] __setup_offsets: buffer 3, plane 0 offset 0x00e7c000 [ 1218.677503] videobuf2_common: [cap-7b50f8bf] __vb2_queue_alloc: allocated 4 buffers, 1 plane(s) each [ 1218.688361] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 0, plane 0 successfully mapped [ 1218.696744] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 1, plane 0 successfully mapped [ 1218.705291] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 2, plane 0 successfully mapped [ 1218.712487] videobuf2_common: [cap-7b50f8bf] vb2_mmap: buffer 3, plane 0 successfully mapped [ 1218.722474] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 0 succeeded [ 1218.730528] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 1 succeeded [ 1218.738153] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 2 succeeded [ 1218.746012] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 3 succeeded [ 1218.756237] videobuf2_common: [cap-7b50f8bf] vb2_core_streamon: successful [ 1218.761969] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers [ 1218.822167] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer [ 1218.828383] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 0, state: dequeued [ 1218.838812] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 0 succeeded [ 1218.846549] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers [ 1218.855624] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer [ 1218.862118] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 1, state: dequeued [ 1218.872406] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 1 succeeded [ 1218.880029] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers [ 1218.889460] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer [ 1218.896756] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 2, state: dequeued [ 1218.905383] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 2 succeeded [ 1218.912309] videobuf2_common: [cap-7b50f8bf] __vb2_wait_for_done_vb: will sleep waiting for buffers [ 1218.923080] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: returning done buffer [ 1218.930392] videobuf2_common: [cap-7b50f8bf] vb2_core_dqbuf: dqbuf of buffer 3, state: dequeued [ 1218.944499] videobuf2_common: [cap-7b50f8bf] vb2_core_qbuf: qbuf of buffer 3 succeeded [ 1218.952210] videobuf2_common: [cap-7b50f8bf] vb2_core_streamoff: successful [ 1218.959921] videobuf2_common: [cap-7b50f8bf] vb2_core_streamoff: successful [ 1218.968800] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 0 [ 1218.978419] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 1 [ 1218.988204] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 2 [ 1218.997501] videobuf2_common: [cap-7b50f8bf] __vb2_buf_mem_free: freed plane 0 of buffer 3
5.2.3. DCMIPP V4L2 kernel driver tracing[edit source]
DCMIPP dynamic debug traces[6] can be enabled using command:
echo "module stm32_dcmipp +p" > /sys/kernel/debug/dynamic_debug/control echo "module dcmipp_bytecap +p" > /sys/kernel/debug/dynamic_debug/control echo "module dcmipp_byteproc +p" > /sys/kernel/debug/dynamic_debug/control echo "module dcmipp_parallel +p" > /sys/kernel/debug/dynamic_debug/control
Here is an example with a 5Mp jpeg capture:
media-ctl -d /dev/media0 --set-v4l2 "'gc2145 1-003c':0[fmt:RGB565_2X8_BE/640x480@1/30 field:none]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_parallel':0[fmt:RGB565_2X8_BE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_parallel':0[fmt:RGB565_2X8_LE/640x480]" media-ctl -d /dev/media0 --set-v4l2 "'dcmipp_dump_postproc':0[fmt:RGB565_2X8_LE/640x480]"
v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-640x480-rgb565.raw
dmesg [ 236.968937] dcmipp-parallel dcmipp-parallel.1.auto: dcmipp_parallel: format update: old:640x480 (0x1007, 8, 1, 2, 1) new:640x480 (0x1007, 3, 0, 0, 0) [ 236.987292] dcmipp-parallel dcmipp-parallel.1.auto: dcmipp_parallel: format update: old:640x480 (0x1007, 3, 0, 0, 0) new:640x480 (0x1008, 3, 0, 0, 0) [ 246.673178] dcmipp-bytecap dcmipp-bytecap.3.auto: dcmipp_dump_capture: format update: old:640x480 (0x50424752, 8, 1, 2, 0) new:640x480 (0x50424752, 8, 1, 2, 0) [ 246.673704] dcmipp-bytecap dcmipp-bytecap.3.auto: Setup queue, count=4, size=614400 [ 246.691053] dcmipp-bytecap dcmipp-bytecap.3.auto: Setup [0] phy=0xd4a00000 size=614400 [ 246.691114] dcmipp-bytecap dcmipp-bytecap.3.auto: Setup [1] phy=0xd4b00000 size=614400 [ 246.691136] dcmipp-bytecap dcmipp-bytecap.3.auto: Setup [2] phy=0xd4c00000 size=614400 [ 246.691156] dcmipp-bytecap dcmipp-bytecap.3.auto: Setup [3] phy=0xd4d00000 size=614400 [ 246.691189] dcmipp-bytecap dcmipp-bytecap.3.auto: Queue [0] cdcc4929 phy=0xd4a00000 [ 246.691208] dcmipp-bytecap dcmipp-bytecap.3.auto: Queue [1] 8cfa694d phy=0xd4b00000 [ 246.691221] dcmipp-bytecap dcmipp-bytecap.3.auto: Queue [2] 57f4cf64 phy=0xd4c00000 [ 246.691233] dcmipp-bytecap dcmipp-bytecap.3.auto: Queue [3] 9a8d0e1c phy=0xd4d00000 [ 246.691397] dcmipp-byteproc dcmipp-byteproc.2.auto: CLR DCMIPP_P0FCTCR 0x00000003 [ 246.691415] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0FCTCR 0x00000000 [ 246.691425] dcmipp-byteproc dcmipp-byteproc.2.auto: SET DCMIPP_P0FCTCR 0x00000000 [ 246.691435] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0FCTCR 0x00000000 [ 246.691445] dcmipp-byteproc dcmipp-byteproc.2.auto: CLR DCMIPP_P0PPCR 0x00000180 [ 246.691455] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0PPCR 0x00000000 [ 246.691465] dcmipp-byteproc dcmipp-byteproc.2.auto: CLR DCMIPP_P0PPCR 0x00000400 [ 246.691474] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0PPCR 0x00000000 [ 246.691484] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0SCSTR 0x00000000 [ 246.691493] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0SCSZR 0x00000000 [ 246.691504] dcmipp-byteproc dcmipp-byteproc.2.auto: crop to 640x480 [ 246.691514] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0SCSTR 0x00000000 [ 246.691524] dcmipp-byteproc dcmipp-byteproc.2.auto: WR DCMIPP_P0SCSZR 0x81e00140 [ 246.691535] dcmipp-bytecap dcmipp-bytecap.3.auto: "dcmipp_dump_postproc" is started [ 246.691547] dcmipp-parallel dcmipp-parallel.1.auto: WR DCMIPP_PRCR 0x02220000 [ 246.691557] dcmipp-parallel dcmipp-parallel.1.auto: SET DCMIPP_PRCR 0x00004000 [ 246.691567] dcmipp-parallel dcmipp-parallel.1.auto: WR DCMIPP_PRCR 0x02224000 [ 246.691576] dcmipp-bytecap dcmipp-bytecap.3.auto: "dcmipp_parallel" is started [ 246.693135] dcmipp-bytecap dcmipp-bytecap.3.auto: "st-mipid02 1-0014" is started [ 246.832561] dcmipp-bytecap dcmipp-bytecap.3.auto: "gc2145 1-003c" is started [ 246.832598] dcmipp-bytecap dcmipp-bytecap.3.auto: SET DCMIPP_P0FSCR 0x80000000 [ 246.832619] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0FSCR 0x80000000 [ 246.832635] dcmipp-bytecap dcmipp-bytecap.3.auto: Start with next [0] cdcc4929 phy=0xd4a00000 [ 246.832661] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0PPM0AR1 0xd4a00000 [ 246.832676] dcmipp-bytecap dcmipp-bytecap.3.auto: Write [0] cdcc4929 phy=0xd4a00000 [ 246.832695] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0DCLMTR 0x80025800 [ 246.832709] dcmipp-bytecap dcmipp-bytecap.3.auto: SET DCMIPP_P0FCTCR 0x00000008 [ 246.832724] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0FCTCR 0x00000008 [ 246.832738] dcmipp-bytecap dcmipp-bytecap.3.auto: SET DCMIPP_CMIER 0x00008600 [ 246.832753] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMIER 0x00008600 [ 247.094680] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR2 0x00000400 [ 247.094723] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMFCR 0x00000400 [ 247.094759] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0PPM0AR1 0xd4b00000 [ 247.094777] dcmipp-bytecap dcmipp-bytecap.3.auto: Write [1] 8cfa694d phy=0xd4b00000 [ 247.128387] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR2 0x00000300 [ 247.128430] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMFCR 0x00000300 [ 247.128469] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_P0DCCNTR 0x00096000 [ 247.128498] dcmipp-bytecap dcmipp-bytecap.3.auto: Done [0] cdcc4929 phy=0xd4a00000 [ 247.129127] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR2 0x00000500 [ 247.129163] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMFCR 0x00000500 [ 247.129357] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0PPM0AR1 0xd4c00000 [ 247.129383] dcmipp-bytecap dcmipp-bytecap.3.auto: Write [2] 57f4cf64 phy=0xd4c00000 [ 247.149857] dcmipp-bytecap dcmipp-bytecap.3.auto: Queue [0] cdcc4929 phy=0xd4a00000 [ 247.150021] dcmipp-bytecap dcmipp-bytecap.3.auto: "dcmipp_dump_postproc" is stopped [ 247.150040] dcmipp-parallel dcmipp-parallel.1.auto: CLR DCMIPP_PRCR 0x00004000 [ 247.150053] dcmipp-parallel dcmipp-parallel.1.auto: WR DCMIPP_PRCR 0x02220000 [ 247.150074] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR2 0x00000300 [ 247.150085] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMFCR 0x00000300 [ 247.150130] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_P0DCCNTR 0x0005f000 [ 247.150147] dcmipp-bytecap dcmipp-bytecap.3.auto: Done [1] 8cfa694d phy=0xd4b00000 [ 247.156441] dcmipp-bytecap dcmipp-bytecap.3.auto: "dcmipp_parallel" is stopped [ 247.156965] dcmipp-bytecap dcmipp-bytecap.3.auto: "st-mipid02 1-0014" is stopped [ 247.157010] dcmipp-bytecap dcmipp-bytecap.3.auto: "gc2145 1-003c" is stopped [ 247.157028] dcmipp-bytecap dcmipp-bytecap.3.auto: CLR DCMIPP_CMIER 0x00008600 [ 247.157043] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_CMIER 0x00000000 [ 247.157053] dcmipp-bytecap dcmipp-bytecap.3.auto: CLR DCMIPP_P0FCTCR 0x00000008 [ 247.157062] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0FCTCR 0x00000000 [ 247.157073] dcmipp-bytecap dcmipp-bytecap.3.auto: CLR DCMIPP_P0FSCR 0x80000000 [ 247.157083] dcmipp-bytecap dcmipp-bytecap.3.auto: WR DCMIPP_P0FSCR 0x00000000 [ 247.157100] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_PRSR 0x00030000 [ 247.157111] dcmipp-bytecap dcmipp-bytecap.3.auto: [DCMIPP_PRSR] =0x00030000 [ 247.157120] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_P0SR 0x00000007 [ 247.157129] dcmipp-bytecap dcmipp-bytecap.3.auto: [DCMIPP_P0SR] =0x00000007 [ 247.157139] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_P0DCCNTR 0x0005f000 [ 247.157148] dcmipp-bytecap dcmipp-bytecap.3.auto: [DCMIPP_P0DCCNTR]=0x0005f000 [ 247.157157] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR1 0x00000003 [ 247.157166] dcmipp-bytecap dcmipp-bytecap.3.auto: [DCMIPP_CMSR1] =0x00000003 [ 247.157175] dcmipp-bytecap dcmipp-bytecap.3.auto: RD DCMIPP_CMSR2 0x00000000 [ 247.157184] dcmipp-bytecap dcmipp-bytecap.3.auto: [DCMIPP_CMSR2] =0x00000000 [ 247.157198] dcmipp-bytecap dcmipp-bytecap.3.auto: Stop streaming, errors=0 (overrun=0, limit=0, nactive=0), underrun=0, vsync=2, frame=2, buffers=2, it=4
5.3. How to debug[edit source]
5.3.1. Errors[edit source]
Errors are unconditionally traced in kernel log:
dmesg [ 1947.932915] dcmipp-bytecap dcmipp-bytecap.3.auto: Stop streaming, errors=1 (overrun=0, limit=0), vsync=2, frame=2, buffers=2, it=4
5.3.2. Memory tracking[edit source]
Frames require large chunks of contiguous memory. They are allocated by V4L2 framework through DMA backend. Those allocations can be traced using:
echo "module dma_contiguous +p" > /sys/kernel/debug/dynamic_debug/control echo "module videobuf2_dma_contig +p" > /sys/kernel/debug/dynamic_debug/control
Here is the trace after a VGA YUV422 capture.
[11311.617688] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb3b6a000, size 614400 [11311.617986] vb2_dc_mmap: mapped dma addr 0xf1a00000 at 0xb3ad4000, size 614400 [11311.618071] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb3a3e000, size 614400 [11311.764146] vb2_dc_mmap: mapped dma addr 0xf1c00000 at 0xb307c000, size 614400
4 frames of VGA YUV422 frames: 640x480x2=614400 bytes
6. Source code location[edit source]
6.1. User space[edit source]
6.2. Kernel space[edit source]
7. References[edit source]
- ↑ Information about V4L2 Linux kernel framework on wikipedia.
- ↑ 2.0 2.1 Linux Media Infrastructure userspace API » Part IV - Media Controller API
- ↑ 3.0 3.1 3.2 3.3 Linux Media Infrastructure userspace API » Part I - Video for Linux API
- ↑ Linux Media Infrastructure userspace API » Part I - Video for Linux API » 4. Interfaces » 4.5. Video Memory-To-Memory Interface
- ↑ 5.0 5.1 Media subsystem kernel internal API » 1. Video4Linux devices
- ↑ How to use the kernel dynamic debug