1. Introduction[edit source]
This article will explain how to set up a Point-to-Point connection to the MPU target, in case of a proxy is also setup on the PC for accessing the Internet.
2. Setting up network[edit source]
To set up the connection go to Windows -> Preferences -> General -> Network Connections.
Select "Manual" in the Active Provider field, and:
- adjust your proxy setup with Edit... in Proxy entries
- configure a new Proxy bypass with Add Host... giving the IP address of the MPU target.
File:Draft CubeIDE-Proxy.png
Network Setting in STM32CubeIDE