STM32PRGFW-UTIL release note

Revision as of 06:19, 16 September 2024 by Registered User (versions updated)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

The STM32PRGFW-UTIL is an STMicroelectronics original initiative to manage the One-time Programmable (OTP) memories and also supports STPMIC programming.

More information can be found in the detailed release notes referenced later in this article.

1. STM32PRGFW-UTIL - version 1.1.1[edit source]

Warning white.png Warning
It is mandatory to use STM32PRGFW-UTIL version v1.1.1 and above, to avoid bricking of your device.
Info white.png Information
This new version has some dependencies with STM32CubeIDE 1.16.0 (at least) and STM32CubeProgrammer v2.17.0 minimum (at least) , it is then highly recommended to update also those 2 other ST tools
STM32PRGFW-UTIL for Linux® and Windows® host PC
Download

Version 1.1.0.rc6

  • STM32PRGFW-UTIL firmware package is available here .
Installing the STM32PRGFW-UTIL
  • To use STM32PRGFW-UTIL, unzip the package on computer..
  • Then refer to READMED.md , to use this tool .
Detailed release note
  • Full details about the content of this tool release are available here .