Some typical troubles related to the system build are listed below. Solutions or ways of debugging are proposed for these troubles.
If your trouble is not listed, it's recommended to go through the articles of the system build category.
Symptom | Resolution |
---|---|
Distribution Package | |
repo init ...<br> repo sync "The requested URL returned error: 404 Not Found" is displayed |
This error has no impact on the process. You can avoid this error by adding the option --no-clone-bundle to your command repo init or repo sync |
repo init ... Some github projects are not accessible |
It is convenient to indicate in your $HOME/.netrc your github credentials like below:
machine github.com login "github login" password "github password" |
Developer Package | |
make ... Any build command fails |
Check that the SDK is started |
<sdk_install_path>/sysroots/x86_64-ostl_sdk-linux/usr/bin/ld: /usr/lib/gcc/x86_64-linux-gnu/9/../../../x86_64-linux-gnu/libcrypto.so: undefined reference to `pthread_rwlock_rdlock@GLIBC_2.2.5' <sdk_install_path>/sysroots/x86_64-ostl_sdk-linux/usr/bin/ld: /usr/lib/gcc/x86_64-linux-gnu/9/../../../x86_64-linux-gnu/libcrypto.so: undefined reference to `pthread_setspecific@GLIBC_2.2.5' .... collect2: error: ld returned 1 exit status The Linux kernel cannot build. |
You are trying to use the SDK on a non-supported Linux system, your glibc is too old. For example, this is the case if you try to build on Ubuntu 20.04. Please refer to the explanation on migration guide on Yocto website. |