Last edited 2 months ago

Ethtool

Applicable for STM32MP13x lines, STM32MP15x lines

1. Article purpose[edit | edit source]

This article provides the basic information needed to start using the Linux® command tool: ethtool [1].

2. Introduction[edit | edit source]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Only supported for STM32MP15x lines More info.png
Warning white.png Warning
The STM32MPU distribution for Android™ is not available in the v4 ecosystem releases: refer to the Ethtool page for the v2 ecosystem releases (in archived wiki).
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
ethtool Monitoring tools ethtool[1] allows to query or control network driver and hardware settings, in particular for wired Ethernet devices. Yes Yes Yes No No No

3. Installing the trace and debug tool on your target board[edit | edit source]

3.1. Using the STM32MPU Embedded Software distribution[edit | edit source]

ethtool is installed by default and ready to be used with all STM32MPU Embedded Software Packages.

 which ethtool
/usr/sbin/ethtool

It is integrated in weston image distribution through the meta-st package: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb.

RDEPENDS_packagegroup-framework-tools-network-base = "\
   ethtool         \
   iproute2        \
   "

4. Getting started[edit | edit source]

The ethernet links available on your board can be listed by using the IP Linux command line:

 ip link | grep eth
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP mode DEFAULT group default qlen 1000
   link/ether 00:80:e1:42:43:65 brd ff:ff:ff:ff:ff:ff
  • Get information about the eth0 network device:
 ethtool eth0
Settings for eth0:
	Supported ports: [ TP AUI BNC MII FIBRE ]
	Supported link modes:   10baseT/Half 10baseT/Full 
	                        100baseT/Half 100baseT/Full 
	                        1000baseT/Half 1000baseT/Full 
	Supported pause frame use: Symmetric Receive-only
	Supports auto-negotiation: Yes
	Advertised link modes:  10baseT/Half 10baseT/Full 
	                        100baseT/Half 100baseT/Full 
	                        1000baseT/Half 1000baseT/Full 
	Advertised pause frame use: No
	Advertised auto-negotiation: Yes
	Link partner advertised link modes:  10baseT/Half 10baseT/Full 
	                                     100baseT/Half 100baseT/Full 
	                                     1000baseT/Full 
	Link partner advertised pause frame use: Symmetric
	Link partner advertised auto-negotiation: Yes
	Speed: 1000Mb/s
	Duplex: Full
	Port: MII
	PHYAD: 0
	Transceiver: internal
	Auto-negotiation: on
	Supports Wake-on: ug
	Wake-on: d
	Current message level: 0x0000003f (63)
			       drv probe link timer ifdown ifup
	Link detected: yes
  • Display Ethernet driver settings for eth0
 ethtool -i eth0
driver: st_gmac
version: Jan_2016
firmware-version: 
expansion-rom-version: 
bus-info: 
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: no
  • Display network statistics for eth0:
 ethtool -S eth0
NIC statistics:
     mmc_tx_octetcount_gb: 0
     mmc_tx_framecount_gb: 0
     mmc_tx_broadcastframe_g: 0
     mmc_tx_multicastframe_g: 0
     mmc_tx_64_octets_gb: 0
     mmc_tx_65_to_127_octets_gb: 0
     mmc_tx_128_to_255_octets_gb: 0
     mmc_tx_256_to_511_octets_gb: 0
     mmc_tx_512_to_1023_octets_gb: 0
     mmc_tx_1024_to_max_octets_gb: 0
     mmc_tx_unicast_gb: 0
     mmc_tx_multicast_gb: 0
     mmc_tx_broadcast_gb: 0
     mmc_tx_underflow_error: 0
     mmc_tx_singlecol_g: 0
     mmc_tx_multicol_g: 0
     mmc_tx_deferred: 0
     mmc_tx_latecol: 0
     mmc_tx_exesscol: 0
     mmc_tx_carrier_error: 0
     mmc_tx_octetcount_g: 0
     mmc_tx_framecount_g: 1809
     mmc_tx_excessdef: 0
     mmc_tx_pause_frame: 0
     mmc_tx_vlan_frame_g: 0
     mmc_rx_framecount_gb: 0
     mmc_rx_octetcount_gb: 0
     mmc_rx_octetcount_g: 0
     mmc_rx_broadcastframe_g: 0
     mmc_rx_multicastframe_g: 0
     mmc_rx_crc_error: 0
     mmc_rx_align_error: 0
     mmc_rx_run_error: 0
     mmc_rx_jabber_error: 0
     mmc_rx_undersize_g: 0
     mmc_rx_oversize_g: 0
     mmc_rx_64_octets_gb: 0
     mmc_rx_65_to_127_octets_gb: 0
     mmc_rx_128_to_255_octets_gb: 0
     mmc_rx_256_to_511_octets_gb: 0
     mmc_rx_512_to_1023_octets_gb: 0
     mmc_rx_1024_to_max_octets_gb: 0
     mmc_rx_unicast_g: 1514
     mmc_rx_length_error: 0
     mmc_rx_autofrangetype: 0
     mmc_rx_pause_frames: 0
     mmc_rx_fifo_overflow: 0
     mmc_rx_vlan_frames_gb: 0
     mmc_rx_watchdog_error: 0
     mmc_rx_ipc_intr_mask: 0
     mmc_rx_ipc_intr: 0
     mmc_rx_ipv4_gd: 0
     mmc_rx_ipv4_hderr: 0
     mmc_rx_ipv4_nopay: 0
     mmc_rx_ipv4_frag: 0
     mmc_rx_ipv4_udsbl: 0
     mmc_rx_ipv4_gd_octets: 0
     mmc_rx_ipv4_hderr_octets: 0
     mmc_rx_ipv4_nopay_octets: 0
     mmc_rx_ipv4_frag_octets: 0
     mmc_rx_ipv4_udsbl_octets: 0
     mmc_rx_ipv6_gd_octets: 0
     mmc_rx_ipv6_hderr_octets: 0
     mmc_rx_ipv6_nopay_octets: 0
     mmc_rx_ipv6_gd: 0
     mmc_rx_ipv6_hderr: 0
     mmc_rx_ipv6_nopay: 0
     mmc_rx_udp_gd: 0
     mmc_rx_udp_err: 0
     mmc_rx_tcp_gd: 0
     mmc_rx_tcp_err: 0
     mmc_rx_icmp_gd: 0
     mmc_rx_icmp_err: 0
     mmc_rx_udp_gd_octets: 0
     mmc_rx_udp_err_octets: 0
     mmc_rx_tcp_gd_octets: 0
     mmc_rx_tcp_err_octets: 0
     mmc_rx_icmp_gd_octets: 0
     mmc_rx_icmp_err_octets: 0
     tx_underflow: 0
     tx_carrier: 0
     tx_losscarrier: 0
     vlan_tag: 0
     tx_deferred: 0
     tx_vlan: 0
     tx_jabber: 0
     tx_frame_flushed: 0
     tx_payload_error: 0
     tx_ip_header_error: 0
     rx_desc: 0
     sa_filter_fail: 0
     overflow_error: 0
     ipc_csum_error: 0
     rx_collision: 0
     rx_crc_errors: 0
     dribbling_bit: 0
     rx_length: 0
     rx_mii: 0
     rx_multicast: 0
     rx_gmac_overflow: 0
     rx_watchdog: 0
     da_rx_filter_fail: 0
     sa_rx_filter_fail: 0
     rx_missed_cntr: 0
     rx_overflow_cntr: 0
     rx_vlan: 0
     tx_undeflow_irq: 0
     tx_process_stopped_irq: 0
     tx_jabber_irq: 0
     rx_overflow_irq: 0
     rx_buf_unav_irq: 0
     rx_process_stopped_irq: 0
     rx_watchdog_irq: 0
     tx_early_irq: 0
     fatal_bus_error_irq: 0
     rx_early_irq: 0
     threshold: 1
     tx_pkt_n: 1809
     rx_pkt_n: 12682
     normal_irq_n: 11110
     rx_normal_irq_n: 11082
     napi_poll: 11118
     tx_normal_irq_n: 28
     tx_clean: 11641
     tx_set_ic_bit: 28
     irq_receive_pmt_irq_n: 0
     mmc_tx_irq_n: 0
     mmc_rx_irq_n: 0
     mmc_rx_csum_offload_irq_n: 0
     irq_tx_path_in_lpi_mode_n: 0
     irq_tx_path_exit_lpi_mode_n: 0
     irq_rx_path_in_lpi_mode_n: 0
     irq_rx_path_exit_lpi_mode_n: 0
     phy_eee_wakeup_error_n: 0
     ip_hdr_err: 0
     ip_payload_err: 0
     ip_csum_bypassed: 544
     ipv4_pkt_rcvd: 9189
     ipv6_pkt_rcvd: 1948
     no_ptp_rx_msg_type_ext: 12682
     ptp_rx_msg_type_sync: 0
     ptp_rx_msg_type_follow_up: 0
     ptp_rx_msg_type_delay_req: 0
     ptp_rx_msg_type_delay_resp: 0
     ptp_rx_msg_type_pdelay_req: 0
     ptp_rx_msg_type_pdelay_resp: 0
     ptp_rx_msg_type_pdelay_follow_up: 0
     ptp_rx_msg_type_announce: 0
     ptp_rx_msg_type_management: 0
     ptp_rx_msg_pkt_reserved_type: 0
     ptp_frame_type: 0
     ptp_ver: 0
     timestamp_dropped: 0
     av_pkt_rcvd: 0
     av_tagged_pkt_rcvd: 0
     vlan_tag_priority_val: 0
     l3_filter_match: 0
     l4_filter_match: 0
     l3_l4_filter_no_match: 0
     irq_pcs_ane_n: 0
     irq_pcs_link_n: 0
     irq_rgmii_n: 1
     mtl_tx_status_fifo_full: 0
     mtl_tx_fifo_not_empty: 0
     mmtl_fifo_ctrl: 0
     mtl_tx_fifo_read_ctrl_write: 0
     mtl_tx_fifo_read_ctrl_wait: 0
     mtl_tx_fifo_read_ctrl_read: 0
     mtl_tx_fifo_read_ctrl_idle: 0
     mac_tx_in_pause: 0
     mac_tx_frame_ctrl_xfer: 0
     mac_tx_frame_ctrl_idle: 0
     mac_tx_frame_ctrl_wait: 0
     mac_tx_frame_ctrl_pause: 0
     mac_gmii_tx_proto_engine: 0
     mtl_rx_fifo_fill_level_full: 0
     mtl_rx_fifo_fill_above_thresh: 0
     mtl_rx_fifo_fill_below_thresh: 0
     mtl_rx_fifo_fill_level_empty: 0
     mtl_rx_fifo_read_ctrl_flush: 0
     mtl_rx_fifo_read_ctrl_read_data: 0
     mtl_rx_fifo_read_ctrl_status: 0
     mtl_rx_fifo_read_ctrl_idle: 0
     mtl_rx_fifo_ctrl_active: 0
     mac_rx_frame_ctrl_fifo: 0
     mac_gmii_rx_proto_engine: 0
     tx_tso_frames: 0
     tx_tso_nfrags: 0

5. To go further[edit | edit source]

Lots of documentation exists on Internet about ethtool.

Refer to ethtool man page[1] for more details on command options.

6. References[edit | edit source]


  • Useful external links
Document link Document Type Description
ethtool Standard Wikipedia article
ethtool-command User guide thegeekstuff web page