STM32CubeProgrammer release note

Revision as of 16:27, 13 December 2023 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines

STM32CubeProgrammer.png

STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.

1. STM32CubeProgrammer - Version v2.14.0-MP25-B02[edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download

Version v2.14.0-MP25-B02


  • Select and download the archive file that fits with your host PC (e.g., "SetupSTM32CubeProgrammer_linux_64_2_14_0_v0.0.0-MP25-B02(V2.14.BETA02).zip" for Linux® host PC)
  • Uncompress this archive file to get the STM32CubeProgrammer installers:
Example for Linux® host PC:
 unzip SetupSTM32CubeProgrammer_linux_64_2_14_0_v0.0.0-MP25-B02(V2.14.BETA02).zip
Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.15.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .