STM32MP2 ROM code resource isolation

Revision as of 16:38, 12 December 2023 by Registered User (→‎SDMMC2 access ensure)

1. Article purpose[edit source]

The purpose of this article is to describe the different requirements on system configuration (RIF, RCC) to guarantee a correct execution of the ROM code in all the supported execution contexts.

2. Introduction[edit source]

The STM32MP2 ROM code is executed in different boot and lower power exit sequences:

  • Cold boot to load the FSBL-A or the FSBL-M depending on main processor selection. In this context, Cortex-M33 and other master peripherals are under reset.
  • Standby exit to reload FSBL-A and restart Cortex-A35. In this context, Cortex-M33 and other master peripherals are maintained under reset. But part of the system is initialized (Mainly RIF)
  • D1Standby exit to (re)load FSBL-A and restart Cortex-A35. In the context, Cortex-M33 and other master peripherals could be running. Moreover system is fully initialized (RIF, RCC...)

Depending on main processor selection (Cortex-A35 TDCID or Cortex-M33 TDCID), ROM code has or has not the right to modify system configuration under TDCID responsibility. Moreover ROM code execution shall not impact rest of system during D1Stanby exit sequence.

Some rules on system configuration (RIF, RCC...) must be applied to guarantee STM32MP2 ROM code execution and isolation in the different contexts:

3. ROM code peripheral assignment[edit source]

3.1. Principles[edit source]

ROM code shall be able to access all resources required for its execution whatever ROM execution modes (Cold boot, Standby exit and D1 Standby exit).

Depending on ROM code execution context, part of the system could be already configured and running. System configuration should be compliant with ROM code resource needs.

  • RIF configuration including RIFSC and RIF-aware peripherals
  • RCC clock tree configuration

At each execution ROM code checks resource access rights based on RIF registers ( RIFSC and RIF-aware).

Four actions are possible:

Resource control type What is controlled How
Ensuring non-exclusive access The ROM code first checks that either resource access rights are not set, or are statically assigned to A35 The ROM code checks that either CID filtering is not configured, or is configured static and assigned to the A35.
Ensuring exclusive access The ROM code checks that either resource is statically assigned to A35, or that resource is shared via its semaphore, and semaphore can be taken within 10 ms. The ROM code checks that either CID filtering is configured static and assigned to the A35, or CID filtering is configured dynamic (meaning resource is shared via a semaphore) and semaphore can be taken within 10 ms.
Checking security level The ROM code checks that resource security level correspond to its needs The ROM code checks that resource security level
Setting security level The ROM code sets resource security level according to its needs. Indeed in that case security level used by SW ecosystem could be different from ROM code one. The ROM code sets resource security level according to its needs.

3.2. Secure peripherals[edit source]

The ROM code always ensure exclusive access and security level on these peripherals:

Peripheral RIF resource number RIF block Comment Secure level checked Cold boot Standby exit D1Standby exit
BSEC clock R103 RCC Yes Yes Yes Yes
CPU1 boot, reset, IWDG management R70 RCC Yes Yes Yes Yes
CPU PWR1 R2 PWR power control Yes Yes Yes Yes
STGEN R33 RCC flexgen Yes Yes Yes Yes


In case of secure boot when the chip is in CLOSED-LOCKED state, the ROM code always ensure exclusive access and security level on these peripherals to perform boot authentication and decryption:

Peripheral RIF resource number RIF block Secure level checked Cold boot Standby exit D1Standby exit
RNG R92 RIFSC Yes Yes Yes Yes
PKA R93 RIFSC Yes Yes Yes Yes
SAES R94 RIFSC Yes Yes Yes Yes
HASH R95 RIFSC Yes Yes Yes Yes
CRYP1 R96 RIFSC Yes Yes Yes Yes
SYSRAM/RISAB1 & RISAB2 R74 RCC Yes Yes Yes Yes
CA35SS R106 RCC Yes Yes Yes Yes

3.3. Non-secure peripherals[edit source]

ROM code ensures non-secure access to non-secure peripherals used during its execution, then it sets security level according to its needs.

ROM code adapts list of non-secure peripherals according to selected boot source.

3.3.1. SDMMC1 access ensure[edit source]

Checked in the following boot selection:

  • Cortex-A35 main processor
  • Boot from eMMC SDMMC1
  • Boot from SD-Card SDMMC1
  • Cortex-M33 main processor single boot device
  • Boot from eMMC SDMMC1
  • Boot from SD-Card SDMMC1
  • Cortex-M33 main processor dual boot device
  • Boot Cortex-M33 from sNOR and Cortex-A35 from eMMC SDMMC1
  • Boot Cortex-M33 from sNOR and Cortex-A35 from SD-Card SDMMC1
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from eMMC SDMMC1
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from SD-Card SDMMC1

The following table list resources associated to SDMMC1.

Function RIF resource number RIF block Resource description Secure level set Check at cold boot Check at Standby exit Check at D1Standby exit
Root Clock SDMMC1 R51 RCC Flexgen 51 No Yes Yes Yes
Clock GPIOE R94 RCC GPIO E clock config No Yes Yes Yes
IO voltage protection R6 PWR VDDIO1 (PWR_C8) Yes Yes Yes Yes
GPIO PE3 R3 GPIOE SDMMC1_CK No Yes Yes Yes
GPIO PE2 R2 GPIOE SDMMC1_CMD No Yes Yes Yes
GPIO PE4 R4 GPIOE SDMMC1_D0 No Yes Yes Yes
SDMMC1 R76 RIFSC SDMMC1 controller No Yes Yes Yes

3.3.2. SDMMC2 access ensure[edit source]

Checked in the following boot selection:

  • Cortex-A35 main processor
  • Boot from eMMC SDMMC2
  • Boot from SD-Card SDMMC2
  • Cortex-M33 main processor single boot device
  • Boot from eMMC SDMMC2
  • Boot from SD-Card SDMMC2
  • Cortex-M33 main processor dual boot device
  • Boot Cortex-M33 from sNOR and Cortex-A35 from eMMC SDMMC2
  • Boot Cortex-M33 from sNOR and Cortex-A35 from SD-Card SDMMC2
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from eMMC SDMMC2
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from SD-Card SDMMC2

The following table list resources associated to SDMMC2.

Function RIF resource number RIF block Resource description Secure level set Check at cold boot Check at Standby exit Check at D1Standby exit
Root Clock SDMMC2 R52 RCC Flexgen 52 No Yes Yes Yes
Clock GPIOE R94 RCC GPIO E clock config No Yes Yes Yes
IO voltage protection R5 PWR VDDIO2 (PWR_C7) Yes Yes Yes Yes
GPIO PE14 R14 GPIOE SDMMC2_CK No Yes Yes Yes
GPIO PE15 R15 GPIOE SDMMC2_CMD No Yes Yes Yes
GPIO PE13 R13 GPIOE SDMMC2_D0 No Yes Yes Yes
SDMMC2 R77 RIFSC SDMMC1 controller No Yes Yes Yes

3.3.3. OCTOSPI1 access ensure[edit source]

Checked in the following boot selection:

  • Cortex-A35 main processor
  • Boot from sNAND
  • Boot from sNOR
  • Boot from Hyperflash
  • Cortex-M33 main processor single boot device
  • Boot from sNAND
  • Boot from sNOR
  • Boot from Hyperflash
  • Cortex-M33 main processor dual boot device
  • Boot Cortex-M33 from sNOR and Cortex-A35 from eMMC SDMMC1
  • Boot Cortex-M33 from sNOR and Cortex-A35 from SD-Card SDMMC1
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from eMMC SDMMC1
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from SD-Card SDMMC1
  • Boot Cortex-M33 from sNOR and Cortex-A35 from eMMC SDMMC2
  • Boot Cortex-M33 from sNOR and Cortex-A35 from SD-Card SDMMC2
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from eMMC SDMMC2
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from SD-Card SDMMC2

The following table list resources associated to OctoSPI1.

Function RIF resource number RIF block Resource description Secure level set Check at cold boot Check at Standby exit Check at D1Standby exit
Root Clock Octospi1 R48 RCC Flexgen 48 0 Yes Yes Yes
Octospi1 Clock gating R110 RCC Octospi1 clock and reset 0 Yes Yes Yes
IOM R111 RIFSC IOManager 0 Yes Yes No
IO voltage protection R0 PWR VDDIO3 & VDDIO4 (PWR_CR1) 1 Yes Yes No
Clock GPIOB R91 RCC GPIO B clock config 0 Yes Yes No
Clock GPIOD R93 RCC GPIO B clock config 0 Yes Yes No
GPIO PD 0, 3-5 R0, 3-5 GPIOD Port 1 config single wire 0 Yes Yes No
GPIO PD 1, 2, 6-11 R1, 2, 6-11 GPIOD Port 1 hyperflash 0 Yes Yes No
GPIO PE 0, 1, 8, 10 R0, 1, 8, 10 GPIOE Port 2 config single wire 0 Yes Yes No
GPIO PE 2-7, 9, 11 R2-7, 9, 11 GPIOE Port 2 hyperflash 0 Yes Yes No


Info white.png Information
OctoSPI1 and OctoSPI2 controllers connected to the physical port thanks to the IO Manager (IOM) which support different modes (direct, swap or muxed). Mode is set by ecosystem SW according to board definition. When executed D1Standby exit procedure, ROM code can't modify IOM configuration set by ecosystem to not disturb rest of the system. It is ecosystem responsibility to set an IOM configuration that guarantee ROM code execution.

3.3.4. FMC raw NAND[edit source]

Checked in the following boot selection:

  • Cortex-A35 main processor
  • Boot from FMC raw NAND
  • Cortex-M33 main processor single boot device
  • Boot from FMC raw NAND
  • Cortex-M33 main processor dual boot device
  • Boot Cortex-M33 from sNOR and Cortex-A35 from FMC raw NAND
  • Boot Cortex-M33 from Hyperflash and Cortex-A35 from FMC raw NAND

The following table list resources associated to FMC.

Function RIF resource number RIF block Resource description Secure level set Check at cold boot Check at Standby exit Check at D1Standby exit
Root Clock FMC R50 [[RCC internal peripheral|RCC] Flexgen 50 0 Yes Yes No
FMC clock gating R112 RCC FMC clock and reset 0 Yes Yes No
Clock GPIOB R91 RCC GPIO B clock config 0 Yes Yes No
Clock GPIOD R93 RCC GPIO D clock config 0 Yes Yes No
Clock GPIOE R94 RCC GPIO E clock config 0 Yes Yes No
IO voltage protection R5 PWR VDDIO2 (PWR_C7) 1 Yes Yes Yes
GPIO PB 13-14 R13-14 GPIOB 8bit config (12 IOs) 0 Yes Yes No
GPIO PD 12,14-15 R12, 14-15 GPIOD 8bit config (12 IOs) 0 Yes Yes No
GPIO PE 6-9, 11-15 R6-9, 11-15 GPIOE 8bit config (12 IOs) 0 Yes Yes No
GPIO PB 5-11 R5-11 GPIOB 16bit config added 0 Yes Yes No
GPIO PD13 R13 GPIOD 16bit config added 0 Yes Yes No
FMC R0 R0 FMC FMC common resource 0 Yes Yes No
FMC R5 R5 FMC FMC NAND controler 0 Yes Yes Yes
Info white.png Information
FMC is a RIF-aware peripheral. Each FMC internal controller could be allocated to a different execution context. That means FMC could be used by Cortex-M33 when ROM code is executing D1Standby exit sequence. As ROM code doesn't know about product definition, ROM code considers that common FMC resources (FMC_R0, clock, associated IOs) are configured by ecosystem SW and is not reconfiguring these items in case of D1Standby exit.

4. ROM code secure context isolation[edit source]

4.1. Principles[edit source]

The STM32MP2 ROM code is SESIP level 3 certified. This implies some guarantees regarding the isolation of the ROM code secure execution. ROM code defines some RIF configuration rules on ecosystem SW to:

  • guarantee that all secure IPs used by ROM code are exclusively assigned to the Cortex-A35 secure context during ROM code execution and can't preempted by another secure processor running in parallel of the ROM code.
  • guarantee that no processor and no bus master peripheral can access secure resources (peripheral and memories) owned by ROM code. That means no master with secure level and CID1 RIF configuration shall be active during ROM code execution

4.2. Rules on Secure SYSRAM[edit source]

SYSRAM is protected by RISAB1 and RISAB2 which are under the control of Cortex-A35 secure context. This is an exception in the RIF as normally all the control of all the RIF units is under the main processor secure context (TDCID) responsibility. This allows to guarantee the SYSRAM isolation during ROM code execution whatever main processor selection.

4.3. Rules on Secure peripherals RIF protection[edit source]

When Cortex-A35 is the main processor, Cortex-A35 secure context controls RIF configuration. When ROM code is running, no other master can modify RIF configuration. Checking access to secure peripheral is enough to guarantee ROM code exclusive access.

When Cortex-M33 is the main processor, the Cortex-M33 secure context controls RIF configuration. When ROM code is running, Cortex-M33 secure context can modify RIF configuration which can compromise ROM code exclusive access. To guarantee ROM code exclusive access to secure peripherals, associated RIF configuration must be locked. In addition to access checking, ROM code also verifies RIF lock status. If not set, ROM code goes in failure mode.

The following table list all RIF locks checked by ROM code in Cortex-M33 main processor, closed-locked boot.

Peripheral RIF resource number RIF block Secure level checked D1Standby exit lock check
BSEC clock R103 RCC 1 Yes
CPU1 boot, reset, IWDG management R70 RCC 1 Yes
CPU PWR1 R2 PWR 1 Yes
STGEN R33 RCC 1 Yes
RNG R92 RIFSC 1 Yes
PKA R93 RIFSC 1 Yes
SAES R94 RIFSC 1 Yes
HASH R95 RIFSC 1 Yes
CRYP1 R96 RIFSC 1 Yes
SYSRAM/RISAB2 R74 RCC 1 Yes
CA35SS R106 RCC 1 Yes

4.4. Rules on master peripherals RIF protection[edit source]

During ROM code execution, it shall not be possible for another master to access peripherals and memories assigned to ROM code secure context (CID1 secure).

For that, ROM code checks RIFSC RIMU configuration to detect any master with CID1 secure configuration:

If the RIF configuration of a master matches CID1 secure one, ROM code verifies if this peripheral is running or not in associated RCC registers (clock enabled). In such case, ROM code goes in failure mode. Note that in case of serial NOR or serial NAND boot, only SDMMC interfaces that are not used for that boot are checked here.

In the case of Cortex-M33 main processor, Cortex-M33 can modify RIFSC RISUP and RIMU during ROM code execution. In addition to access right verification, ROM code also verifies that RIMU and associated RISUP are locked.

The following table sums up the master peripheral RIFSC resources checked by ROM code.

Bus master peripheral RIFSC RIMU index RIFSC RISUP index D1Standby exit RISUP lock check
SDMMC1 1 76 Yes
SDMMC2 2 77 Yes
SDMMC3 3 78 Yes
USB3DR 4 66 Yes
USBH 5 63 Yes
ETH1 6 60 Yes
ETH2 7 61 Yes
PCIE 8 68 Yes
GPU 9 79 Yes
DCMIPP 10 87 Yes
LTDC 11, 12, 13 NA No
VDEC 14 89 Yes
VENC 15 90 Yes

In addition, ROM code checks that no HPDMA channel owned by CID1 secure context is armed.