1. Purpose[edit source]
This article describes how to configure TSN (Time-Sensitive Networking) on switch
This article provides different steps to execute TSN scenario with switch:
- Need synchronization across the network. TSN requires precise time synchronization to ensure that time-critical data is delivered on time and in the correct order.
- TSN 802.1Qav
- TSN 802.1Qbv
2. IEEE 802.1AS-Rev or gPTP synchronization[edit source]
Proprietary PTP stack used for gPTP synchronization, which is provided by TTTech
Deptp is started by default
Basic configuration of the PTP stack is done via configuration file, which has XML format. See /etc/deptp/ptp_config.xml for stack config This stack:
- Start gPTP protocol
- synchronize system time to PTP clock
PTP Management tool called deptp tool can be used to access PTP runtime data from Linux command line. Useful commands:
// Show offset from master watch -n1 deptp_tool --get-current-dataset // Show PTP state of sw0p2 deptp_tool -t1 --get-port-dataset // Show PTP state of sw0p3 deptp_tool -t2 --get-port-dataset
To check if relevant
Time synchro GMAC1 / Switch: GMAC ETH1 must be synchronized to the switch: For Qbv / AVB use case, when the MP25 needs to send “TSN” frames
Pour synchroniser le gmac ETH1 au switch il y adeux méthodes :
- La synchro hw (utilisant un bus hw entre le gmac et le switch) : snps,ext-systime;
- La synchro software : phc2sys -s /dev/ptp2 -c /dev/ptp0 -O 0 &
3. TSN 802.1Qav[edit source]
Maximum 4 Queues supported by GMAC and maximum 8 Queues supported by switch
An example configuration with 4 reserved bandwidth across Switch given below:
- Uses 4 Queues (Q0-Q3). Each Q has a bandwidth reserved in h/w.
- Queue 0 (Yellow stream) has No Bandwidth Restriction, general traffic (Prio 0)
- Queue 1 (Blue stream) has 40% of Maximum bandwidth reserved (400Mbps) (Prio 2)
- Queue 2 (Green stream) has 30% of Maximum bandwidth reserved (300Mbps) (Prio 4)
- Queue 3 (Red stream) has 20% of Maximum bandwidth reserved (200Mbps) (Prio 6)
Q3 is the highest priority Queue and Q0 is the lowest priority
Here are the steps to configure this setup.
Bring up end1/sw0ep interface
ip link add link sw0ep name sw0ep.200 type vlan id 200 ip link set sw0ep.200 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7 ifconfig sw0ep.200 192.168.200.60 netmask 255.255.255.0 bridge vlan add vid 200 dev sw0p1 bridge vlan add vid 200 dev sw0p2 bridge vlan add vid 200 dev sw0p3
CBS is used to enforce a Quality of Service by limiting the data rate of a traffic class, to separate packets into traffic classes the user may choose mqprio(8) https://man7.org/linux/man-pages/man8/tc-mqprio.8.html, and configure it like this:
Network core and Driver uses the skb priority to deliver frames to specific h/w queues. In the above case, priority 6 (packet) goes to Q3, priority 4 goes to Q2, priority 2 goes to Q1 and priority 0 SKB goes to Q0.
./set-cbs-idleslope.sh sw0p3 6 200000 + tsntool fqtss tsa 6 cbs sw0p3 + tsntool fqtss slope 6 200000 sw0p3 + tsntool fqtss show sw0p3 Traffic Class Algorithm operIdleSlope 0 Strict prio n/a 1 Strict prio n/a 2 Strict prio n/a 3 Strict prio n/a 4 Strict prio n/a 5 Strict prio n/a 6 CBS 200000 bps 7 Strict prio n/a
./set-cbs-idleslope.sh sw0p3 4 300000 + tsntool fqtss tsa 4 cbs sw0p3 + tsntool fqtss slope 4 300000 sw0p3 + tsntool fqtss show sw0p3 Traffic Class Algorithm operIdleSlope 0 Strict prio n/a 1 Strict prio n/a 2 Strict prio n/a 3 Strict prio n/a 4 CBS 300000 bps 5 Strict prio n/a 6 CBS 200000 bps 7 Strict prio n/a
./set-cbs-idleslope.sh sw0p3 2 400000 + tsntool fqtss tsa 2 cbs sw0p3 + tsntool fqtss slope 2 400000 sw0p3 + tsntool fqtss show sw0p3 Traffic Class Algorithm operIdleSlope 0 Strict prio n/a 1 Strict prio n/a 2 CBS 400000 bps 3 Strict prio n/a 4 CBS 300000 bps 5 Strict prio n/a 6 CBS 200000 bps 7 Strict prio n/a
With set-cbs-idleslope.sh :
#!/bin/bash #implemented for tsntool 2.4.0 if "$#" -ne 3 ; then echo "Usage: $0 port traffic-class idleSlope" exit 1 fi port=$1 trafficClass=$2 idleSlope=$3 set -x tsntool fqtss tsa $trafficClass cbs $port tsntool fqtss slope $trafficClass $idleSlope $port tsntool fqtss show $port
Run 4 iperf sessions to generate several streams with different priorities. Remote PC or other device connected to sw0p3 (ETH1) with IP address 192.168.200.30, and other device/PC connected to sw0p2 (ETH3) to launch 2 x iperf3 client to generate streams.
Run 4 iperf sessions to generate several streams with different priorities Remote PC or other device connected to sw0p3 with IP address 192.168.200.30
iperf3 -s -p 5003& iperf3 -s -p 5002& iperf3 -s -p 5001& iperf3 -s -p 5000&
Remote PC or other device connected to sw0p2 with IP address 192.168.200.40
//Stream with SKB priority 6 : TOS=0x14 == SO_PRIORITY=6 // https:man7.org/linux/man-pages/man8/tc-prio.8.html iperf3 -c 192.168.200.30 -u -b 0 -p 5003 -l1472 -t60 --tos 0x14 &
//Stream with SKB priority 4 iperf3 -c 192.168.200.30 -u -b 0 -p 5002 -l1472 -t60 --tos 0x1a &
At DUT, start transmission of stream using iperf3
//Stream with SKB priority 2 iperf3 -c 192.168.200.30 -u -b 0 -p 5001 -l1472 -t60 --tos 0xa &
//Stream with SKB priority 0 (Best effort) iperf3 -c 192.168.200.30 -u -b 0 -p 5000 -l1472 -t60 &
Result without set-cbs-idleslope.sh rule apply :
For Traffic with priority 6:
[ 5] 0.00-60.85 sec 3.33 GBytes 470 Mbits/sec 0.009 ms 949906/3376499 (28%) receiver
For Traffic with priority 4:
[ 5] 0.00-60.00 sec 1.84 GBytes 264 Mbits/sec 0.061 ms 144921/1489033 (9.7%) receiver
For Traffic with priority 2:
[ 5] 0.00-60.00 sec 276 MBytes 38.6 Mbits/sec 0.072 ms 1783276/1979848 (90%) receiver
For Traffic with priority 0 (Best effort):
[ 5] 0.00-60.00 sec 2.02 GBytes 290 Mbits/sec 0.019 ms 2278581/3755507 (61%) receiver
Without CBS TSN rules in place, multiple traffic streams may contend for network resources, causing congestion and possible packet loss. This can lead to poor network performance and lower quality of service for users. Furthermore, without CBS TSN rules, there no prioritization of important traffic, such as real-time audio or video streams, which can cause delays and interruptions in these applications. In summary, the absence of CBS TSN rules can create an unstable and undependable network environment.
Result with set-cbs-idleslope.sh rule apply:
For Queue 3 with priority 6 and with BW of 200Mbps:
[ 5] 0.00-60.00 sec 1.72 GBytes 246 Mbits/sec 0.052 ms 189322/1444777 (13%) receiver
For Queue 2 with priority 4 and with BW of 300Mbps:
[ 5] 0.00-60.00 sec 1.16 GBytes 167 Mbits/sec 0.064 ms 110342/959769 (11%) receiver
For Queue 1 with priority 2 and with BW of 400Mbps:
[ 5] 0.00-60.00 sec 276 MBytes 38.6 Mbits/sec 0.072 ms 1783276/1979848 (90%) receiver
For Queue0 with priority 0 (Best effort):
[ 5] 0.00-60.00 sec 2.31 GBytes 331 Mbits/sec 0.006 ms 234299/1921970 (12%) receiver
When TSN rules are implemented, the network can provide guaranteed bandwidth allocation and prioritization for different traffic streams. CBS TSN rules allow for the allocation of credits to different traffic streams, which can be used to transmit data over the network. This ensures that critical traffic, such as real-time audio or video streams, receive the necessary bandwidth and are not affected by other traffic streams. CBS TSN rules also prevent congestion and packet loss by limiting the amount of data that can be transmitted by each traffic stream. This results in a more predictable and reliable network environment, with improved quality of service for users.
4. TSN 802.1Qbv[edit source]
An example configuration with 4 schedule entries given below:
- Uses 4 Queues (Q0-Q3). Each Q has a Gate associated in h/w. Maximum 4 Queues/Gates supported
- 3 higher priority Gates open for 125usec (Q1, Q2 and Q3)
- Q3 is the higest priority Queue and Q0 is the lowest priority
- 1 lower priority (Q0) opens remaining gates for 250 usec
Here are the steps to configure this schedule.
Bring up end0 interface
ip link add link end0 name end0.200 type vlan id 200 ip link set end0.200 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7 ifconfig end0.200 192.168.200.60 netmask 255.255.255.0
Setup EST schedule with 4 Gates (Q0-Q3). For description of Command parameters, see manual page for taprio. https://man7.org/linux/man-pages/man8/tc-taprio.8.html TC0 <-> Q0, TC1 <-> Q1, TC2 <-> Q2 and TC3 <-> Q3
tc qdisc replace dev end0 parent root handle 100 taprio \ num_tc 4 \ map 0 0 1 1 2 2 3 3 3 3 3 3 3 3 3 3 \ queues 1@0 1@1 1@2 1@3 \ base-time 0000 \ sched-entry S 8 125000 \ sched-entry S 4 125000 \ sched-entry S 2 125000 \ sched-entry S 1 250000 \ sched-entry S 0 375000 \ flags 2
Where num_tc is same as number of queues = 4, maps 16 priorities to one of 4 TCs, queues specify the Queue associated with each TC, TC0 - One queue @0, TC1 - One queue @1, TC2 - One queue @2 and TC3 - One queue @3
sched-entry S 8 125000 S - SetGateStates operation 8 - Bit mask showing bit 4 set (Q3/TC3) 125000 - 125000 nsecs (125 usecs ) duration of Gate open The cycle-time is 1 msec (which is the sum of the intervals of individual schedule)
Enable classifier. Classifier is used to mark the packet based on packet meta data.
tc qdisc add dev end0 clsact
Network core and Driver uses the skb priority to deliver frames to specific h/w queues. In the above case, priority 6 to 15 SKB (packet) goes to Q3 (4th entry in map in the tc qdisc command), priority 4 to 5 SKB goes to Q2 (3rd entry in map) priority 2 to 3 SKB goes to Q1 (2nd entry in map) and priority 0 to 1 SKB goes to Q0 (1st entry in map)
Run 4 iperf sessions to generate several streams with different priorities Remote PC or other device connected to end0 with IP address 192.168.200.30
iperf3 -s -p 5003& iperf3 -s -p 5002& iperf3 -s -p 5001& iperf3 -s -p 5000&
At DUT, start transmission of stream using iperf3
//Stream with SKB priority 6 : TOS=0x14 == SO_PRIORITY=6 // https:man7.org/linux/man-pages/man8/tc-prio.8.html iperf3 -c 192.168.200.30 -u -b 0 -p 5003 -l1472 -t60 --tos 0x14 &
//Stream with SKB priority 4 iperf3 -c 192.168.200.30 -u -b 0 -p 5002 -l1472 -t60 --tos 0x1a &
//Stream with SKB priority 2 iperf3 -c 192.168.200.30 -u -b 0 -p 5001 -l1472 -t60 --tos 0xa &
//Stream with SKB priority 0 (Best effort) iperf3 -c 192.168.200.30 -u -b 0 -p 5000 -l1472 -t60 &
Result without tc rule apply :
Result with tc rule apply:
5. References[edit source]