How to configure TSN switch

Revision as of 15:30, 10 November 2023 by Registered User (→‎TSN 802.1Qav)
Applicable for STM32MP25x lines

1. Purpose[edit source]

This article describes how to configure TSN (Time-Sensitive Networking) on switch
This article provides different steps to execute TSN scenario with switch:

  • Need synchronization across the network. TSN requires precise time synchronization to ensure that time-critical data is delivered on time and in the correct order.
  • TSN 802.1Qav
  • TSN 802.1Qbv

The choice between 802.1Qav and 802.1Qbv depends on the specific requirements of the application. 802.1Qav is typically used in applications where bandwidth requirements are variable and unpredictable, while 802.1Qbv is typically used in applications where bandwidth requirements are fixed and predictable.

2. IEEE 802.1AS-Rev or gPTP synchronization[edit source]

PTP is a protocol that enables the synchronization of clocks in a network. It uses a master-slave architecture, where one device acts as the master clock and the other devices act as slave clocks. The master clock sends synchronization messages to the slave clocks, which adjust their clocks to match the master clock.

Proprietary PTP stack used for gPTP synchronization, which is provided by TTTech

Deptp is started by default

Basic configuration of the PTP stack is done via configuration file, which has XML format. See /etc/deptp/ptp_config.xml for stack config This stack:

  • Start gPTP protocol
  • synchronize system time to PTP clock

PTP Management tool called deptp tool can be used to access PTP runtime data from Linux command line. Useful commands:

// Show offset from master
watch -n1 deptp_tool --get-current-dataset
 
// Show PTP state of sw0p2
deptp_tool -t1 --get-port-dataset

// Show PTP state of sw0p3
deptp_tool -t2 --get-port-dataset
Warning white.png Warning
Be careful if you are using PHY which managed “low power mode” (i.e EEE)

Most of the time this feature is not compatible with TSN. To be considered “asCapable” the maximum acceptable value for neighborPropDelayThresh is 800ns (default value), if you need to tune this value you can add in your Interface describe in XML ptp_config file: <delay_thresh>800</delay_thresh> and update value




To check if relevant

Time synchro GMAC1 / Switch: GMAC ETH1 must be synchronized to the switch: For Qbv / AVB use case, when the MP25 needs to send “TSN” frames

Pour synchroniser le gmac ETH1 au switch il y adeux méthodes :

  • La synchro hw (utilisant un bus hw entre le gmac et le switch) : snps,ext-systime;
  • La synchro software : phc2sys -s /dev/ptp2 -c /dev/ptp0 -O 0 &

3. TSN 802.1Qav[edit source]

In TSN 802.1Qav or CBS (Credit-Based Shaper), each device is assigned a credit value that determines the amount of data it can transmit. The credit value is based on the bandwidth requirements of the device and the available bandwidth in the network. Devices with higher bandwidth requirements are assigned more credits, while devices with lower bandwidth requirements are assigned fewer credits.

As data is transmitted across the network, the credit values are decremented. When a device runs out of credits, it can no longer transmit data until it receives more credits. This ensures that time-critical traffic is given priority over other traffic, as devices with higher bandwidth requirements are able to transmit more data.

An example configuration with 2 reserved bandwidth given below:

  • Uses 2 Queues (Q0-Q1). Each Q has a bandwidth reserved in h/w.

Maximum 4 Queues supported by GMAC and maximum 8 Queues supported by switch

  • Queue 0 has No Bandwidth Restriction, general traffic
  • Queue 1 has 40% of Maximum bandwidth reserved (400Mbps)
  • Q1 is the highest priority Queue and Q0 is the lowest priority
File:Cbs switch streams.png
Streams across the switch

Here are the steps to configure this setup.

Warning white.png Warning
If you want to perform CBS test, gPTP synchronization is not needed


Bring up end0 interface

ip link add link end0 name end0.200 type vlan id 200
ip link set end0.200 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
ifconfig end0.200 192.168.200.60 netmask 255.255.255.0

CBS is used to enforce a Quality of Service by limiting the data rate of a traffic class, to separate packets into traffic classes the user may choose mqprio(8) https://man7.org/linux/man-pages/man8/tc-mqprio.8.html, and configure it like this:

 tc qdisc add dev end0 clsact
 tc qdisc add dev end0 handle 100: parent root mqprio \
  num_tc 4 \
  map 0 0 1 1 2 2 3 3 3 3 3 3 3 3 3 3 \
  queues 1@0 1@1 1@2 1@3 hw 0

Configure Bandwidth allocated for each queue (https://man7.org/linux/man-pages/man8/tc-cbs.8.html)

 // Set bandwidth of queue 1 to be 100Mbps
 tc qdisc replace dev end0 parent 100:2 cbs \
  idleslope 100000 \
  sendslope -900000 \
  hicredit 150 \
  locredit -1350 \
  offload 1
 // Set bandwidth of queue 2 to be 200Mbps
 tc qdisc replace dev end0 parent 100:3 cbs \
  idleslope 200000 \
  sendslope -800000 \
  hicredit 300 \
  locredit -1200 \
  offload 1
 // Set bandwidth of queue 3 to be 300Mbps
 tc qdisc replace dev end0 parent 100:4 cbs \
  idleslope 300000 \
  sendslope -700000 \
  hicredit 450 \
  locredit -1050 \
  offload 1

So for queue 0 the bandwidth should be around 400Mbps (port_transmit_rate - sum of all bandwidth of each queue)

sendslope = idleslope - port_transmit_rate
hicredit = max_interference_size * (idleslope / port_transmit_rate) locredit = max_frame_size * (sendslope / port_transmit_rate) with max_interference_size = max_frame_size = 1500

For more details: https://en.wikipedia.org/wiki/Time-Sensitive_Networking#IEEE_802.1Qav_Forwarding_and_queuing_enhancements_for_time-sensitive_streams

Network core and Driver uses the skb priority to deliver frames to specific h/w queues. In the above case, priority 6 to 15 SKB (packet) goes to Q3 (4th entry in map in the tc qdisc command), priority 4 to 5 SKB goes to Q2 (3rd entry in map) priority 2 to 3 SKB goes to Q1 (2nd entry in map) and priority 0 to 1 SKB goes to Q0 (1st entry in map)

Run 4 iperf sessions to generate several streams with different priorities Remote PC or other device connected to end0 with IP address 192.168.200.30

iperf3 -s -p 5003&
iperf3 -s -p 5002&
iperf3 -s -p 5001&
iperf3 -s -p 5000&

At DUT, start transmission of stream using iperf3

//Stream with SKB priority 6  : TOS=0x14 == SO_PRIORITY=6
// https:man7.org/linux/man-pages/man8/tc-prio.8.html
iperf3 -c 192.168.200.30 -u -b 0 -p 5003 -l1472 -t60 --tos 0x14 &
//Stream with SKB priority 4
iperf3 -c 192.168.200.30 -u -b 0 -p 5002 -l1472 -t60 --tos 0x1a &
//Stream with SKB priority 2
iperf3 -c 192.168.200.30 -u -b 0 -p 5001 -l1472 -t60 --tos 0xa &
//Stream with SKB priority 0 (Best effort)
iperf3 -c 192.168.200.30 -u -b 0 -p 5000 -l1472 -t60  &

Result without tc rule apply :
For Traffic with priority 6:

[  5]   0.00-60.00  sec  1.40 GBytes   200 Mbits/sec  0.046 ms  11841/1031880 (1.1%)  receiver

For Traffic with priority 4:

[  5]   0.00-60.00  sec  40.1 MBytes  5.60 Mbits/sec  39.651 ms  936/29490 (3.2%)  receiver

For Traffic with priority 2:

[  5]   0.00-60.00  sec  4.94 GBytes   707 Mbits/sec  0.035 ms  164701/3768910 (4.4%)  receiver

For Traffic with priority 0 (Best effort):

[  5]   0.00-60.00  sec   106 MBytes  14.8 Mbits/sec  0.017 ms  1765/76956 (2.3%)  receiver

Without CBS TSN rules in place, multiple traffic streams may contend for network resources, causing congestion and possible packet loss. This can lead to poor network performance and lower quality of service for users. Furthermore, without CBS TSN rules, there no prioritization of important traffic, such as real-time audio or video streams, which can cause delays and interruptions in these applications. In summary, the absence of CBS TSN rules can create an unstable and undependable network environment.

Result with tc rule apply:
For Queue 3 with priority 6 and with BW of 300Mbps:

[  5]   0.00-60.00  sec  1.72 GBytes   246 Mbits/sec  0.052 ms  189322/1444777 (13%)  receiver

For Queue 2 with priority 4 and with BW of 200Mbps:

[  5]   0.00-60.00  sec  1.16 GBytes   167 Mbits/sec  0.064 ms  110342/959769 (11%)  receiver

For Queue 1 with priority 2 and with BW of 100Mbps:

[  5]   0.00-60.00  sec   641 MBytes  89.6 Mbits/sec  0.266 ms  32740/489287 (6.7%)  receiver

For Queue0 with priority 0 (Best effort):

[  5]   0.00-60.00  sec  2.31 GBytes   331 Mbits/sec  0.006 ms  234299/1921970 (12%)  receiver

When TSN rules are implemented, the network can provide guaranteed bandwidth allocation and prioritization for different traffic streams. CBS TSN rules allow for the allocation of credits to different traffic streams, which can be used to transmit data over the network. This ensures that critical traffic, such as real-time audio or video streams, receive the necessary bandwidth and are not affected by other traffic streams. CBS TSN rules also prevent congestion and packet loss by limiting the amount of data that can be transmitted by each traffic stream. This results in a more predictable and reliable network environment, with improved quality of service for users.

4. TSN 802.1Qbv[edit source]

802.1Qbv (Time-Aware Shaper) is a traffic scheduling technique that uses time-based scheduling to ensure that time-critical traffic is given priority over other traffic. It assigns time slots to each device based on its priority level.

An example configuration with 4 schedule entries given below:

  • Uses 4 Queues (Q0-Q3). Each Q has a Gate associated in h/w. Maximum 4 Queues/Gates supported
  • 3 higher priority Gates open for 125usec (Q1, Q2 and Q3)
  • Q3 is the higest priority Queue and Q0 is the lowest priority
  • 1 lower priority (Q0) opens remaining gates for 250 usec

Here are the steps to configure this schedule.

Warning white.png Warning
Be careful if you want to perform QBV test, you need to start gPTP synchronization before


Bring up end0 interface

ip link add link end0 name end0.200 type vlan id 200
ip link set end0.200 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
ifconfig end0.200 192.168.200.60 netmask 255.255.255.0

Setup EST schedule with 4 Gates (Q0-Q3). For description of Command parameters, see manual page for taprio. https://man7.org/linux/man-pages/man8/tc-taprio.8.html TC0 <-> Q0, TC1 <-> Q1, TC2 <-> Q2 and TC3 <-> Q3

 tc qdisc replace dev end0 parent root handle 100 taprio \
  num_tc 4 \
  map 0 0 1 1 2 2 3 3 3 3 3 3 3 3 3 3 \
  queues 1@0 1@1 1@2 1@3 \
  base-time 0000 \
  sched-entry S 8 125000 \
  sched-entry S 4 125000 \
  sched-entry S 2 125000 \
  sched-entry S 1 250000 \
  sched-entry S 0 375000 \
  flags 2

Where num_tc is same as number of queues = 4, maps 16 priorities to one of 4 TCs, queues specify the Queue associated with each TC, TC0 - One queue @0, TC1 - One queue @1, TC2 - One queue @2 and TC3 - One queue @3

 sched-entry S 8 125000
 S - SetGateStates operation
 8 - Bit mask showing bit 4 set (Q3/TC3)
 125000 - 125000 nsecs (125 usecs ) duration of Gate open
 The cycle-time is 1 msec (which is the sum of the intervals of individual schedule)

Enable classifier. Classifier is used to mark the packet based on packet meta data.

 tc qdisc add dev end0 clsact

Network core and Driver uses the skb priority to deliver frames to specific h/w queues. In the above case, priority 6 to 15 SKB (packet) goes to Q3 (4th entry in map in the tc qdisc command), priority 4 to 5 SKB goes to Q2 (3rd entry in map) priority 2 to 3 SKB goes to Q1 (2nd entry in map) and priority 0 to 1 SKB goes to Q0 (1st entry in map)

Run 4 iperf sessions to generate several streams with different priorities Remote PC or other device connected to end0 with IP address 192.168.200.30

iperf3 -s -p 5003&
iperf3 -s -p 5002&
iperf3 -s -p 5001&
iperf3 -s -p 5000&

At DUT, start transmission of stream using iperf3

//Stream with SKB priority 6  : TOS=0x14 == SO_PRIORITY=6
// https:man7.org/linux/man-pages/man8/tc-prio.8.html
iperf3 -c 192.168.200.30 -u -b 0 -p 5003 -l1472 -t60 --tos 0x14 &
//Stream with SKB priority 4
iperf3 -c 192.168.200.30 -u -b 0 -p 5002 -l1472 -t60 --tos 0x1a &
//Stream with SKB priority 2
iperf3 -c 192.168.200.30 -u -b 0 -p 5001 -l1472 -t60 --tos 0xa &
//Stream with SKB priority 0 (Best effort)
iperf3 -c 192.168.200.30 -u -b 0 -p 5000 -l1472 -t60  &

Result without tc rule apply :

Alternate text
schedule without QBV rule: it's anarchy

Result with tc rule apply:

Alternate text
schedule with QBV rule: each traffic has its time frame

5. References[edit source]