Touchscreen hardware components

Revision as of 13:45, 23 October 2023 by Registered User (→‎Goodix GT9147)
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines


1. Article purpose[edit source]

The purpose of this article is to:

  • list the touchscreen hardware components that might be integrated in the different boards
  • link these components to the corresponding software framework(s)
  • point to the datasheet(s) of these components
  • explain, when necessary, how to configure these components

2. Software frameworks[edit source]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Visual and Inputs Goodix GT9147 Inputs framework[1] Touchscreen input driver
Visual and Inputs FocalTech FT6236 Inputs framework[1] Touchscreen input driver

3. Goodix GT9147[edit source]

The Goodix GT9147 is a single-layer multi-touch capacitive touch controller driver.

For details and the datasheet please contact the GT9147 driver provider.

Info white.png Information
This touchscreen controller driver can be found on some STM32MP15 Evaluation boards.

3.1. Linux driver[edit source]

Bindings: Documentation/devicetree/bindings/input/touchscreen/goodix.yaml

Sources: drivers/input/touchscreen/goodix.c

Devicetree example: arch/arm/boot/dts/stm32mp157d-ev1.dts

...
&dsi {
	#address-cells = <1>;
	#size-cells = <0>;
	status = "okay";

	ports {
		#address-cells = <1>;
		#size-cells = <0>;

		port@0 {
			reg = <0>;
			dsi_in: endpoint {
				remote-endpoint = <&ltdc_ep0_out>;
			};
		};

		port@1 {
			reg = <1>;
			dsi_out: endpoint {
				remote-endpoint = <&dsi_panel_in>;
			};
		};
	};

	panel_dsi: panel-dsi@0 {
		compatible = "raydium,rm68200";
		reg = <0>;
		reset-gpios = <&gpiof 15 GPIO_ACTIVE_LOW>;
		backlight = <&panel_backlight>;
		power-supply = <&v3v3>;
		status = "okay";

		port {
			dsi_panel_in: endpoint {
				remote-endpoint = <&dsi_out>;
			};
		};
	};
};


&i2c2 {
...
	stmfx: stmfx@42 {
		compatible = "st,stmfx-0300";
		reg = <0x42>;
		interrupts = <8 IRQ_TYPE_EDGE_RISING>;
		interrupt-parent = <&gpioi>;
		vdd-supply = <&v3v3>;

		stmfx_pinctrl: pinctrl {
			compatible = "st,stmfx-0300-pinctrl";
			gpio-controller;
			#gpio-cells = <2>;
			interrupt-controller;
			#interrupt-cells = <2>;
			gpio-ranges = <&stmfx_pinctrl 0 0 24>;

			goodix_pins: goodix {
				pins = "gpio14";
				bias-pull-down;
			};

			joystick_pins: joystick-pins {
				pins = "gpio0", "gpio1", "gpio2", "gpio3", "gpio4";
				bias-pull-down;
			};
		};
	};

	gt9147: goodix-ts@5d {
		compatible = "goodix,gt9147";
		reg = <0x5d>;
		panel = <&panel_dsi>;
		pinctrl-0 = <&goodix_pins>;
		pinctrl-names = "default";
		AVDD28-supply = <&v3v3>;
		VDDIO-supply = <&v3v3>;
		status = "okay";

		interrupts = <14 IRQ_TYPE_EDGE_RISING>;
		interrupt-parent = <&stmfx_pinctrl>;
	};
};

4. FocalTech FT6236[edit source]

The FocalTech FT6236 is a self-capacitive touch panel controller driver.

For details and the datasheet please contact the FT6236 driver provider.

4.1. Linux driver[edit source]

Bindings: Documentation/devicetree/bindings/input/touchscreen/edt-ft5x06.yaml

Sources: drivers/input/touchscreen/edt-ft5x06.c

5. References[edit source]

  1. 1.0 1.1 Linux Input Subsystem kernel API and userspace API