1. Article purpose[edit source]
This section details the TF-M stage (Trusted Firmware-M).
It explains how to configure and build TF-M in STM32 MPU context, describes the build process from sources, and shows how to deploy it on your target.
2. Source code access and build process[edit source]
2.1. Prerequisites[edit source]
2.1.1. Linux® PC[edit source]
2.1.1.1. Install build environment[edit source]
install dependencies:
sudo apt-get install -y git curl wget build-essential libssl-dev python3 \ python3-pip cmake make
add CMake path into environment:
export PATH=<CMake path>/bin:$PATH
2.1.1.2. Install python dependencies[edit source]
From the TF-M source code installed in your PC:
pip3 install --upgrade pip \ pip3 install -r tools/requirements.txt
2.1.1.3. Install a toolchain[edit source]
If you use STM32CubeIDE, you do not need to install a toolchain as STM32CubeIDE uses its own toolchain
If you build by command line, you can use the toolchain from the SDK OSTL and you need to update the path as follow:
export PATH=$PATH:$<SDK installation directory>/sysroots/x86_64-ostl_sdk-linux/usr/share/gcc-arm-none-eabi/bin
2.1.2. Windows PC[edit source]
2.1.2.1. Install build environment[edit source]
install dependencies:
- Git client latest version (https://git-scm.com/download/win) - CMake (`native Windows version <https://cmake.org/download/>`) - GNU make (http://gnuwin32.sourceforge.net/packages/make.htm) - Python3 `(native Windows version) <https://www.python.org/downloads/>` and the pip package manager (from Python 3.4 it's included)
add CMake path into environment:
set PATH=<CMake_Path>\bin;%PATH%
2.1.2.2. Install python dependencies[edit source]
From the TF-M source code installed in your PC:
cd trusted-firmware-m \ pip3 install -r tools/requirements.txt
2.1.2.3. Install a toolchain[edit source]
If you use STM32CubeIDE, you do not need to install a toolchain as STM32CubeIDE uses its own toolchain
If you build by command line, you can use the toolchain from STM32CubeIDE and you need to update the path as follow in your .bashrc:
- PATH="/c/ST/<STM32 CubeIDE path>/STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.2.202309201523\tools\bin":$PATH
Note: plugin version can differ from a STM32CubeIDE version to another, so you should adapt it accordingly
2.2. Install sources[edit source]
2.2.1. From the Developer package[edit source]
Not available in developer package...
2.2.2. Official source tree[edit source]
Download the source code from the official Trusted Firmware-A git repository.
git clone https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git/
For a full-featured software, go to STMicroelectronics github:
git clone https://github.com/STMicroelectronics/trusted-firmware-m.git git clone https://github.com/STMicroelectronics/tf-m-tests.git
2.2.3. Distribution Package[edit source]
Not possible to build TF-M inside distribution package.
2.3. Build process[edit source]
2.3.1. TF-M Build flags[edit source]
Generic build flags for TF-A are described in the Build Options page of the official TF-A documentation[1].
Generic build flags for STM32 MPU platforms can be found in the build instruction chapter in docs/plat/st/stm32mpus.rst .
Specific STM32MP1 series platform flags can be found in the build instruction chapter of the official TF-A documentation [2].
Specific STM32MP2 series platform flags can be found in the build instruction chapter in docs/plat/st/stm32mp2.rst .
Other optional flags:
- CONFIG_STM32MP25X_REVA (only for STM32MP2 series): Set this flag to 1 if the STM32MP2 chip is a revision A. Default: 0 (chip revision B)
- STM32MP1_OPTEE_IN_SYSRAM (only for STM32MP15x lines
): To put OP-TEE pager in SYSRAM. Default: 0 (OP-TEE is in DDR)
- STM32MP_FORCE_MTD_START_OFFSET = <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout).
2.4. Build command[edit source]
2.4.1. Build command details[edit source]
For example, default build command for STM32MP25 EV1 board is:
cmake -S <SRC_DIRECTORY> -B <BUILD_DIRECTORY> \ -DTFM_PLATFORM=stm/stm32mp257f_ev1 \ -DTFM_TOOLCHAIN_FILE=toolchain_GNUARM.cmake \ -DTFM_PROFILE=profile_small \ -DCMAKE_BUILD_TYPE=debug \ -DNS=OFF
Example mp25 ev1 board in profile medium:
cmake -S . -B build \ -DTFM_PLATFORM=stm/stm32mp257f_ev1 \ -DTFM_TOOLCHAIN_FILE=toolchain_GNUARM.cmake \ -DTFM_PROFILE=profile_medium \ -DCMAKE_BUILD_TYPE=debug \ -DNS=OFF
2.4.2. OSTL device tree for STM32MP2 series[edit source]
For STM32MP257F-EV1 Evaluation board , ST provides OSTL device tree configurations in a dedicated git repository: tf-a/stm32mp257f-ev1-ca35tdcid-ostl.dts . You can use the
git submodule
command:
git submodule add https://github.com/STMicroelectronics/dt-stm32mp fdts/external-dt make PLAT=stm32mp2 DTB_FILE_NAME=stm32mp257f-ev1-ca35tdcid-ostl.dtb STM32MP_SDMMC=1 \ SPD=opteed STM32MP_DDR4_TYPE=1
or git clone
command with TFA_EXTERNAL_DT:
git clone https://github.com/STMicroelectronics/dt-stm32mp ${DT_PATH} make PLAT=stm32mp2 DTB_FILE_NAME=stm32mp257f-ev1-ca35tdcid-ostl.dtb STM32MP_SDMMC=1 \ SPD=opteed STM32MP_DDR4_TYPE=1 TFA_EXTERNAL_DT=${DT_PATH}/tf-a
Here DT_PATH can be chosen to whatever you wish, but it must not be a relative path, for example:
export DT_PATH=`pwd`/../dt-stm32mp
2.5. Final image[edit source]
The final image is available for Flash memory or SDCard update in the corresponding folder:
<BUILD_PLAT>/tf-a-<board>.stm32 Ex: build/stm32mp1/release/tf-a-stm32mp157c-ev1.stm32