1. Introduction[edit source]
ThreadX is a real-time operating system (RTOS), designed for embedded systems.
It offers two functional modes:
- Common mode: Contains the common RTOS functionalities such as thread management and synchronization, memory pool management, messaging, and event handling.
- Module mode: An advanced usage mode that allows loading and unloading of pre-linked ThreadX modules on-the-fly through a module manager.
The ThreadX core provides the common RTOS features, such as management of threads, semaphores, mutexes and SW timers. The block diagram below shows the different functional blocks in the ThreadX core.
The Azure RTOS ThreadX library has a FreeRTOS compatibility layer. This adaptation layer allows the user to develop a ThreadX application using FreeRTOS APIs.
1.1. Unique features[edit source]
ThreadX offers a set of unique features that give higher flexibility to the user:
- Various scheduling policies and preemption threshold [1]
- On-the-fly properties update [2]
- Object notifications [3]
- Event chaining [4]
- Runtime performance information [5]
- Tracing mechanism [6]
1.2. Folder/file structure[edit source]
- common: Contains the implementation of all ThreadX APIs. It also provides some utility features such as: SW timers, performance information and tracing.
- common_modules: Contains the implementation of the ThreadX Module feature, allowing dynamic loading of a prelinked ThreadX module. It is split into two folders:
- module_lib: implements the txm_*.c API and should be used instead of tx_*.c when writing a ThreadX module.
- module_manager: implements the functional block to be put on top of the ThreadX core to handle module loading, unloading, running, and so on.
- ports/<core>/<compiler>: contains the implementation of the kernel scheduler, mostly in assembly language.
- ports_module/<core>/<compiler>: contains the implementation of the ThreadX module related scheduler to fit with Module Manager requirements. The files in this directory are used instead of the port's files when the ThreadX Module is enabled.
Further details of the ThreadX features are available in the official documentation[7]
2. STM32 integration[edit source]
There are two possible modes: Common Mode and Module Mode.
2.1. Common mode[edit source]
To correctly run ThreadX on STM32-based MPUs, the application should provide the 3 following user-level files:
- tx_initialize_low_level.s: Implements the tx_initialize_low_level() function called by the threadX kernel to initialize the RTOS heap base address and setup the SYSTick_Handler().
As tx_initialize_low_level.s is compiler and core dependent, a template of this file is provided for each compiler/core in the ThreadX source tree.
- stm32XXX_hal_timebase_tim.c: Implements a timebase used by the HAL drivers, as the systick is reserved for the ThreadX kernel scheduler.
- tx_user.h: Configures the ThreadX RTOS using some of defines. A template for this file is provided in the ThreadX source tree. It is included in the ThreadX stack by the define TX_INCLUDE_USER_DEFINE_FILE.
2.2. Module mode[edit source]
In addition to the common mode files, which need to be kept on the module manager side, the application should provide the following user-level file on the module side.
- txm_module_preamble.s: A preamble is required with each module to expose the module configuration to the Module Manager. The preamble contains particular information such as the module unique ID and attributes.
3. CMSIS-RTOS API Support[edit source]
The CMSIS-RTOS v2 (CMSIS-RTOS2) provides generic RTOS interfaces for Arm® Cortex® processor-based devices. It provides a standardized API for software components that require RTOS functionality.
The list of features supported for ThreadX is as follows:
Feature | Supported | Short description |
---|---|---|
Kernel information and control | Y | Provides version/system information and starts/controls the RTOS Kernel. More… |
Thread management | Y | Defines, creates, and controls thread functions. More… |
Thread flags | N | Synchronizes threads using flags. More… |
Event flags | Y | Synchronizes threads using event flags. More… |
Generic wait functions | Y | Waits for a certain period of time. More… |
Timer management | Y | Creates and controls timer and timer callback functions. More… |
Mutex management | Y | Synchronizes resource access using Mutual Exclusion (Mutex). More… |
Semaphores | Y | Accesses shared resources simultaneously from different threads. More… |
Memory pool | N | Manages thread-safe fixed-size blocks of dynamic memory. More… |
Message queue | Y | Exchanges messages between threads in a FIFO-like operation. More… |
For further information about CMSIS-RTOS v2 APIs, refer to the ARM manual: CMSIS-RTOS API v2.
For further information about the implementation of CMSIS-RTOS wrapper for ThreadX, refer to its readme file.
4. FreeRTOS API Support[edit source]
The FreeRTOS adaptation layer for ThreadX provides a set of APIs to configure, initialize and use ThreadX through FreeRTOS APIs. API support by category:
- task creation, control and utilities
- semaphores and mutexes
- queues
- queue sets
- direct to task notifications
- software timers
- event groups
ThreadX flags required configuration:
Name | Default value | Description |
---|---|---|
configUSE_16_BIT_TICKS | 0 | Set to 1 to use 16-bit tick. |
configSTACK_DEPTH_TYPE | uint16_t | Use to override the type used to specify stack depth. |
configTICK_RATE_HZ | - | Set the kernel tick rate, used by the pdMS_TO_TICKS() macro. |
configMAX_PRIORITIES | - | Maximum number of priorities. Must be less than or equal to the configured number of ThreadX priorities. |
configMINIMAL_STACK_SIZE | 512U | Minimum stack size, used as the stack size of the idle task if TX_FREERTOS_IDLE_STACK is not defined. |
configTOTAL_HEAP_SIZE | - | Amount of internal memory allocated to the adaptation layer when creating FreeRTOS objects. Can be set to 0 to disable dynamic allocation. |
INCLUDE_vTaskDelete | 1 | Set to 0 to disable the task delete API. When disabled, the adaptation layer does not create the idle task in order to save resources. |
TX_FREERTOS_IDLE_STACK | 512U | Define to a macro invoked on internal assertion failures from within the adaptation layer. |
configASSERT | - | Define to a macro invoked for invalid arguments. |
For more information about the implementation of the FreeRTOS adaptation layer for ThreadX, refer to its readme file [8]
5. How to use[edit source]
5.1. Common mode[edit source]
1. In order to initialize and configure the Azure RTOS ThreadX kernel, the user must include the "tx_api.h" file.
2. Call tx_kernel_enter function from the main.
/* Start the ThreadX kernel */
tx_kernel_enter();
This function initializes the internal ThreadX data structure before calling the application’s definition function (tx_application_define) and starting the scheduler.
3. The user must also properly define the initial system resources in the tx_application_define function. Examples of system resources include threads, queues, memory pools, event flag groups, mutexes, timers and semaphores.
VOID tx_application_define(VOID *first_unused_memory)
{
VOID *memory_ptr = first_unused_memory;
/* USER CODE BEGIN tx_application_define */
/* User can add his own implementation to define the initial ThreadX system resources*/
/* USER CODE END tx_application_define */
}
The input parameter of tx_application_define is the first available RAM address to be used for the run-time memory allocation of thread stacks, queues and memory pools.
4. Initialize system resources using ThreadX APIs :
- Thread creation using ThreadX API :
/* Create ThreadOne. */
if (tx_thread_create(&ThreadOne, "Thread One", ThreadOne_Entry, 0,
pointer, THREAD_ONE_STACK_SIZE,
THREAD_ONE_PRIORITY, THREAD_ONE_PREEMPTION_THRESHOLD,
TX_NO_TIME_SLICE, TX_AUTO_START) != TX_SUCCESS)
{
status = TX_THREAD_ERROR;
}
- Mutex creation using ThreadX API :
/* Create the Mutex */
if (tx_mutex_create(&MutexOne, "Mutex One", TX_NO_INHERIT) != TX_SUCCESS)
{
ret = TX_MUTEX_ERROR;
}
5. Define the entry function for each created thread :
void ThreadOne_Entry(ULONG thread_input)
{
/* User can add their own implementation*/
}
5.2. Module mode[edit source]
5.2.1. Module manager[edit source]
- In order to initialize and configure Azure RTOS ThreadX kernel in module mode, the user must include the “txm_module.h” file.
- Call tx_kernel_enter function from the main.
/* Start the ThreadX kernel */
tx_kernel_enter();
- The user must also properly define the initial system resources in the tx_application_define function. Examples of system resources include threads, queues, memory pools, event flag groups, mutexes, timers and semaphores.
VOID tx_application_define(VOID *first_unused_memory)
{
VOID *memory_ptr = first_unused_memory;
/* USER CODE BEGIN tx_application_define */
/* User can add his own implementation to define the initial ThreadX system resources*/
/* USER CODE END tx_application_define */
}
The input parameter of tx_application_define is the first available RAM address to be used for the run-time memory allocation of thread stacks, queues and memory pools.
- The user must create a module manager thread to:
- Initialize the module manager.
status = txm_module_manager_initialize((VOID *) module_data_area, MODULE_DATA_SIZE);
- Create a pool for module objects
status = txm_module_manager_object_pool_create(object_memory, OBJECT_MEM_SIZE);
- Register the module manager memory fault notification
status = txm_module_manager_memory_fault_notify(module_fault_handler);
- Load the module from his specific address.
status = txm_module_manager_in_place_load(&ModuleOne, "Module One", (VOID *) MODULE_FLASH_ADDRESS);
- Configure the memory management (example: enable the shared memory for the module).
status = txm_module_manager_external_memory_enable(&ModuleOne, (void*)READONLY_REGION, SHARED_MEM_SIZE, TXM_MODULE_ATTRIBUTE_READ_ONLY);
- Start the module.
status = txm_module_manager_start(&ModuleOne);
- Stop the module.
status = txm_module_manager_stop(&ModuleOne);
- Unload the module.
status = txm_module_manager_unload(&ModuleOne);
- Initialize the module manager.
5.2.2. Module[edit source]
In order to initialize and configure the module, the user must:
- Define “TXM_MODULE” and include the “txm_module.h” file.
- Define the default module entry function “default_module_start”.
VOID default_module_start(ULONG id)
{
/* Users can add their own implementation to define the initial ThreadX module system resources*/
}
- Initialize system resource using ThreadX APIs:
- Allocate object from the created memory pool for module objects.
txm_module_object_allocate((void*)&MainThread, sizeof(TX_THREAD));
- Create system resource using ThreadX common API. Example:
/* Create ThreadOne. */
if (tx_thread_create(&ThreadOne, "Thread One", ThreadOne_Entry, 0,
pointer, THREAD_ONE_STACK_SIZE,
THREAD_ONE_PRIORITY, THREAD_ONE_PREEMPTION_THRESHOLD, TX_NO_TIME_SLICE, TX_AUTO_START) != TX_SUCCESS)
{
status = TX_THREAD_ERROR;
}
- Request access to the module manager object:
status = txm_module_object_pointer_get(TXM_QUEUE_OBJECT, "Resident Queue", (VOID **)&ResidentQueue);
6. Migration from FreeRTOS to ThreadX[edit source]
ThreadX supports the same standard groups of APIs as most RTOS's such as FreeRTOS. It is possible to use either the CMSIS-RTOS wrapping layer or the ThreadX FreeRTOS wrapping layer in order to migrate from an RTOS to ThreadX. The table below lists the API equivalence between FreeRTOS and ThreadX.
Feature | ThreadX | FreeRTOS | Example of ThreadX APIs | Example of FreeRTOS APIs |
---|---|---|---|---|
Thread management | Supported | Supported | tx_thread_create tx_thread_sleep tx_thread_suspend |
xTaskCreate vTaskDelay vTaskSuspend |
Message queue | Supported | Supported | tx_queue_create tx_queue_send tx_queue_receive |
xQueueCreate xQueueSend xQueueReceive |
Event flags | Supported | Supported | tx_event_flags_create tx_event_flags_get tx_event_flags_set |
xEventGroupCreate xEventGroupGetBits xEventGroupSetBits |
Mutex | Supported | Supported | tx_mutex_create tx_mutex_put, tx_mutex_get |
xSemaphoreCreateMutex |
Semaphore | Supported | Supported | tx_semaphore_create tx_semaphore_put tx_semaphore_get |
xSemaphoreCreateCounting xSemaphoreGive xSemaphoreTake |
Software Timer | Supported | Supported | tx_timer_create tx_timer_delete |
xTimerCreate xTimerDelete |
Memory Mangement | Advanced (using Byte Pools and Block Pools) |
Simple | ||
Low Power | Supported | Supported | ||
TrustZone | Supported | Supported | ||
BasePri | Supported | Supported | ||
MPU | In Module Mode |
Managed in FreeRTOS Kernel |
7. Applications[edit source]
STM32Cube firmware provides a set of functional applications covering the main features of Azure RTOS ThreadX. The ThreadX applications for STM32MP13xx MPUs are listed below.
ThreadX application | Overview |
---|---|
Tx_Thread_Creation | This application provides an example of Azure RTOS ThreadX stack usage. It shows how to develop an application using the ThreadX thread management APIs. It demonstrates how to create and destroy multiple threads using Azure RTOS ThreadX APIs. It also shows how to use a preemption threshold between threads, and change priorities on-fly.
For more information, refer to the application Projects/STM32MP135C-DK/Applications/ThreadX/Tx_Thread_Creation/README.md file. |
Tx_Thread_MsgQueue | This application provides an example of Azure RTOS ThreadX stack usage, and shows how to develop an application using the ThreadX message queue APIs. It also demonstrates how to send and receive messages between threads using ThreadX message queue APIs, and shows how to use the event chaining feature.
For further information, refer to the application Projects/STM32MP135C-DK/Applications/ThreadX/Tx_Thread_MsgQueue/README.md file. |
Tx_Thread_Sync | This application provides an example of Azure RTOS ThreadX stack usage. It shows how to develop an application using the ThreadX synchronization APIs.
For further information, refer to application Projects/STM32MP135C-DK/Applications/ThreadX/Tx_Thread_Sync/README.md file. |
Tx_MPU | This application provides an example of Azure RTOS ThreadX stack usage, and shows how to develop an application using the ThreadX Module feature. It also demonstrates how to load, start and unload modules, and shows how ThreadX memory protection on modules using the Memory Protection Unit (MPU). This application is only available for products having the MPU feature.
For further information,refer to the application Projects/STM32MP135C-DK/Applications/ThreadX/Tx_MPU /README.md file. |