The STM32MP135x-DK Discovery kit (STM32MP135F-DK
) constitutes a flexible and complete solution for evaluating the capabilities of the STM32MP135 line
microprocessor devices.
All useful information to start with the STM32MP135x-DK Discovery kit is accessible through the links provided below.
1. Supported software distribution[edit source]
Only one software distribution is supported with STM32MP135x-DK Discovery kit :
- The STM32MPU Embedded Software distribution[1].
Take also a look at the latest STM32 MPU ecosystem release note for complementary information.
For this distribution, three software Packages are delivered:
- the Starter Package
- the Developer Package
- the Distribution Package
Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.
The STM32MP135x-DK Discovery kit includes the software packages (image, source code) and the tools needed to get started.
![]() | ||
Starter Package | Developer Package | Distribution Package |
|
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE |
|
2. Hardware description[edit source]
A brief article (see link below) describes the board, and provides indications on how to:
- assemble the board
- configure the hardware switches
- connect the board to external material
It also contains a short introduction of the board hardware components and connectors.
Board description |
---|
![]() STM32MP135x-DK - hardware description |
3. References[edit source]