1. Purpose[edit source]
This article describes the configuration of the PWR wake-up pins.
The PWR Wake-up pins are used to wake-up from Standby from an external device.
2. Overview[edit source]
- Button: one external device plugged to a wake-up pin. Could also be a PMIC.
- PWR: PWR internal peripheral
- OP-TEE PWR IRQ Driver: Driver in charge of PWR peripheral that provides access to the wake-up pin via an interrupts interface.
- OP-TEE PWR IRQ User driver: PWR IRQ consumer used to enable one wake-up pin and forward events as notifications to the non-secure world.
- OP-TEE notification: stack in charge of communication with the non secure world.
- Linux Linaro OP-TEE TZ: stack in charge of communication with secure world. Provides OP-TEE notifications as interrupts.
- GPIO keys: OP-TEE interrupts client.
3. OP-TEE Wake-up pin configuration[edit source]
Wake-up pins are configured in OP-TEE via device-tree. A pwr-irq-user can be instantiated to handle the desired wake-up pin and send a OPTEE notification to Linux in case of event.
fixme need yaml.
4. Linux Wake-up pin usage[edit source]
Linux does not handle wake-up pin, but it can handle an OP-TEE notification as an interrupt. This is configured via device-tree.
fixme need yaml.
5. Example with wake-up pin 2[edit source]
In the example below, the wake-up pin number 2 is configured by OP-TEE, forwarded as notification number 4 to Linux, and used by "gpio-keys" driver in Linux to generate a key-press.
OP-TEE device tree:
wakeup_button: wakeup-button { compatible = "st,stm32mp1,pwr-irq-user"; st,wakeup-pin-number = <2>; st,notif-it-id = <4>; status = "okay"; };
Linux device tree:
wake_up { compatible = "gpio-keys"; status = "okay"; button { label = "wake-up"; linux,code = <KEY_WAKEUP>; interrupts-extended = <&optee 4>; status = "okay"; }; };
6. References[edit source]