1. Purpose[edit source]
This article describes the configuration of the PWR wake-up pins.
The PWR Wake-up pins are used to wake-up from Standby from an external peripheral source.
2. Overview[edit source]
schema
- bloc1.
- bloc2.
- bloc3.
3. OP-TEE Wake-up pin configuration[edit source]
Wake-up pins are configured in OP-TEE via device-tree. A very small driver named pwr-irq-user can be instantiated to handle the desired wake-up pin and send a OPTEE notification to Linux in case of event.
fixme need yaml.
4. Linux Wake-up pin usage[edit source]
Linux does not handle wake-up pin, but it can receives OP-TEE notifications as any interrupt. This is configured via device-tree.
fixme need yaml.
5. Example with wake-up pin 2[edit source]
OP-TEE device tree:
wakeup_button: wakeup-button { compatible = "st,stm32mp1,pwr-irq-user"; st,wakeup-pin-number = <1>; st,notif-it-id = <2>; status = "okay"; };
Linux device tree:
wake_up { compatible = "gpio-keys"; status = "okay"; button { label = "wake-up"; linux,code = <KEY_WAKEUP>; interrupts-extended = <&optee 2>; status = "okay"; }; };
6. References[edit source]