Netdata

Revision as of 15:00, 4 April 2022 by Registered User (→‎Customized netdata web page)
Applicable for STM32MP13x lines, STM32MP15x lines

1. Article Purpose[edit source]

This article provides the basic information needed to start using the Linux® monitoring tool: netdata[1].

2. Introduction[edit source]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Warning white.png Warning
No Developer Package is presently delivered.
The tool (even if marked as present) has not been yet tested with the current release.
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
netdata Monitoring tools netdata[1] is a system for distributed real-time performance and health monitoring. It provides unparalleled insights, in real-time, of everything happening on the system it runs (including applications such as web and database servers), using modern interactive web dashboards. Yes Yes Yes No No No

3. Installing the trace and debug tool on your target board[edit source]

3.1. Using the STM32MPU Embedded Software distribution[edit source]

netdata is installed by default and ready to be used with all STM32MPU Embedded Software Packages.

 which netdata
/usr/sbin/netdata

It is integrated in weston image distribution through meta-st package: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb.

RDEPENDS_packagegroup-framework-tools-ui = "\
   ${@bb.utils.contains('DISTRO_FEATURES', 'x11', 'xvinfo', , d)}    \
   ${@bb.utils.contains('DISTRO_FEATURES', 'gplv3', 'glmark2', , d)} \
   ${@bb.utils.contains('DISTRO_FEATURES', 'gplv3', 'netdata', , d)} \
   ${@bb.utils.contains('DISTRO_FEATURES', 'gplv3', 'lmsensors-libsensors', , d)} \
   "

4. Getting started[edit source]

netdata provides all monitoring information on a web page accessible at the IP address of the board.

It proposes a default web page, on port 19999. It is also possible to create a custom page.

4.1. netdata service[edit source]

netdata is managed as a service. In OpenSTLinux distribution, it can be found under meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata/netdata.service.

The following command allows to verify if the service is active and running on the target board:

 systemctl | grep netdata
  netdata.service                           loaded active running  Netdata, Real-time performance monitoring

In case it is not running, the service can be started using the following command:

 systemctl start netdata

It is recommended to stop the service when it is not needed any longer:

  systemctl stop netdata

4.2. Generic netdata web page[edit source]

On host PC browser, the generic netdata web page is found at address:

http://<ip_of_board>:19999

Netdata screenshot main.png

4.3. Customized netdata web page[edit source]

Some customized web pages are proposed in OpenSTLinux environment to monitor some specific indicators: STM32MP1 Dashboard
The web page are proposed as example and could be adapted to the platform used.

  • Starter and Developer Packages
- directly accessible on the target under: /usr/share/netdata/web/stm32mp15.html
- directly accessible on the target under: /usr/share/netdata/web/stm32mp13.html
  • Distribution Package
- available under recipes-webadmin directory in file: meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata/stm32mp15.html
- available under recipes-webadmin directory in file: meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata/stm32mp13.html


On host PC browser, it is available at address:

http://<ip_of_board>:19999/stm32mp13.html

or

http://<ip_of_board>:19999/stm32mp15.html

File:Netdata screenshot stm32.png

5. References[edit source]


  • Useful external links
Document link Document Type Description
netdata source and documentation page Standard GitHub link reference