1. Article Purpose[edit source]
The purpose of this article is to explain how to integrate the NFC05A1 expansion board with STM32MP157C-DK2, Software will run on Linux on Cortex®-A7. NFC05A1 board is a NFC card reader expansion board based on ST25R3911B for STM32 and STM8 Nucleos.
2. Prerequisites[edit source]
- STM32MP157C-DK2 : Discovery kit for STM32MPU
- X-NUCLEO-NFC05A1: Nucleo extension board featuring NFC front end IC ST25R3911B
- Linux PC with Ubuntu installed will be required for development. Please refer to the page : [[1]]
- All the dependencies as per the LINK:Getting_started/STM32MP1_boards/STM32MP157C-DK2 should be installed
- SDK must be installed and also enabled. [[2]]
- Starter Package must be flashed onto SD-Card and board should boot up successfully.
3. Hardware setup - connections explained[edit source]
The X-NUCLEO-NFC005A1 is docked on to the Arduino connector present on the bottom side of the STM32MP157C-DK2 board as shown in below figure -
4. Software setup, build and run[edit source]
4.1. Booting STM32MP157C-DK2 with Starter Package[edit source]
Instructions for Booting the board using Starter Package are available for reference on wiki page: Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let's_start/Populate_the_target_and_boot_the_image
4.2. Software platform configuration for running the application[edit source]
Before running the application, platform configuration needs to be updated. User need to download Developer Package and update device tree for enabling the relevant peripheral configuration.
For quick evaluation of the software user can refer to section 4.2.1 and use the pre-built images and easily have the application running on discovery kit.
In case the user wants a full-fledged development environment, detailed description of how to modify the device tree and build updated kernel images is mentioned in section 4.2.2
Note: In this document, we will access the Discovery Kit from host PC via TCP/IP network (using ssh and scp commands). Another method to access the board could be through serial link (UART / USB) using tools such as ‘minicom’ (on Linux PC) or ‘Tera-term’ (on Windows PC). For more details, please refer to wiki page: How to get Terminal.
4.2.1. Steps for quick evaluation of software[edit source]
In order to speed-up the development process and quickly evaluate the software, please follow below mentioned steps–
- Please follow instructions in the link : STM32MP157C-DK2 Let's start. to flash the Starter Package on the SD Card.
- Boot the board with Starter Package.
- Enable internet connectivity on the board via Ethernet OR WiFi. Refer to wiki pages for help.
- Download pre-built images - Link for download :: TBD after release on www.st.com
- Use below commands to copy the device tree blob and update the new platform configuration –
PC $> cd RFAL_STMPU_release_v1.0/STM32MP157C-DK2_DeviceTree/Binaries PC $> scp stm32mp157c-dk2.dtb root@<ip address of board>:/boot/ PC $> ssh root@<ip address of board> Board $> /sbin/depmod –a Board $> sync Board $> reboot
Note: In case network connectivity is not available, please refer to section: 'How to transfer files using ‘Tera Term’: Windows PC to Discovery Kit' for doing file transfer locally.
- After the board boots up, copy the application binary and the shared lib to discovery board –
PC $> cd RFAL_STMPU_release_v1.0/NFCPollerApplication/Binaries PC $> scp ./* root@<ip address of board>:/usr/local PC $> ssh root@<ip address of board> Board $> cd /usr/local Board $> export LD_LIBRARY_PATH=/usr/local/:$LD_LIBRARY_PATH Board $> chmod +x nfc_poller_st25r3911 Board $> ./nfc_poller_st25r3911
The application will start running once the above mentioned commands are executed.
4.2.2. Updating platform configuration in developer package[edit source]
In order to set up the development platform, please follow below mentioned steps –
- Download Developer Package and install the SDK in the default folder structure on your Ubuntu machine. Plese follow : Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm®_Cortex®-A7/Install_the_SDK
- Update the device tree as mentioned below to enable and configure the SPI4 driver interface. Open the device tree file ‘stm32mp157c-dk2.dts’ in the Developer Package source code and add below code snippet to the file-
&pinctrl{ spi4_pins_a: spi4-0 { pins1 { pinmux = <STM32_PINMUX('E', 12, AF5)>, /* SPI4_SCK */ <STM32_PINMUX('E', 14, AF5)>; /* SPI4_MOSI */ bias-disable; drive-push-pull; slew-rate = <1>; }; pins2 { pinmux = <STM32_PINMUX('E', 13, AF5)>; /* SPI4_MISO */ bias-disable; }; }; spi4_sleep_pins_a: spi4-sleep-0 { pins { pinmux = <STM32_PINMUX('E', 12, ANALOG)>, /* SPI4_SCK */ <STM32_PINMUX('E', 13, ANALOG)>, /* SPI4_MISO */ <STM32_PINMUX('E', 14, ANALOG)>; /* SPI4_MOSI */ }; }; }; &spi4 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&spi4_pins_a>; pinctrl-1 = <&spi4_sleep_pins_a>; /*status = "disabled";*/ cs-gpios = <&gpioe 11 0>; status = "okay"; spidev@0x00 { compatible = "semtech,sx1301"; spi-max-frequency = <5000000>; reg = <0>; }; };
- Compile the Developer package to get the stm32mp157c-dk2.dtb file. Please refer to following link for help. Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm®_Cortex®-A7/Modify,_rebuild_and_reload_the_Linux®_kernel
- Please refer to section x.x of this article for pushing the compiled device tree blob onto the discovery kit.
4.2.3. Build the RFAL Linux application code[edit source]
- SDK must be downloaded, installed and enabled. This should already be in place if you executed step #1 of section 4.2.2
- Download the application from the link: Link for download :: TBD after release on www.st.com
- Follow below commands to cross-compile the code -
sudo apt-get install cmake
cd RFAL_STMPU_release_v1.0/NFCPollerApplication/Source/Linux_RFAL_st25r3911_v2.1.0/linux_demo/build
cmake ..
make
- The above-mentioned commands would build following files –
The example application: "RFAL_STMPU_release_v1.0/NFCPollerApplication/Source/Linux_RFAL_st25r3911_v2.1.0/linux_demo/build/nfc_poller/nfc_poller_st25r3911"
The shared library : "RFAL_STMPU_release_v1.0/NFCPollerApplication/Source/Linux_RFAL_st25r3911_v2.1.0/linux_demo/build/rfal/st25r3911/librfal_st25r3911.so"
4.2.4. RUN the RFAL Linux application on STM32MP157C-DK2[edit source]
Copy generated binaries onto the Discovery Kit using below commands
scp RFAL_STMPU_release_v1.0/NFCPollerApplication/Source/Linux_RFAL_st25r3911_v2.1.0/linux_demo/build/nfc_poller/nfc_poller_st25r3911 root@<board ip address>:/usr/local scp RFAL_STMPU_release_v1.0/NFCPollerApplication/Source/Linux_RFAL_st25r3911_v2.1.0/linux_demo/build/rfal/st25r3911/librfal_st25r3911.so root@<board ip address>:/usr/local
Open terminal on the Discovery Kit board or use ssh login and run the application using below commands.
ssh root@<board ip address>
Export the shared lib to the environment
export LD_LIBRARY_PATH=/usr/local:$LD_LIBRARY_PATH
Enter the directory where binaries were copied
cd /usr/local
RUN the application
./nfc_poller_st25r3911
The user will see the below message on the screen:
“Welcome to the ST25R3911B NFC Poller Demo on Linux. Scanning for NFC Technologies ...........”
When a NFC tag is brought near the reader antenna, the communication takes place between the tag and reader and the UID is displayed on the screen. Snapshot below [ upload snapshot pic]