Template:ArticleMainWriter Template:ArticleApprovedVersion
1. Purpose[edit source]
This article describes how to perform remote connection using the ssh[1] tool.
1.1. Perform ssh connection[edit source]
- On host PC, one can type:
If it is a first connection:
ssh root@10.48.1.172 The authenticity of host '10.48.1.172 (10.48.1.172)' can't be established. ECDSA key fingerprint is a0:a2:a3:09:b4:99:b3:90:6a:d0:35:05:6e:37:d0:6e. Are you sure you want to continue connecting (yes/no)? yes Warning: Permanently added '10.48.1.172' (ECDSA) to the list of known hosts. root@(none):~#
Otherwise:
ssh root@10.48.1.172 root@(none):~#
If the below error message is showing, it means that sshd is not running on the target:
ssh root@10.48.1.172 ssh: connect to host 10.48.1.172 port 22: Connection refused
- On stm32mp1, one can type:
mkdir /var/run/sshd /etc/init.d/sshd restart
- In the console, the following log should appear:
mkdir /var/run/sshd
/etc/init.d/sshd restart
generating ssh RSA key...
generating ssh ECDSA key...
generating ssh DSA key...
generating ssh ED25519 key...
Restarting OpenBSD Secure Shell server: sshdno /usr/sbin/sshd found; none killed