MDMA internal peripheral

Revision as of 12:45, 1 February 2019 by imported>Frq07269 (→‎Overview)


Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Article purpose[edit source]

The purpose of this article is to:

  • briefly introduce the MDMA peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the MDMA peripheral.


2. Peripheral overview[edit source]

The MDMA is used to perform high-speed data transfers between memory and memory or between peripherals and memory. The MDMA controller features 32 channels, dedicated to DMA transfers. The selection of the device connected to each channel and controlling DMA transfers is directly done by the MDMA.


Among all the requestor lines described in the STM32MP15 reference manuals, DMA channels are the only lines that allow to perform transfers with chained DMA and MDMA (refer to DMA internal peripheral article). As a result, when a device is not connected to the MDMA, it is anyway possible to operate in DMA mode via the DMA controller and chain DMA and MDMA.

2.1. Features[edit source]

Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2. Security support[edit source]

The MDMA is a secure peripheral. This means that it performs each transfer in the context of the master that requested it:

  • a transfer requested by the Arm® Cortex®-A7 non-secure core propagates non-secure accesses to the targeted device and/or memory.
  • a transfer requested by Arm Cortex-A7 secure core propagates secure accesses to the targeted device and/or memory.

3. Peripheral usage and associated software[edit source]

3.1. Boot time[edit source]

The MDMA is used at boot time by the FMC.

3.2. Runtime[edit source]

3.2.1. Overview[edit source]

The MDMA is visible from the Arm Cortex-M4 core. However, it is not supported in this context by STMicroelectronics distribution.


As stated in the 'Security support' chapter above, the MDMA is a secure peripheral. This means that its channels have to be allocated to:

  • the Arm Cortex-A7 non-secure core to be controlled in Linux® by the dmaengine framework

and

  • the Arm Cortex-A7 secure core to be controlled by the MDMA OP-TEE driver

STM32CubeMX allows to distinguish between non-secure and secure channels, among all the available channels.

3.2.2. Software frameworks[edit source]

Internal peripherals software table template

| Core/DMA
| MDMA
| OP-TEE MDMA driver
| Linux dmaengine framework
| 
|
|-
|}

3.2.3. Peripheral configuration[edit source]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4. Peripheral assignment[edit source]

Internal peripherals assignment table template

| rowspan="1" | Core/DMA
| rowspan="1" | MDMA
| MDMA
| 
| 
|
| Shareable (multiple choices supported)
|-
|}

4. How to go further[edit source]

Not applicable

5. References[edit source]