Power overview

Revision as of 15:55, 31 May 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

1. Framework purpose[edit source]

The purpose of this article is to explain how to handle the STM32 Arm® Cortex® MPUs More info.png low-power modes:

  • Low-power modes available on the device
  • Linux software overview for Power Management (on/off support, Suspend / Resume, Idle behavior, policy and control)
  • How to enter and exit a platform low-power mode

2. Software overview[edit source]

The Linux® Power Management (PM) is spitted in:

  • Static PM or System-Wide Power Management
    • power off
    • the suspend framework is used to trigger a low-power mode entry/exit sequence.
  • Dynamic PM or Working-State Power Management or Active Power Management based on other frameworks:

Refer to power and in admin-guide/pm for more details.

The OpenSTLinux power management support is based on Arm® interface standards:

  • Power state coordination interface (PSCI) [1]
  • System Control and Management Interface (SCMI)[2]

On STM32MP1 series, the "System-Wide Power Management" is supported:

Power mgt.png

The user application issues a suspend request to the kernel. This request is handled by the suspend Framework, which notifies all the device drivers to prepare for low-power entry. It then calls the PSCI service.

On STM32MP2 series:

STM32MP2 Power mgt.png

The suspend framework use the PSCI suspend support and the associated generic power domains (GenPD) and PSCI CPUIdle for OS initiated low power more with S2IDLE and CPUIdle.

2.1. Component description[edit source]

Kernel components for low power:

  • Dynamic PM: CPU Idle and device Idle with Runtime PM
  • CPUFreq: DVFS for CPU (see the page How to change the CPU frequency for details)
  • Suspend framework: this framework schedules the overall sequence by stopping all the ongoing tasks
  • GenPD: domain framework, based on runtime PM
    • GenPD driver: this driver is used for low-power mode selection according to the activated wakeup sources.
  • PSCI library: this is a set of standardized functions to request a low-power service to the secure monitor
  • Clock framework
    • RCC driver: this driver handles the circuit non-secure clocks
  • Regulator framework
  • SCMI framework: including SCMI drivers for secure resource as clock, regulators, reset, performance domain

Secure monitor components (TF-A BL31 on AArch64 platforms, OP-TEE on AArch32 platforms) :

  • PSCI library: this is a set of standardized functions handling the low-power services
  • Low power driver: the role of this driver is to choose the low-power mode according to the programmed wakeup source(s)
  • PWR driver: this driver is responsible for configuring the low-power mode
  • RCC driver: this driver handles the circuit secure clocks

Secure world components (OP-TEE):

  • SCMI stack: SCMI stack with access to secure resources, clock with RCC driver, regu with PWR driver and STPMIC driver

2.2. API description[edit source]

The suspend process is triggered from the user space through standard commands.

The system sleep control file is the state file, located under: /sys/power/

Further details can be found in admin-guide/pm/sleep-states.html and in power/interface.html.

The sysfs ABI are described in ABI/testing/sysfs-power and ABI/testing/sysfs-devices-power.

The device power API are described in driver-api/pm/index.html, in particular in driver-api/pm/devices.html.

For Weston OpenSTLinux distribution, the direct access to sysfs must be avoided and must be replaced by systemctl command.

2.2.1. Modes for STM32MP1 series[edit source]

Only the 'mem' command is supported for STM32MP1 series: the whole system activity is stopped and a low-power mode is entered. The software selects the deepest mode according to the activated wakeup source(s).

Example:

  echo mem > /sys/power/state

or

  systemctl suspend

STM32MP1 series STMicroelectronics deliveries propose a default mapping of the low-power modes for each type of board, this default mapping can be changed thanks to the device tree as explain in the next paragraph.

2.2.2. Modes for STM32MP2 series[edit source]

For each mode the PSCI stack in TF-A BL31 selects the deepest mode according to the activated wake-up source(s).

  • Suspend-to-RAM (S2RAM)¶
  echo mem > /sys/power/state

The mode 'deep' for S2RAM is default at boot, you can force it with:

  echo deep > /sys/power/mem_sleep
  echo mem > /sys/power/state

or

  systemctl suspend

with 'SuspendState=mem' in /etc/systemd/sleep.conf

  • Suspend-to-Idle (S2Idle)
  echo freeze > /sys/power/state

or

  echo s2idle > /sys/power/mem_sleep
  echo mem > /sys/power/state

or

  systemctl suspend

with 'SuspendState=freeze' in /etc/systemd/sleep.conf

  • Power-Off
  shutdown -P now
  systemctl poweroff

3. Configuration[edit source]

The objective of this chapter is to explain how to configure the Linux kernel and device tree to have the Power Management (PM) framework activated.

3.1. Kernel configuration[edit source]

The Power Management framework is activated by default in ST deliveries.

It can be deactivated through the kernel menuconfig using Power management options/Suspend to RAM and standby: Menuconfig or how to configure kernel .

3.2. Device tree configuration[edit source]

3.2.1. STM32MP1 series[edit source]

The default system low-power mode mapping can be modified through the secure monitor device tree, as described OP-TEE page.

Below an example in OP-TEE core/arch/arm/dts/stm32mp135f-dk.dts

 &pwr_regulators {
 	system_suspend_supported_soc_modes = <
 		STM32_PM_CSLEEP_RUN
 		STM32_PM_CSTOP_ALLOW_LP_STOP
 		STM32_PM_CSTOP_ALLOW_LPLV_STOP
 		STM32_PM_CSTOP_ALLOW_LPLV_STOP2
 		STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR
 	>;
 
 	system_off_soc_mode = <STM32_PM_SHUTDOWN>;
 };

3.2.2. STM32MP2 series[edit source]

The Soc device tree describes the PSCI topology in sub-nodes of cpus/domain-idle-states:

The select PSCI power level is indicated to OP-TEE with Secure-EL1 Payload Dispatcher (SPD) PSCI hooks. The STPMIC25 driver in OP-TEE configures the regulators for the expected low power mode as describes in device tree with regulator-state-XXX subnodes, see PMIC page for details and OP-TEE device tree example in core/arch/arm/dts/stm32mp257f-ev1.dts .

The unsupported low power modes must be deleted in your board device-tree for TF-A BL31 and for Linux, and also its references in power domaine nodes with domain-idle-states.

For example on board without PMIC, if the used regulator controlled by PWR_LP pins force the reduced voltage on VDDCORE and VDDCPU, the LP-Stop1 and LP-Stop2 modes are not supported.

  • in TF-A device tree
/ {
	cpus {
		domain-idle-states {
			/delete-node/ lp-stop1;
			/delete-node/ lp-stop2;
		};
	};
};
/ {
	cpus {
		domain-idle-states {
			/delete-node/ domain-lp-stop1;
		};
	};
};

&CLUSTER_PD {
	domain-idle-states = <&STOP1>;
};

4. How to use the framework[edit source]

4.1. Low-power modes available on the device[edit source]

Refer to STM32MP13 reference manuals, STM32MP15 reference manuals or STM32MP25 reference manuals for the full description of low-power modes.
The modes are handled by the RCC and the PWR peripherals.

4.1.1. On STM32MP13x lines More info.png[edit source]

The table below summarizes the device hardware states corresponding to each low-power mode.

MPU mode Platform mode VDDCORE state VDDCPU state Clocks state
CRun Run On On On
CStop Stop/LPLV-Stop On/Retention On/Retention Off/Off
CStandby Stop/LPLV-Stop/LPLVL-STOP2/Standby On/Retention/Retention/Off On/Retention/Off/Off Off/Off/Off/Off

The following tables give the list of wake-up sources available in each mode.

Platform mode Available wake-up sources
Stop BOR, PVD, AVD, Vbat mon, Temp mon, HSE CSS, LSE CSS, RTC, TAMP, USBH, OTG, ETH, USART, I2C, SPI, DTS, LPTIM, IWDG, GPIO, Wakeup pins (from PWR)
LPLV-Stop
LPLV-Stop2
BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, USART, I2C, SPI, DTS, LPTIM, IWDG, GPIO, Wakeup pins (from PWR)
Standby BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, Wakeup pins (from PWR)

4.1.2. On STM32MP15x lines More info.png[edit source]

The AN5109 low-power application note also gives much more information on these modes, including:

  • the detailed description of the operating modes,
  • the low-power mode entry and exit sequences,
  • the low-power mode control registers.
  • the wake-up sources and the software mechanism that ensures the consistency between the low-power mode and the activated wake-up source,

The table below summarizes the device hardware states corresponding to each low-power mode.

The term "subsystem" either refers to Arm® Cortex®-A7 (also called MPU) or to Arm® Cortex®-M4 (also called MCU). A mode prefixed by 'C' corresponds to a subsystem mode.

Level Mode VDDCORE state Subsystem Clocks state
MPU Subsystem MPU CRun on on
MPU CStop on off
MPU CStandby on off
MCU Subsystem MCU CRun on on
MCU CStop on off

A platform mode is the combination of MPU and MCU modes.

MPU mode MCU mode Platform mode VDDCORE state Clocks state
CRun/CStop/CStandby CRun Run On On
CStop/CStandby CStop Stop (LPDS = 0) On Off
CStop/CStandby CStop LP-Stop or LPLV-Stop (LPDS = 1) Retention Off
CStandby CStop
MCU PDDS = 1
Standby Off Off

The following tables give the list of wake-up sources available in each mode.

Plaform mode Available wake-up sources
Stop BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, USB, CEC, ETH, USART, I²C, SPI, LPTIM, IWDG, GPIO, Wakeup pins (from PWR)
LPLV-Stop BOR, PVD, AVD, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, GPIO, Wakeup pins (from PWR)
Standby BOR, Vbat mon, Temp mon, LSE CSS, RTC, TAMP, IWDG, Wakeup pins (from PWR)

This list of Wake-up capability peripheral for each mode is defined in the Table 35. Functionalities depending on system operating mode of the STM32MP15 reference manuals.

4.1.3. On STM32MP25x lines More info.png[edit source]

The AN5726 Guidelines for using low-power modes on STM32MP2 MPU also gives much more information on these modes and on associated the wake-up sources.

System mode Linux Command Power consumption Wake-up time VDDCPU VDDCORE DDR state
Stop1 freeze
(s2idle)
Medium Medium ON ON SR, VTT on
LP-Stop1 Medium Medium SR, VTT off
LPLV-Stop1 Low Medium ON (reduced) ON (reduced)
Stop2 mem
(deep)
Low Medium OFF ON SR, VTT off
LP-Stop2 Low Medium
LPLV-Stop2 Low Medium ON (reduced)
Standby1 Low Medium OFF
Standby2 shutdown Low Low Off
VBAT Low Low

OpenSTLinux set the DDR in Self Refresh mode (SR) in all the low-power mode except power off and for LP-Stop1 and LP-Stop2 modes, the DDR VTT supply is switched off on STMicroelectronics reference design thought the PWR_LP signal connected to PWRCTRL1 pin of STPMIC25.

This list of Wake-up capability peripheral for each mode is defined in the Table 94. Functionalities depending on system operating mode of the STM32MP25 reference manuals.

The following tables give the list of wake-up sources available in each mode.

Plaform mode Available wake-up sources
Stop1/2 and
LP-Stop1/2
Group1 : Group2 + HPDMAx (x = 1, 2, 3), HSI frequency monitoring, USB, UCPD1, ETHx (x = 1,2), USARTx (x = 1 to 9), I2Cx (x = 1 to 7), I3Cx (x = 1 to 3), SPIx (x = 1 to 7), DTS, LPTIMx (x = 1, 2)
LPLV-Stop1/2 Group2 : Group3 + PVD, PVM, GPIOs
Standby1 Group3 : Group4 + CPU3, DBG, LPDMA, LPUART1[note 1], I2C8[note 1], I3C4[note 1], SPI8[note 1], ADF1[note 1], LPTIMy (y = 3, 4, 5), WWDG2, MBOX2, HSEM, GPIOZ
Standby2 Group4 : Group5 + 6 x WKUP pins
VBAT Group5 : BOR, VBATH/VBATL, TEMPH/TEMPL, LSE CSS, RTC/auto wake-up, tamper pins, IWDGx
  1. 1.0 1.1 1.2 1.3 1.4 The wake-up associated to autonomous mode is not managed in OpenSTLinux.
4.1.3.1. PSCI topology[edit source]

The low power modes for STM32MP2 use the PSCI stack in TF-A BL31, including the PSCI OSI mode.

The PSCI topology is defined in TF-A PM driver: plat/st/stm32mp2/stm32mp2_pm.c .

Each low power more is associated to a PSCI State-id, which use the ARM Recommended StateID Encoding with OS initiated support, based on the PSCI state system topology defined in plat/st/stm32mp2/include/platform_def.h with:

  • PLAT_MAX_PWR_LVL = 4, for Core(0), D1(1), D1LPLV(2), D2(3), D2_LPLV(3)
  • PLAT_MIN_SUSPEND_PWR_LVL =2, limit level for PSCI_CPU_SUSPEND support
  • PLAT_NUM_PWR_DOMAINS = 6 (2 cores and 4 power level)

and with the power domaine states:

  • STM32MP_LOCAL_STATE_RUN(0)
  • STM32MP_LOCAL_STATE_RET(1)
  • STM32MP_LOCAL_STATE_LP(2)
  • STM32MP_LOCAL_STATE_OFF(3)

For PSCI suspend requests, STM32MP25 supports 5 power levels in the PSCI topology to handle the regulators configuration done in OP-TEE for STPMIC2, in particular to differentiate the tension for LP and the LPLV modes.

The composite PSCI State-id are used in PSCI_CPU_SUSPEND requests and in device tree (for S2Idle and for OS initiated support) and for used internal in TF-A BL31 for PSCI_CPU_SUSPEND request (Deep).

PSCI request Name State-id PState D2_LPLV D2 D1_LPLV D1 Core
PSCI_CPU_SUSPEND Sleep (WFI) 0x00000001 STANDBY RUN RUN RUN RUN RET
Stop1 0x00000011 STANDBY RUN RUN RUN RET RET
LP-Stop1 0x00000021 STANDBY RUN RUN RUN LP RET
LPLV-Stop1 0x00000211 STANDBY RUN RUN LP RET RET
PSCI_SYSTEM_SUSPEND Stop2 0x40001333 POWERDOWN RUN RET OFF OFF OFF
LP-Stop2 0x40002333 POWERDOWN RUN LP OFF OFF OFF
LPLV-Stop2 0x40023333 POWERDOWN LP OFF OFF OFF OFF
Standby 0x40002333 POWERDOWN OFF OFF OFF OFF OFF
4.1.3.2. PSCI in Linux (PSCI_CPU_SUSPEND)[edit source]

In Linux the power domain and associated low power modes for OS initiated mode are described in SoC device tree (in arch/arm64/boot/dts/st/stm32mp251.dtsi and in arch/arm64/boot/dts/st/stm32mp253.dtsi ) using the hierarchical model as described in Documentation/devicetree/bindings/arm/psci.yaml .

/ {
	cpus {PM runtime: Lin
		idle-states {
			entry-method = "psci";

			CPU_PWRDN: cpu-power-down {
				compatible = "arm,idle-state";
				arm,psci-suspend-param = <0x00000001>;
			};
		};

		domain-idle-states {
			STOP1: domain-stop1 {
				compatible = "domain-idle-state";
				arm,psci-suspend-param = <0x00000011>;
			};

			LP_STOP1: domain-lp-stop1 {
				compatible = "domain-idle-state";
				arm,psci-suspend-param = <0x0000021>;
			};

			LPLV_STOP1: domain-lplv-stop1 {
				compatible = "domain-idle-state";
				arm,psci-suspend-param = <0x00000211>;
			};
		};
	};

	psci {
		compatible = "arm,psci-1.0";
		method = "smc";
		CPU_PD0: power-domain-cpu0 {
			#power-domain-cells = <0>;
			domain-idle-states = <&CPU_PWRDN>;
			power-domains = <&CLUSTER_PD>;
		};
		CPU_PD1: power-domain-cpu1 {
			#power-domain-cells = <0>;
			domain-idle-states =  <&CPU_PWRDN>;
			power-domains = <&CLUSTER_PD>;
		};
		CLUSTER_PD: power-domain-cluster {
			#power-domain-cells = <0>;
			domain-idle-states = <&STOP1>, <&LP_STOP1>;
			power-domains = <&RET_PD>;
		};
		RET_PD: power-domain-retention {
			#power-domain-cells = <0>;
			domain-idle-states = <&LPLV_STOP1>;
		};
	};

This power domain hierarchy is used in generic power domain (GenPD) for S2IDLE request and for dynamic power management, based PSCI OS initiated mode PM runtime: Linux kernel selects the lowest possible low power mode with the associated PSCI State Id, according the state of each power domain (device in the power domain is running, wake-up source is activated) and which respects the OS constraint (wake-up latency in OS initiated mode for example).

STM32MP2 power domain.png

The devices are assigned to a domain in Soc device tree according the Table 94. Functionalities depending on system operating mode of the reference manuals (autonomous mode is not managed in OpenSTLinux).

  • CLUSTER_PD for peripherals not functional in "Stop1/2 and LP-Stop1/2"
  • RET_PD for peripherals not functional in "LPLV-Stop1/2"

The EXTI1 driver manage the activated wake up source which not functional in LPLV-Stop1 mode (see Wake-up capability column in the same Table 94. of reference manual).

4.1.3.3. PSCI in TF-A (PSCI_SYSTEM_SUSPEND)[edit source]

For deep request the PSCI_SYSTEM_SUSPEND is sent to T-FA when the secondary core is stopped and all the process are frozen. The activated wake-up are consolidated in TF-A BL31 to select the lowest POWERDOWN supported mode in stm32_get_sys_suspend_power_state() .

If a low power mode is not supported by a board design, it must be removed in TF-A BL31 device tree.

You can limit the maximum supported mode with wake-up sources, but you can't force Stop2 mode by Linux command if LP-Stop2 is supported (same functionalities, same supported wake-up sources).

To debug purpose, you can force the selected mode in stm32_get_sys_suspend_power_state(), for example:

/* Search the max supported POWERDOWN modes  <= max_pwr_state */
for (i = ARRAY_SIZE(stm32mp_supported_pwr_states) - 1U; i > 0U; i--) {
	pwr_state = stm32mp_supported_pwr_states[i];
	if ((pwr_state != 0U) && (pwr_state <= max_pwr_state) &&
		(psci_get_pstate_type(pwr_state) == PSTATE_TYPE_POWERDOWN)) {
	break;
	}
}

{{{1}}}

state_id = psci_get_pstate_id(pwr_state);

4.2. How to enter and exit low-power modes[edit source]

4.2.1. System-Wide Power Management[edit source]

The platform selects the allowed modes depending on the required wakeup source and the coprocessor state.

So you need:

  1. Activate the MCU needed wakeup source(s) and call the expected low-power mode for MCU side
    or stop the MCU firmware
  2. Activate the MPU needed wakeup source(s) and call the expected low-power mode for MPU side
Info white.png Information
You must be sure your wakeup device is able to provide the wake up signal during low-power mode.

E.g. supply, clock, reset, etc... must be present, if any

4.2.1.1. MCU side[edit source]

Please refer to Coprocessor power management for Arm® Cortex®-M commands or the MCU firmware can also be stopped before entering in low power (it is mandatory if this firmware is running in DDR).

4.2.1.2. MPU side[edit source]

The wakeup source(s) activation (device dependent) is done in the corresponding Linux driver (see the 'wakeup' attribute in sysfs) and it is possible to check the state of each wakeup source by displaying this attribute.

Then the low-power mode request is done by issuing the following command:

  echo mem > /sys/power/state

When systemd[3] is used, for example on the Weston OpenSTLinux configuration, the low-power mode is safely entered with the systemctlcommand:

  systemctl suspend

In this case, the configuration file /etc/systemd/sleep.conf [4] map the Weston power state to the kernel power state (in /sys/power/state). The OpenSTlinux configuration is:

[Sleep]
SuspendMode=
HibernateMode=
HybridSleepMode=
SuspendState=mem
HibernateState=mem
HybridSleepState=mem

To exploit the “freeze” mode:

[Sleep]
SuspendState=freeze
4.2.1.3. Example[edit source]
entering/exiting MPU CStop mode

Enable at least one wakeup source from table 2.1 in CStop category, for example USART4 on STM32MP15:

 echo enabled > /sys/devices/platform/soc/40010000.serial/tty/ttySTM0/power/wakeup
 echo enabled > /sys/devices/platform/soc/40010000.serial/power/wakeup

Call the low-power entry:

 echo mem > /sys/power/state

or systemd function:

  systemctl suspend

The MPU is now in CStop mode, and can be woken up by sending a character to the console.

5. Source code location[edit source]

6. How to trace and debug[edit source]

The suspend/resume process execution is logged in the MPU console. It gives useful information on the platform state (sleeping or active).

 root@stm32mp1:~# echo mem > /sys/power/state
 [ 1072.267571] PM: suspend entry (deep)
 [ 1072.269687] PM: Syncing filesystems ... done.
 [ 1072.279114] Freezing user space processes ... (elapsed 0.008 seconds) done.
 [ 1072.292835] OOM killer disabled.
 [ 1072.296046] Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
 [ 1072.303431] Suspending console(s) (use no_console_suspend to debug)
 [ 1072.332520] dwc2 49000000.usb-otg: suspending usb gadget configfs-gadget
 [ 1072.332537] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0
 [ 1072.332546] dwc2 49000000.usb-otg: dwc2_hsotg_ep_disable: called for ep0
 [ 1072.468536] Disabling non-boot CPUs ...
 [ 1072.507876] CPU1 killed.
 [ 1072.509635] Enabling non-boot CPUs ...
 [ 1072.510508] CPU1 is up
 [ 1072.527553] dwmac4: Master AXI performs any burst length
 [ 1072.527583] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
 [ 1072.527621] stm32-dwmac 5800a000.ethernet eth0: ERROR failed to create debugfs directory
 [ 1072.527631] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: failed debugFS registration
 [ 1072.588234] dwc2 49000000.usb-otg: resuming usb gadget configfs-gadget
 [ 1072.738469] OOM killer enabled.
 [ 1072.741575] Restarting tasks ... done.
 [ 1072.752596] PM: suspend exit

Get more debug information from the console with the following commands:

 echo N > /sys/module/printk/parameters/console_suspend 
 echo "func pm_dev_dbg +p" > /sys/kernel/debug/dynamic_debug/control

It is also possible to monitor the hardware signals related to the system low-power modes thanks to the HDP internal peripheral.
Please refer to HDP Linux driver for its configuration.

7. To go further[edit source]

Refer to reference manual for a detailed description of low-power modes and peripheral wakeup sources:

The next application notes gives additional information on the hardware settings used for low-power management:

8. References[edit source]

  1. Arm Power State Coordination Interface (PSCI):
    https://developer.arm.com/documentation/den0022
  2. Arm System Control and Management Interface Platform Design Document (SCMI) specification:
    https://developer.arm.com/documentation/den0056
  3. systemd: https://systemd.io/
  4. https://manpages.debian.org/jessie/systemd/systemd-sleep.conf.5.en.html