1. Purpose[edit source]
In this article, the stm32key
U-Boot command is used to illustrate and experiment the steps to provision the keys in the correct OTP needed to activate secure boot features: authentication and encryption.
It also allows setting the device directly to the CLOSED state.
1.1. Prerequisite[edit source]
All the required keys must be generated to provision the OTP.
The OTP write support must be activated in OP-TEE STM32MP BSEC PTA with CFG_STM32_BSEC_WRITE and the OTPs for these keys must be accessible by non-secure world, see st,non-secure-otp-provisioning in BSEC device configuration of OP-TEE.
In ecosystem release ≤ v4.1.0 , this configuration is activated only in OP-TEE debug release with:
CFG_STM32_BSEC_WRITE ?= $(CFG_TEE_CORE_DEBUG)
The command stm32key is not functional by default with the release version of OP-TEE.
2. stm32key command[edit source]
U-Boot in OpenSTLinux embeds a stm32key
command that can be called from U-Boot command-line interface to manage the keys in OTPs.
stm32key help stm32key - Manage key on STM32 Usage: stm32key list: list the supported key with description stm32key select [<key>]: Select the key identified by <key> or display the key used for read/fuse command stm32key read [<addr> | -a ]: Read the curent key at <addr> or current / all (-a) key in OTP stm32key fuse [-y] <addr>: Fuse the current key at addr in OTP stm32key close [-y]: Close the device, force use of PKH stored in OTP
The optional option -y
is used to skip the confirmation message.
The name of the used <key> is
stm32key list PKHTH: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) OTP24..31 EDMK: Encryption/Decryption Master Key" OTP92..95
stm32key list PKH: Hash of the ECC Public Key (ECDSA is the authentication algorithm) OTP24..31
- for STM32MP25x lines : OEM-KEY1 for authentication and EDMK1 for encryption of FSBL-A or FSBL-M. OEM-KEY2 is for the authentication and EDMK2 for the encryption of FSBL-M. FIP-EDMK for the encryption of the FIP.
STM32MP25x lines can use a dedicated set of keys for FSBL-M by fusing the bit 8 of OTP17. stm32key automatically fuse bit 8 of OTP 17 after having successfully programmed OEM-KEY2.
stm32key list OEM-KEY1: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) for FSBLA or M OTP144..151 OEM-KEY2: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) for FSBLM OTP152..159 FIP-EDMK: Encryption/Decryption Master Key for FIP OTP260..267 EDMK2: Encryption/Decryption Master Key for FSBLM OTP360..363 EDMK1: Encryption/Decryption Master Key for FSBLA or M OTP364..367
3. Authentication keys provisioning[edit source]
The key provisioning is the first step to enable the authentication: burn the keys in OTPs with the key hash output file from STM32 KeyGen.
3.1. Select keys[edit source]
Key is selected with the command stm32key select <key>
, with <key>=
stm32key select PKHTH PKHTH selected
stm32key select PKH PKH selected
stm32key select OEM-KEY1 OEM-KEY1 selected
3.2. Load keys file in DDR[edit source]
The keys hash file, output file from STM32 KeyGen, publicKeysHash.bin (for STM32MP15x lines ) or publicKeysHashHashes.bin (for STM32MP13x lines and STM32MP25x lines ), must be available in DDR before proceeding with the stm32key
command.
In the next chapters, this file is assumed to be loaded at ${loadaddr} = 0xc4000000 for STM32MP1 series and ${loadaddr} = 0x84000000 for STM32MP2 series.
For example the file can be loaded from a filesystem partition on a storage device by using the load
command (see documentation), if the file publicKeysHash.bin is in the bootfs (partition 7) on SD™ card (mmc0):
load mmc 0#bootfs ${loadaddr} publicKeysHash.bin
or
load mmc 0:7 0xc4000000 publicKeysHash.bin 32 bytes read in 50 ms (0 Bytes/s)
3.3. Verify keys file in DDR[edit source]
Once the publicKeysHash.bin (for STM32MP15x lines ) or publicKeysHashHashes.bin (for STM32MP13x lines ) file is loaded in DDR, you can verify the content of the file with the command:
stm32key read ${loadaddr}
Example for STM32MP13x lines with PKHTH
stm32key read ${loadaddr} Read PKHTH at 0xc4000000 PKHTH OTP 24: [c4000000] 27051956 PKHTH OTP 25: [c4000004] b56aef2d PKHTH OTP 26: [c4000008] 6215263c PKHTH OTP 27: [c400000c] 00000439 PKHTH OTP 28: [c4000010] 00000000 PKHTH OTP 29: [c4000014] 00000000 PKHTH OTP 30: [c4000018] 72429173 PKHTH OTP 31: [c400001c] 05020600
Example for STM32MP15x lines with PKH
stm32key read ${loadaddr} Read PKH at 0xc4000000 PKH OTP 24: [c4000000] 27051956 PKH OTP 25: [c4000004] b56aef2d PKH OTP 26: [c4000008] 6215263c PKH OTP 27: [c400000c] 00000439 PKH OTP 28: [c4000010] 00000000 PKH OTP 29: [c4000014] 00000000 PKH OTP 30: [c4000018] 72429173 PKH OTP 31: [c400001c] 05020600
Example for STM32MP25x lines with OEM-KEY1
stm32key read ${loadaddr} Read OEM-KEY1 at 0x84000000 OEM-KEY1 OTP 144: [84000000] 27051956 OEM-KEY1 OTP 145: [84000004] b56aef2d OEM-KEY1 OTP 146: [84000008] 6215263c OEM-KEY1 OTP 147: [8400000c] 00000439 OEM-KEY1 OTP 148: [84000010] 00000000 OEM-KEY1 OTP 149: [84000014] 00000000 OEM-KEY1 OTP 150: [84000018] 72429173 OEM-KEY1 OTP 151: [8400001c] 05020600
3.4. Key provisioning[edit source]
To write and lock the keys in OTP, you use the command:
stm32key fuse ${loadaddr}
3.5. Verify keys file in OTP[edit source]
After the previous command, the device contains the keys to authenticate images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with PKHTH
stm32key read PKHTH OTP 24: 27051956 lock : 50000000 PKHTH OTP 25: b56aef2d lock : 50000000 PKHTH OTP 26: 6215263c lock : 50000000 PKHTH OTP 27: 00000439 lock : 50000000 PKHTH OTP 28: 00000000 lock : 50000000 PKHTH OTP 29: 00000000 lock : 50000000 PKHTH OTP 30: 72429173 lock : 50000000 PKHTH OTP 31: 05020600 lock : 50000000
Result for STM32MP15x lines with PKH
stm32key read PKH OTP 24: 27051956 lock : 50000000 PKH OTP 25: b56aef2d lock : 50000000 PKH OTP 26: 6215263c lock : 50000000 PKH OTP 27: 00000439 lock : 50000000 PKH OTP 28: 00000000 lock : 50000000 PKH OTP 29: 00000000 lock : 50000000 PKH OTP 30: 72429173 lock : 50000000 PKH OTP 31: 05020600 lock : 50000000
Example for STM32MP25x lines with OEM-KEY1
stm32key read ${loadaddr} Read OEM-KEY1 at 0x84000000 OEM-KEY1 OTP 144: 27051956 lock : 50000000 OEM-KEY1 OTP 145: b56aef2d lock : 50000000 OEM-KEY1 OTP 146: 6215263c lock : 50000000 OEM-KEY1 OTP 147: 00000439 lock : 50000000 OEM-KEY1 OTP 148: 00000000 lock : 50000000 OEM-KEY1 OTP 149: 00000000 lock : 50000000 OEM-KEY1 OTP 150: 72429173 lock : 50000000 OEM-KEY1 OTP 151: 05020600 lock : 50000000
4. Encryption Decryption Master Key provisioning[edit source]
The EDMK key provisioning is the first step to enable the image decryption.
It is only available on STM32MP13x lines and STM32MP25x lines .
4.1. Select EDMK[edit source]
Key is selected with the command stm32key select <key>
, with <key>=
stm32key select EDMK EDMK selected
stm32key select EDMK1
EDMK1 selected
4.2. Load EDMK file in DDR[edit source]
The keys file must be available in DDR before proceeding the stm32key
command;
this file is loaded at ${loadaddr} = 0xc4000000 in the next examples.
The file edmk.bin can be loaded from a filesystem partition on a storage device by using the load
command (see documentation).
For example, the file edmk.bin is in the bootfs (partition 7) on SD™ card (mmc0):
load mmc 0#bootfs ${loadaddr} edmk.bin
4.3. Verify EDMK in DDR[edit source]
Then you can verify the content of keys files loaded in DDR with the command: stm32key read <addr>
Example for STM32MP13x lines with EDMK
stm32key read ${loadaddr} Read EDMK at 0xc4000000 EDMK OTP 92: [c4000000] 27051956 EDMK OTP 93: [c4000004] b56aef2d EDMK OTP 94: [c4000008] 6215263c EDMK OTP 95: [c400000c] 00000439
Example for STM32MP25x lines with EDMK
stm32key read ${loadaddr} Read EDMK at 0xc4000000 EDMK OTP 364: [84000000] 27051956 EDMK OTP 365: [84000004] b56aef2d EDMK OTP 366: [84000008] 6215263c EDMK OTP 367: [8400000c] 00000439
4.4. EDMK provisioning[edit source]
To write and lock the EDMK in OTP, you use the command with the same address:
stm32key fuse ${loadaddr}
4.5. Verify EDMK in OTP[edit source]
After the previous command, the device contains the keys to decrypt the images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with EDMK
stm32key read EDMK OTP 92: 00000000 lock : 50000000 EDMK OTP 93: 00000000 lock : 50000000 EDMK OTP 94: 00000000 lock : 50000000 EDMK OTP 95: 00000000 lock : 50000000
Result for STM32MP25x lines with EDMK
stm32key read EDMK OTP 364: 00000000 lock : 50000000 EDMK OTP 365: 00000000 lock : 50000000 EDMK OTP 366: 00000000 lock : 50000000 EDMK OTP 367: 00000000 lock : 50000000
5. Closing the device[edit source]
Once the authentication process is confirmed in ROM code and in TF-A, the device can be closed to ensure that only signed images can be used.
This operation is performed with the U-Boot command:
stm32key close