1. Purpose[edit source]
In this article, the stm32key
U-Boot command is used to illustrate and experiment the steps to provision the keys in the correct OTP needed to activate secure boot features: authentication and encryption.
It also allows setting the device directly to the CLOSED state.
1.1. Prerequisite[edit source]
All the required keys must be generated to provision the OTP.
The OTP write support must be activated in OP-TEE STM32MP BSEC PTA with CFG_STM32_BSEC_WRITE and the OTPs for these keys must be accessible by non-secure world, see st,non-secure-otp-provisioning in BSEC device configuration of OP-TEE.
In ecosystem release ≤ v4.1.0 , this configuration is activated only in OP-TEE debug release with:
CFG_STM32_BSEC_WRITE ?= $(CFG_TEE_CORE_DEBUG)
The command stm32key is not functional by default with the release version of OP-TEE.
2. stm32key command[edit source]
U-Boot in OpenSTLinux embeds a stm32key
command that can be called from U-Boot command-line interface to manage the keys in OTPs.
stm32key help stm32key - Manage key on STM32 Usage: stm32key list: list the supported key with description stm32key select [<key>]: Select the key identified by <key> or display the key used for read/fuse command stm32key read [<addr> | -a ]: Read the curent key at <addr> or current / all (-a) key in OTP stm32key fuse [-y] <addr>: Fuse the current key at addr in OTP stm32key close [-y]: Close the device, force use of PKH stored in OTP
The optional option -y
is used to skip the confirmation message.
The name of the used <key> is
stm32key list PKHTH: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) OTP24..31 EDMK: Encryption/Decryption Master Key" OTP92..95
stm32key list PKH: Hash of the ECC Public Key (ECDSA is the authentication algorithm) OTP24..31
- for STM32MP25x lines : OEM-KEY1 for authentication and EDMK1 for encryption of FSBL-A or FSBL-M. OEM-KEY2 is for the authentication and EDMK2 for the encryption of FSBL-M. FIP-EDMK for the encryption of the FIP.
STM32MP25x lines allows to use a dedicated set of keys for FSBL-M by fusing the bit 8 of OTP17. stm32key automatically fuse bit 8 of OTP 17 after having successfully programmed OEM-KEY2.
stm32key list OEM-KEY1: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) for FSBLA or M OTP144..151 EDMK1: Encryption/Decryption Master Key for FSBLA or M OTP364..367 OEM-KEY2: Hash of the 8 ECC Public Keys Hashes Table (ECDSA is the authentication algorithm) for FSBLM OTP152..159 EDMK2: Encryption/Decryption Master Key for FSBLM OTP360..363 FIP-EDMK: Encryption/Decryption Master Key for FIP OTP260..267
3. Authentication keys provisioning[edit source]
The key provisioning is the first step to enable the authentication: burn the keys in OTPs with the key hash output file from STM32 KeyGen.
3.1. Select keys[edit source]
Key is selected with the command stm32key select <key>
, with <key>=
stm32key select PKHTH PKHTH selected
stm32key select PKH PKH selected
3.2. Load keys file in DDR[edit source]
The keys hash file, output file from STM32 KeyGen, publicKeysHash.bin (for STM32MP15x lines ) or publicKeysHashHashes.bin (for STM32MP13x lines ), must be available in DDR before proceeding with the stm32key
command;
this file is assumed to be loaded at ${loadaddr} = 0xc4000000 in the next chapters.
For example the file can be loaded from a filesystem partition on a storage device by using the load
command (see documentation), if the file publicKeysHash.bin is in the bootfs (partition 7) on SD™ card (mmc0):
load mmc 0#bootfs ${loadaddr} publicKeysHash.bin
or
load mmc 0:7 0xc4000000 publicKeysHash.bin 32 bytes read in 50 ms (0 Bytes/s)
3.3. Verify keys file in DDR[edit source]
Once the publicKeysHash.bin (for STM32MP15x lines ) or publicKeysHashHashes.bin (for STM32MP13x lines ) file is loaded in DDR, you can verify the content of the file with the command:
stm32key read ${loadaddr}
Example for STM32MP13x lines with PKHTH
stm32key read ${loadaddr} Read PKHTH at 0xc4000000 PKHTH OTP 24: [c4000000] 27051956 PKHTH OTP 25: [c4000004] b56aef2d PKHTH OTP 26: [c4000008] 6215263c PKHTH OTP 27: [c400000c] 00000439 PKHTH OTP 28: [c4000010] 00000000 PKHTH OTP 29: [c4000014] 00000000 PKHTH OTP 30: [c4000018] 72429173 PKHTH OTP 31: [c400001c] 05020600
Example for STM32MP15x lines with PKH
stm32key read ${loadaddr} Read PKH at 0xc4000000 PKH OTP 24: [c4000000] 27051956 PKH OTP 25: [c4000004] b56aef2d PKH OTP 26: [c4000008] 6215263c PKH OTP 27: [c400000c] 00000439 PKH OTP 28: [c4000010] 00000000 PKH OTP 29: [c4000014] 00000000 PKH OTP 30: [c4000018] 72429173 PKH OTP 31: [c400001c] 05020600
3.4. Key provisioning[edit source]
To write and lock the keys in OTP, you use the command:
stm32key fuse ${loadaddr}
3.5. Verify keys file in OTP[edit source]
After the previous command, the device contains the keys to authenticate images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with PKHTH
stm32key read PKHTH OTP 24: 27051956 lock : 50000000 PKHTH OTP 25: b56aef2d lock : 50000000 PKHTH OTP 26: 6215263c lock : 50000000 PKHTH OTP 27: 00000439 lock : 50000000 PKHTH OTP 28: 00000000 lock : 50000000 PKHTH OTP 29: 00000000 lock : 50000000 PKHTH OTP 30: 72429173 lock : 50000000 PKHTH OTP 31: 05020600 lock : 50000000
Result for STM32MP15x lines with PKH
stm32key read PKH OTP 24: 27051956 lock : 50000000 PKH OTP 25: b56aef2d lock : 50000000 PKH OTP 26: 6215263c lock : 50000000 PKH OTP 27: 00000439 lock : 50000000 PKH OTP 28: 00000000 lock : 50000000 PKH OTP 29: 00000000 lock : 50000000 PKH OTP 30: 72429173 lock : 50000000 PKH OTP 31: 05020600 lock : 50000000
4. Encryption Decryption Master Key provisioning[edit source]
The EDMK key provisioning is the first step to enable the image decryption.
It is only available on STM32MP13x lines .
4.1. Select EDMK[edit source]
Key is selected with the command stm32key select <key>
, with <key>=
stm32key select EDMK EDMK selected
4.2. Load EDMK file in DDR[edit source]
The keys file must be available in DDR before proceeding the stm32key
command;
this file is loaded at ${loadaddr} = 0xc4000000 in the next examples.
The file edmk.bin can be loaded from a filesystem partition on a storage device by using the load
command (see documentation).
For example, the file edmk.bin is in the bootfs (partition 7) on SD™ card (mmc0):
load mmc 0#bootfs ${loadaddr} edmk.bin
or
load mmc 0:7 0xc4000000 edmk.bin 32 bytes read in 50 ms (0 Bytes/s)
4.3. Verify EDMK in DDR[edit source]
Then you can verify the content of keys files loaded in DDR with the command: stm32key read <addr>
Result for STM32MP13x lines with EDMK and ${loadaddr }=0xc4000000
stm32key read ${loadaddr} Read EDMK at 0xc4000000 EDMK OTP 92: [c4000000] 27051956 EDMK OTP 93: [c4000004] b56aef2d EDMK OTP 94: [c4000008] 6215263c EDMK OTP 95: [c400000c] 00000439
4.4. EDMK provisioning[edit source]
To write and lock the EDMK in OTP, you use the command with the same address:
stm32key fuse ${loadaddr}
4.5. Verify EDMK in OTP[edit source]
After the previous command, the device contains the keys to decrypt the images and it can be verified with the command:
stm32key read
Result for STM32MP13x lines with EDMK
stm32key read EDMK OTP 92: 00000000 lock : 50000000 EDMK OTP 93: 00000000 lock : 50000000 EDMK OTP 94: 00000000 lock : 50000000 EDMK OTP 95: 00000000 lock : 50000000
Warning: the content of the key cannot be read. It is masked, but the lock property can be verified to ensure that the key has been written.
5. Closing the device[edit source]
Once the authentication process is confirmed in ROM code and in TF-A, the device can be closed to ensure that only signed images can be used.
This operation is performed with the U-Boot command:
stm32key close