1. Article purpose[edit source]
This article explains how to configure TAMP internal peripheral.
This article describes the TAMP configuration performed using the device tree mechanism, which provides an hardware description of the TAMP peripheral.
2. DT bindings documentation[edit source]
The following binding-related documentation explains how to write device tree files for TAMP:
- TF-A: docs/devicetree/bindings/soc/st,stm32-tamp.txt
- OP-TEE: documentation/devicetree/bindings/hwmon/st,stm32-tamp.yaml
- Linux Kernel: Backup register management: Documentation/devicetree/bindings/power/reset/syscon-reboot-mode.yaml
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
3.1.1. STM32 TAMP node in Linux[edit source]
- for STM32MP13x lines
in stm32mp131.dtsi[1]
tamp: tamp@5c00a000 { compatible = "st,stm32-tamp", "syscon", "simple-mfd"; #address-cells = <1>; #size-cells = <1>; reg = <0x5c00a000 0x400>; ranges; nvram: nvram@5c00a100 { compatible = "st,stm32mp15-tamp-nvram"; #address-cells = <1>; #size-cells = <1>; reg = <0x5c00a100 0x80>; saes_secret_key: tamp-bkp@0 { /* see saes secret key feature */ reg = <0x0 0x20>; }; boot_mode: tamp-bkp@78 { /* see boot mode selection feature */ reg = <0x78 0x4>; }; boot_counter: tamp-bkp@7c { /* see boot counter feature */ reg = <0x7c 0x4>; }; }; reboot_mode: reboot-mode { compatible = "nvmem-reboot-mode"; nvmem-cells = <&boot_mode>; nvmem-cell-names = "reboot-mode"; mode-normal = <0x00>; mode-fastboot = <0x01>; mode-recovery = <0x02>; mode-stm32cubeprogrammer = <0x03>; mode-ums_mmc0 = <0x10>; mode-ums_mmc1 = <0x11>; mode-ums_mmc2 = <0x12>; mode-romcode_serial = <0xff>; }; };
- for STM32MP15x lines
in stm32mp151.dtsi[2]
tamp: tamp@5c00a000 { compatible = "st,stm32-tamp", "syscon", "simple-mfd"; #address-cells = <1>; #size-cells = <1>; reg = <0x5c00a000 0x400>; ranges; nvram: nvram@5c00a100 { compatible = "st,stm32mp15-tamp-nvram"; #address-cells = <1>; #size-cells = <1>; reg = <0x5c00a100 0x80>; boot_mode: tamp-bkp@50 { /* see boot mode selection feature */ reg = <0x50 0x4>; }; }; reboot-mode { compatible = "nvmem-reboot-mode"; nvmem-cells = <&boot_mode>; nvmem-cell-names = "reboot-mode"; mode-normal = <0>; mode-fastboot = <0x1>; mode-recovery = <0x2>; mode-stm32cubeprogrammer = <0x3>; mode-ums_mmc0 = <0x10>; mode-ums_mmc1 = <0x11>; mode-ums_mmc2 = <0x12>; mode-romcode_serial = <0xFF>; }; };
3.1.2. STM32 TAMP node in OP-TEE[edit source]
- for STM32MP13x lines
in stm32mp131.dtsi[3]
tamp: tamp@5c00a000 { compatible = "st,stm32mp13-tamp", "syscon", "simple-mfd"; reg = <0x5c00a000 0x400>; secure-interrupts = <GIC_SPI 128 IRQ_TYPE_LEVEL_HIGH>; clocks = <&rcc RTCAPB>; st,tamp-passive-precharge = <0>; st,tamp-passive-nb-sample = <0>; st,tamp-passive-sample-clk-div = <32768>; st,tamp-active-clk-div = <1>; };
- for STM32MP15x lines
in stm32mp151.dtsi[4]
tamp: tamp@5c00a000 { compatible = "st,stm32-tamp", "syscon", "simple-mfd"; reg = <0x5c00a000 0x400>; secure-interrupts = <GIC_SPI 197 IRQ_TYPE_LEVEL_HIGH>; clocks = <&rcc RTCAPB>; };
3.1.3. How to use TAMP Backup Registers[edit source]
In order to use free Backup registers, users should :
- locate one or more free Backup registers (cf STM32MP2 Backup register memoy mapping)
- Add the NVMEM cell description under the nvram node in the device tree
&nvram {
//TAMP_BKP127R : HEX(127*4) = 0x1FC
my_free_backup_register: tamp-bkp@1fc {
reg = <0x1FC 0x4>;
};
};
- Add a the nvmem-cells and nvmem-cell-names properties to the node of the device that would use the backup registers (following NVMEM consumer device tree bindings[5])
&my_device_node { nvmem-cells = <&my_free_backup_register>; nvmem-cell-names = "my_backup_register"; }
- Invoke nvmem_cell_get to get your nvmem_cell within your device driver and nvmem_cell_read/nvmem_cell_write to read or write the backup register(s). Please refer to the linux kernel documentation[6] for details). The following example increases by 1 the value in "my_backup_register":
struct nvmem_cell *my_cell = nvmem_cell_get(my_driver_dev, "my_backup_register"); if (IS_ERR_OR_NULL(my_cell)) { dev_err(my_driver_dev, "No cell for my device %ld\n", PTR_ERR(my_cell)); return PTR_ERR(my_cell); } //Read the cell int my_cell_length = 0; int* my_cell_content = nvmem_cell_read(my_cell, &my_cell_length); *my_cell_content += 1; //Update the cell nvmem_cell_write(my_cell, &my_cell_length,sizeof(int)); ...
3.2. DT configuration (board level)[edit source]
3.2.1. STM32MP1 TAMP node append (OP-TEE specific)[edit source]
The board definition in the device tree may include some additional board-specific pin control management, some global configuration for the tampers and the backup registers configuration.
Example for STM32MP13x lines in core/arch/arm/dts/stm32mp135f-dk.dts :
&tamp { st,backup-zones = <10 5 17>; st,tamp-passive-nb-sample = <4>; st,tamp-passive-sample-clk-div = <16384>; wakeup-source; wakeup-parent = <&exti>; /* Tamper button */ tamp_button: tamp-passive@2 { status = "okay"; reg = <EXT_TAMPER_2>; pinctrl-0 = <&tamp0_in2_pin_a>; st,tamp-mode = <TAMPER_CONFIRMED_MODE>; }; /* Connect pin8 and pin22 from CN8 */ tamp-active@3 { pinctrl-0 = <&tamp0_in3_pin_a &tamp0_out1_pin_a>; reg = <EXT_TAMPER_3>; st,tamp-mode = <TAMPER_POTENTIAL_MODE>; status = "disabled"; }; };
Learn more about the topology of the backup registers in pages:
3.2.2. STM32MP2 TAMP node append (OP-TEE specific)[edit source]
The STM32MP25x lines embeds a RIF board device tree source file. The TAMP peripheral is RIF-Aware, meaning it is responsible to apply its own RIF configuration.
Contrary to the STM32MP1 series, the backup registers configuration is present in RIF configuration file . Learn more about the topology of the backup registers on STM32MP25x lines
platforms here.
Example for the STM32MP25x lines :
&tamp { st,protreg = < //Tamper configuration and interrupt can only be done by the CID1, secure and privileged context RIFPROT(RIF_TAMP_RESOURCE(0), RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN) //Monotonic counter 1 can be read and written by the CID1, secure and privileged context RIFPROT(RIF_TAMP_RESOURCE(1), RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_PRIV, RIF_CID1, RIF_SEM_DIS, RIF_CFEN) //Monotonic counter 2 can be read and written by the CID2, secure and privileged context RIFPROT(RIF_TAMP_RESOURCE(2), RIF_UNUSED, RIF_UNLOCK, RIF_SEC, RIF_PRIV, RIF_CID2, RIF_SEM_DIS, RIF_CFEN) >; //Declaration of the number of backup registers per zone (Zone1-RIF1, Zone1-RIF2, etc...) st,backup-zones = <24 24 24 24 12 12 8>; };
3.2.3. Common TAMP node append[edit source]
Some system configuration can be overriden in the board tamp node, as these depend of the board. These global configuration are defined for all external tampers.
- st,tamp-passive-precharge can be 0, 1, 2, 4, 8.
- 0 is no precharge, so the pull-up is disabled for all external passive tamper.
- 1, 2, 3, 4, 8 define the number of cycle the STM32 precharge the pin before checking the value (low/high) for all external tamper.
- st,tamp-passive-nb-sample: the number of sample to read in a row to raise a passive tamper. Can be 0 (activation on edge), 2, 4, 8.
- st,tamp-passive-sample-clk-div: clock divider to define frequency to read a sample for a passive tamper.
- st,tamp-active-filter:
- 0: Active tamper filtering disable
- 1: Active tamper filtering enable: a tamper event is detected when 2 comparison mismatches occur out of 4 consecutive samples.
- st,tamp-active-clk-div: clock divider to define the frequency of read/write cycle for all active tampers.
- wakeup-source: not yet implemented. TAMP event will exit from low power mode.
- st,backup-zones: Define the number of backup register per zone. Please refer to the YAML documentation
Each sub-node define an external tamper, and within this node:
- pinctrl-0 entry defines which pin for which tamper id (see stm32mp13-pinctrl.dtsi [7] for possible values). If only one pin is defined, the external tamper is a passive one, otherwise the external tamper is an active one (first entry is the input pin, second the output pin)
- st,trig_on defines the active level to activate this passive tamper (not used if pintctrl-0 as 2 entries). It depends also of st,tamp_passive_precharge value.
- if st,tamp_passive_precharge=0 this passive tamper activate at edge.
- if st,tamp_passive_precharge != 0, with st,trig_on defined, this passive tamper will activate if st,tamp_passive_nb_sample in a row are high. If not defined the passive tamper event is raised if st,tamp_passive_nb_sample in a row are low.
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in the documents listed in DT bindings documentation above. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties that are preserved from one generation to another. Refer to the STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information:
- ↑ arch/arm/boot/dts/stm32mp131.dtsi
- ↑ arch/arm/boot/dts/stm32mp151.dtsi
- ↑ core/arch/arm/dts/stm32mp131.dtsi
- ↑ core/arch/arm/dts/stm32mp151.dtsi
- ↑ Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml , NVMEM consumer device tree bindings
- ↑ Documentation/driver-api/nvmem.rst , NVMEM subsystem documentation
- ↑ core/arch/arm/dts/stm32mp13-pinctrl.dtsi