Signing tool release note

Revision as of 18:33, 29 January 2024 by Registered User
Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP25x lines

The STM32MPU Signing tool generates signed binary files from:

  • a binary image file,
  • a public Key file,
  • a private Key file.

More information can be found in the detailed release note referenced later in this article.

1. Signing tool - Version v2.14.0-MP25-B02[edit source]

Signing tool for Linux® and Windows® host PC
Download

Version v2.14.0-MP25-B02

Installing the Signing tool
  • To use STM32MP Signing Tool, the installation of STM32CubeProgrammer is needed.
  • The installation is then complete. To use this tool, follow the instruction given in Signing tool.
Detailed release note
  • Full details about the content of this tool release are available here.