This article explains how to import OpenSTLinux projects supporting FIP (TF-A firmware image package) into STM32CubeIDE on a Linux® workstation.
1. Overview[edit source]
It is possible to import, into an existing STM32MP15 project, some OpenSTLinux projects using STM32CubeIDE, v1.11.0, compatible with ecosystem release ≥ v4.0.0 .
This is done using the Import an OpenSTLinux project... Cortex®-A hierarchical project contextual menu, providing access to Linux®, TF-A, U-boot, and OP-TEE.
2. OpenSTLinux project structure[edit source]
All OpenSTLinux projects follow the same project structure approach with three main parts:
- Eclipse artifact, to make project usage easier
- Build artifact identifying clearly the project output
- Sources, as they appear in the Yocto Project® environment
Device tree sources are generated by STM32CubeMX into the DeviceTree/ directory of the Cortex®-A hierarchical project. They are automatically included inside the corresponding OpenSTLinux projects: Linux®, TF-A and U-boot, with:
- source file links
- dedicated Build target
STM32CubeIDE supports FIP. The FIP_artifacts/ directory of the Arm®-Cortex®-A hierarchical project hosts all the deployment objects needed to build the FIP image. Those objects are generated by the TF-A, U-boot, or OP-TEE projects.
3. Linux project[edit source]
Several Build targets are proposed for a Linux® project addressing device trees, module, and kernel.
Double-click on Build target to launch the corresponding compilation with the associated Yocto Project® SDK.
It is then possible to update the running STM32MP15 target with the new build artifacts using the STM32 Cortex-A Linux Deployment > Run Configurations... menu.
In this dedicated Run Configurations... menu, build artifact (such as device tree binary, module, kernel or other) is added using the Add... button and providing:
- Local path, on the Linux® workstation (here builld/arch/arm/boot/dts/stm32mp157-dk2f-mx-mx.dtb)
- Remote path, browsing the remote target file system
For a new device tree, it is possible to update the extlinux.conf target file to take it into account at the next target reboot. See the Actions sub-window.
After download of build artifacts to the STM32MP15 board:
- a script can be executed (optional)
- STM32MP15 board is rebooted (default)
4. Bootloader projects[edit source]
For ecosystem release ≥ v3.0.0 , the boot architecture has been updated, as explained in TF-A overview. Now, two objects are needed to update the STM32MP15 flash memory device: TF-A BL2 flash partition and FIP Image. Both of them are generated inside STM32CubeIDE:
- TF-A BL2 flash partition, available from TF-A project build artifact,
- FIP image, located into fip directory of FIP artifacts.
Since the FIP image relies onto three projects, some dependencies exist between TF-A, U-boot and OP-TEE.
all build target in those projects is launching the fiptool, which builds the FIP image. This succeeds only if all the objects are generated.
A build target using generated device tree sources is also proposed inside STM32CubeIDE.
These generated device trees are targeting only trusted mode so there is no support inside the OP-TEE project.
As depicted in the figure below, the generated device tree sources for TF-A and U-boot are inside the DeviceTree/ directory. They are linked into project TF-A and U-boot and specific build targets are generated:
- stm32 (stm32mp157c-mymp157cdk2-mx) for the TF-A project, which must be launched first,
- and all (stm32mp157c-mymp157cdk2-mx) for the U-boot project.
FIP image for the generated device tree is then available from the fip directory of FIP artifact.
From STM32CubeIDE release v1.8.0, it is possible to update bootloader objects (TF-A BL2 & FIP image) directly on a running STM32MP15 target. Before working with STM32CubeIDE, it is recommended to first update STM32MP15 boot flash memory with STM32CubeProgrammer.
All flash devices available on STM32MP157x-EV1 (SD-Card, eMMC, NAND & NOR) are supported by STM32CubeIDE. It is possible to update them, typically with customized device tree, thanks to integrated STM32CubeMX. Note that trusted image only is supported.
- SD card update with customized trusted image, SD card is also supported on STM32MP157x-DKx Discovery kit
and STM32MP135x-DK Discovery kit
- eMMC update with customized trusted image
- NAND update with customized trusted image
- NOR update with customized trusted image